Subscribe

Latest Blog Post

compare 34 collaborative robots

An All-Inclusive Collaborative Robot Solution at the Fraction of the Price

Mathieu Bélanger-Barrette
by Mathieu Bélanger-Barrette on Aug 2, 2017 7:00:00 AM

We have been seeing a lot of new collaborative robot companies appear in the last few years. Most of them (in opposite to bigger multinationals) will have super high-tech robots and all-inclusive solutions for end-users. It is the case for Productive Robotics, a company that is manufacturing all of their robots in the USA at the fraction of the price.


OB7 No Background (1).jpgProductive Robotics' first robot the OB7 is a 7-axis robot with a one meter reach and a 5kg payload. It doesn't seem that impressive, right? But this robot has all the features that a collaborative robot should come with. In fact, it has an embedded camera, an easy-to-use software, a small footprint and has safety light rings to indicate its movements. All of these features are available for less than 20,000 USD.

So to make a base line, Universal Robots UR5 that has a similar reach and payload but is uniquely a 6-axis robot with no options is at a price point of 35,000 USD. So this basically means that using either robot will almost bring back a return on investment twice as fast.

OB7-cobot.jpg

Other than pricing there is also a graphic interface and an easy programming method that allows beginners to program the robot easily. Also, it has been designed to fit with our 2-Finger Adaptive Gripper, isn't that cool?

To learn more about the robot itself, I recommend to take a look at their website. If you want to get more information on different collaborative robots, take a look at our buyers guide or comparison sheet that we've built just for you!

choose the right collaborative robot

 
x

Subscribe to Robotiq's Blog

Leave a comment

Mathieu Bélanger-Barrette
Mathieu works as the production engineer at Robotiq, where he strives to constantly optimize the production line for Robotiq Grippers. Mathieu is always looking for new manufacturing processes to make operators as efficient as possible. He is also seeking out new robotic applications and their effect on improving our world, then keeps Robotiq’s blog readers updated on his finds.
Connect with the writer:

Related posts

What's New in Robotics This Week - Sep 08

 - Manufacturing & cobot roundup- John Deere acquires Blue River Technologies- Meet Musio - India's Ganpati bot and much more....

Emmet Cole
By Emmet Cole - September 8, 2017
How Procter and Gamble Is Leading the Way With Cobots

The consumer goods industry is starting to accept collaborative robots. Procter and Gamble is leading the way, and has been for...

Alex Owen-Hill
By Alex Owen-Hill - September 6, 2017
How to Quickly Integrate Your New Collaborative Robots

Collaborative robots are a massive new trend that makes life easier for businesses by providing safe and easy to program option...

Mariane Davids
By Mariane Davids - September 5, 2017

Is it possible to save programs using a network connections rather than the USB key

Hi pros,anyone know if it is possible to save programs on our plant network directly from the UR rather than saving on a USB stick? Could we also load the programs from the network? Read more

Is it possible to process the image acquired from the wrist camera with a different img proc toolbox

Because of the camera's form factor and integration with Robotiq products, I'd like to use the wrist camera. However, I need to leverage some of the features and functions that Halcon Merlic offers....Read more

Updated specs for new FT300 sensor?

So I'm looking at this page in the FT300 manual and it says it was last updated April 2017.With the overhaul of the sensor that decreased signal noise, are the updated specs available anywhere...Read more