Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

Fast Setup for Robotic Welders at Fabtech

Samuel Bouchard
by Samuel Bouchard. Last updated on May 05, 2016 5:09 PM
Posted on Nov 11, 2014 8:50 AM. 2 min read time

Fabtech, the largest metal fabrication show in the US, is happening in Atlanta this week. Robotiq and partners are presenting Kinetiq Teaching, a device designed to make your robotic welder fast and easy to program, even reducing the setup time between runs. We are also displaying our latest 2-Finger Adaptive Gripper.

What you'll see in Robotiq Booth #C2230

fabtech robot

The Robotiq booth will display our full range of products: Adaptive Grippers, Force Torque sensors and Kinetiq Teaching. Our friends at Cross brought a UR robot to display our new 2-Finger 85 Adaptive Gripper on a Universal Robot arm.

Our partners Yaskawa/Motoman also provided a robot so that we can do hands on demonstrations of Kinetiq Teaching. Kinetiq Teaching is a device that can be added to their reliable arc welding robots to make it easier and faster to program with minimum training. To allow this, Kinetiq Teaching has the following two features:

  1. Ability to hand-guide the welding torch to the desired positions
  2. A user-friendly, icon-based interface that does not require any programming skills

What you'll see in Yaskawa/Motoman Booth #C1534

A few aisles away from the Robotiq booth is the Yaskawa booth. In their booth you will have the chance to try Kinetiq Teaching. It will be set up as a complete cell from their ArcWorld linenup of pre-engineered welding cells. This welding machine is a great example of a turnkey system that you can put on your shop floor to start welding right away. The demo also shows how compatible Kinetiq Teaching is with their latest MA1440 welding robot and how easy the DX200 robot controller is to use with the external axis. 

robotic welder

 

So, if you want to try out Kinetiq Teaching or take a closer look at any of our Grippers, stop by for a visit at Fabtech. By the way, this is also a good opportunity to get hands on expertise and maybe even some answers to those questions about your particular automation dilemma.

Looking forward to seeing you in Atlanta!

COMPARE SPECIFICATIONS FOR 31 WELDING ROBOTS  RIGHT HERE

Leave a comment

Samuel Bouchard
Written by Samuel Bouchard
Samuel is CEO and co-founder of Robotiq. His mission is to free human hands from repetitive tasks. He is also the author of Lean Robotics: A Guide to Making Robots Work in Your Factory. He lives in Québec City with his wife and four children.
Connect with the writer:
http://robotiq.com

Related posts

What's New In Robotics? 13.03.2020

Good morning. In this week's news mix: Universal Robots launches UR+ Application Kits, Kassow begins new cobot production and...

Emmet Cole
By Emmet Cole - March 13, 2020
10 Steps to Automate a Finishing Process

Looking back to only a year ago, automate finishing applications with a cobot was something that only robotics experts were...

David Maltais
By David Maltais - March 5, 2020
Why Partnerships Are Now the Future of Robotics

Collaboration is truly the future! A lot of robotics companies are partnering up now. Why are partnerships important and what...

Alex Owen-Hill
By Alex Owen-Hill - February 25, 2020