Subscribe

Latest Blog Post

Integrate two grippers and one UR robot

Call for Beta Users: 2-Finger Gripper Tactile Sensors

Jean-Philippe Jobin
by Jean-Philippe Jobin on Nov 30, 2016 7:00:00 AM

Robotiq is ready to test out a new technology in the field! We’ve developed tactile sensors that fit on the 2-Finger Gripper, which have the potential to improve grasping abilities for robots.

demetan8-1.png

The tactile sensor built by Robotiq is an ultrasensitive multimodal tactile sensor that can measure pressure, contact location, and vibration. Designed to be installed on the 2-Finger Gripper, the tactile sensor pads replace the usual fingertips and connect to a data acquisition module at the base of the 2-Finger Gripper.

Software is then used to interpret data from the tactile sensors, to determine the quality of the good grasp.

More information on the philosophy behind the Robotiq 2-Finger Gripper Tactile Sensor is available here.

Apply here for the beta program. A 2-Finger Gripper is required to qualify for the beta program.

We have a limited set of test units to loan and will confirm the chosen testers by the end of December.

 

Integrate two grippers and one UR robot

 
x

Subscribe to Robotiq's Blog

Leave a comment

Jean-Philippe Jobin
Written by Jean-Philippe Jobin
Jean-Philippe Jobin co-founded Robotiq in 2008. As CTO, he leads Robotiq's R&D team to develop, produce and support the company's robotics solutions from hardware to software.
Connect with the writer:

Related posts

Join Us for Happy Hour at Automate!

What's trending on DoF this week? Robotiq on RBR50 2017 list, Automate Happy Hour event, 2-Finger Gripper force setting, code...

Amanda Lee
By Amanda Lee - March 23, 2017
Robotiq’s Gripper URCap Now Supports Multiple Grippers on the Same Arm

Our popular Gripper URCap for Universal Robots is getting a serious upgrade, just in time for Automate 2017 in Chicago. The new...

Karine Simard
By Karine Simard - March 15, 2017
Continental Automotive Pushes for Industry 4.0 With Robotiq and Universal Robots

When Continental Automotive Spain pushed Industry 4.0 in their factory, it saw the immediate advantage of easy integration,...

Amanda Lee
By Amanda Lee - March 13, 2017