Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

How To Handle Fragile Parts With Robots

Samuel Bouchard
by Samuel Bouchard. Last updated on May 05, 2016 4:26 PM
Posted on Jul 17, 2011 10:03 PM. 4 min read time

Robots were initially used in dull, dirty and dangerous jobs. Today, you can add yet another D to that list: delicate. Handling fragile parts comes with its challenges. This article offers examples and guidelines to use to avoid damaging fragile parts when handling them with a robot.

Fragile parts are subject to damage from three sources:

  1. Excessive holding/handling force from the gripper

  2. High acceleration/deceleration from the robot

  3. Being crushed while picked or placed

Here are a few fragile part examples by industry:

  • Electronics Industry: handling thin wafers

  • Food Industry: handling fruits, vegetables or baked goods that vary in size and shape 

  • Automotive Industry: handling ceramic catalytic converters

  • Casting Industry: handling wax patterns in investment casting - any deformation made on the wax part will result in a deformation in the final metal part 

Best practices for handling fragile parts with robots

Robotiq Adaptative Gripper manipulating an egg

Different factors can be considered at the gripper, robotic system or programming levels to avoid damaging parts.

Gripper level

  • Position control
    Control the gripper position to avoid finger collision damage.

  • Force control
    Control the force to avoid crushing the part.

  • Force sensing
    For very precise force control, you'll need feedback using force sensing.

  • Gripping modes
    Encompassing grips will have more contact points and distribute the pressure more evenly on a part.

  • Fingertip design
    Similar to an encompassing grip, it is possible to adapt the finger shape for more friction surface to distribute the pressure or use a soft material, to reduce the necessary actuation force.

Robotic system level

  • Vision system
    A vision system can be used to adjust the trajectory precisely to avoid hitting the part and to pick it up in the proper orientation.

  • Compliance device or force-torque sensor
    Compliance, or force-torque control, can be used at the wrist to avoid hitting the part or coming at it too hard.

Programming level

  • Minimize acceleration and deceleration
    This will reduce the reaction efforts from the tool due to acceleration. Having smooth trajectories with gradual acceleration will also help.

  • Part orientation
    Choose a place and orientation to pick the part so it minimizes the required holding force.

 

Leave a comment

Samuel Bouchard
Written by Samuel Bouchard
Samuel is CEO and co-founder of Robotiq. His mission is to free human hands from repetitive tasks. He is also the author of Lean Robotics: A Guide to Making Robots Work in Your Factory. He lives in Québec City with his wife and four children.
Connect with the writer:
http://robotiq.com

Related posts

What's New In Robotics?  07.12.2018

-UR celebrates 10 years since 1st sale-China robot production data -World's first automated ferry -Hello Bennu-Elowan the...

Emmet Cole
By Emmet Cole - December 7, 2018
Demo Week Highlights

What's trending on DoF this week? Demo week kick-off, circle move looped twice, security planes, use of Arduino to control...

Amanda Lee
By Amanda Lee - February 9, 2017
Trending on DoF This Week - Nov. 17

What's trending on DoF this week? Using one snapshot position to sort multiple parts, sampling rate for polishing, Revtech...

Amanda Lee
By Amanda Lee - November 17, 2016