Subscribe

Select Topics

Posts by Tag

See all
W3Schools.com

Kate Stern is a freelance editor specializing in robotics. Based in Montreal, she has 3 years' experience helping research labs and businesses refine their writing.

What Is Dynamic Tactile Sensing?

When it comes to robots that are built to handle objects, tactile sensing is one of the keys to success. Obviously, it’s helpful for a robot to feel what it’s holding and understand its grasp position, so it can manipulate the object properly. But what you may not realize is that tactile information is not only about sensing static events, such as contact location or forces – it’s also about sensing dynamic events.

Kate Stern
By Kate Stern
on Jun 06, 2017 7:00 AM. 4 min read time
 
What Is Dynamic Tactile Sensing?

When it comes to robots that are built to handle objects, tactile sensing is one of the keys to success. Obviously, it’s...

Kate Stern
By Kate Stern
on Jun 06, 2017 7:00 AM
Read more 4 min read time

Leave a comment

Written by
Connect with the writer: