Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

What's New In Robotics?  10.05.2019

Emmet Cole
by Emmet Cole. Last updated on May 10, 2019 6:59 AM
Posted on May 10, 2019 6:44 AM. 8 min read time

Good morning.  In this week's news mix:  Yaskawa's new European plant opens, Ford's 'Survival' robot is unveiled and why Albrecht Jung has deployed 8 cobots in 5 years.  We also admire an autonomous cargo trip, boggle at Blue Origin's lunar bot, meet 'Ugo' a teleoperated domestic robot and much more! 

Cobots & manufacturing

Yaskawa Motoman officially opened a new EUR25 million robot factory and robotics development centre in Slovenia, Europe this week.  Driven by growing demand for industrial robots in Europe, Russia, the Middle East and Africa, the factory supplements Yaskawa's existing production facilities in Japan and China and will satisfy about 80% of European demand for Motoman robots.  The new facility is expected to produce 10,000 industrial robots per year, including cobots.  (H/T IntelliNews)

Carmaker Ford has developed a mobile delivery robot called 'Survival' that's designed to deliver spare parts to factory workers.  As CNBC reported this week, the bot, which recently rolled out in Valencia, Spain is the first of its kind to be deployed in one of Ford's European manufacturing facilities...

 

Toyota has opened a hybrid electric vehicle battery manufacturing facility in Chachoengsao province, Thailand, with cobots "integrated into the production environment to efficiently work in conjunction with humans in the production and quality control process."  (H/T The Nation)

Albrecht Jung introduced its first UR5 cobot as part of a research project five years ago.  Following the success of their cobot deployment, the firm now has eight cobots working in close collaboration with humans on smart radio assembly tasks... 

 

Vietnamese cobot maker Robot3T has grown rapidly since its founding in 2014 and now boasts more than 500 customers in 60 countries and territories, according to company sources quoted in The Star

100995
The firm's R3T-02 cobot has a payload of 3 kg (6.61 lb) and a repeatability of +/- 0.15 mm (0.005 in) Credit: Robot3T

To resolve the problems faced by SMEs, the Robot3T team has focused on building specific robots with simple structures, high efficiency and low costs that are easy to operate for SMEs.

Australis Engineering released video this week showcasing a neat setup in which a TM5 cobot detects an object based on its shape, then picks it up and places it in its correct position on the puzzle board; otherwise known as completing a jigsaw puzzle...

 

In other cobot & manufacturing news:

Elsewhere...

An autonomous uncrewed surface vessel successfully completed a cargo run from the UK to Belgium early this week, traversing some of the world's busiest shipping lanes in the process.  The 12 meter (39.37 ft)- long SEA-KIT Maxlimer took 22 hours to deliver its cargo (a 5 kg (11.02 lb) box of oysters), moving at a speed of 4 knots.   (H/T BBC News

 _106858057_theboxofmersea-caughtoystersdeliveredbysea-kitseenhereonthe...
Credit: SEA-KIT International

Blue Origin founder Jeff Bezos unveiled the company's lunar lander for the first time, Thursday.  The 'Blue Moon' space bot will have a payload of 3.6 metric tons. 

 105904733-1557437271008imagefromios7.530x298

 Via CNBC:

"I love Vice President Pence's 2024 lunar landing goal," Bezos said, adding that Blue Origin can meet that timeline "because we started this three years ago."

Chinese researchers have created a skeletal robot of Caudipteryx (a non-flying dinosaur with 'proto-wings') to investigate whether the passive flapping motions of its proto-wings could have led to the evolution of flying in this species. They tested the bot on a treadmill and confirmed that running indeed causes a flapping motion in the proto-wings. (H/T Xinhua)

screen_shot_2019-05-07_at_4.04.25_pm
Credit: Jing-Shan Zh et al.

The Verge profiled the work of Miro Robotics,  a Japanese firm hoping to bring teleoperated robot butlers to our homes.  Ugo is expected to go on sale in 2020, with a price tag of around USD225 per month for rental.  

AAB8yAb.img
The Ugo robot is operated by a team of humans.  Credit: Miro Robotics

Meanwhile, in other headlines:

  • Indian Scientists Are Working on a Robot to Patrol the Borders  (Vice)
  • This Robot Hummingbird Is Almost as Agile as the Real Thing  (IEEE Spectrum)
  • New drones check ships for cracks and rust  (AlphaGalileo)
  • A dust devil passed over NASA's lander on Mars  (CNN)
  • Two AgriFood Robotics Startups Raise $15m for Diverse Applications across Supply Chain  (AgFunder News)


Come by next week for more of the latest robotics news!  Until then, please enjoy...


Five vids for Friday

1.  Interns at NASA's Langley Research Center are working on a series of 3D-printed soft robot actuators to study how such devices might be built and used in space.  (NASA has the full story.)

2.  VOA’s Elizabeth Lee reported this week on the robotic leg developed at the University of Southern California that can learn to walk by itself in just 5 minutes.  (H/T VOA News)

 

3.  Researchers at the University of Zurich have been throwing balls at drones for fun to study the effects of perception latency on the speed with which robots can move through cluttered environments.  (Paper: How Fast is Too Fast? The Role of Perception Latency in High-Speed Sense and Avoid)

4.  Experts at The Institute for Human & Machine Cognition in Florida, USA have developed a series of algorithms that enable Boston Dynamics' Atlas humanoid to autonomously make its way across narrow terrain.  (H/T Washington Post)

5.  Roboticists and medics from Johns Hopkins Applied Physics Laboratory and the Johns Hopkins School of Medicine are working together to better understand bio-inspired path replanning in robot swarms.  How do groups of animals manage to change direction mid-journey and can this skill be implemented in groups of robots?  

Leave a comment

Emmet Cole
Written by Emmet Cole
A freelance robotics writer since 2006, Emmet is an Economist contributor, and a regular contributor to Robotics Business Review and Robotics Trends. His writing on robots has also appeared in Wired, BBC Future, BBC Focus magazine, Space Quarterly, and numerous other outlets.
Connect with the writer:

Related posts

8 Benefits of Palletizing Cobots in the Coffee Packaging Process

The coffee industry is very competitive. If you're looking for a way to solve labor shortages, speed up your processes, reduce...

Nicolas Lauzier
By Nicolas Lauzier - November 16, 2022
How to capture sharper images of moving objects

So you’d like to count or inspect moving objects?  Here are a few tips that might help you out.

You can work with a few...

Audrey Boucher-Genesse
By Audrey Boucher-Genesse - May 7, 2020
Surface Finishing: The Essential Guide for Busy People

Surface finishing makes the difference between a quality product and a bargain-bin reject. This guide explains how to choose...

Alex Owen-Hill
By Alex Owen-Hill - February 22, 2020