Subscribe

Latest Blog Post

screw insertion using robotiq camera

What's New in Robotics This Week - Mar 31

Emmet Cole
by Emmet Cole on Mar 31, 2017 7:00:00 AM

Robot skins & robot touch; Artificial intelligence brief (Musk, deep-learning & more); Automation & jobs debate redux; Trust issues, and much more. We hope that the news we have selected will interest and amuse you. Enjoy!  

Robot Skins & Robot Touch 

Researchers at MIT’s Computer Science and Artificial Intelligence Laboratory have developed a prototype "robot skin" that's designed to to demonstrate the feasibility of flexible, printable electronics. 

The device combines sensors and processing circuitry and responds to mechanical stresses by changing the color of a spot on its surface. 

Robohub reports that "the device was inspired by the golden tortoise beetle, or “goldbug,” an insect whose exterior usually appears golden but turns reddish orange if the insect is poked or prodded — that is, mechanically stressed." 

ROBOT SKIN.jpg

Meanwhile in Glasgow, researchers unveiled a solar-powered, synthetic skin system made of graphene which, the researchers hope, could greatly enhance the sense of touch in robotic and prosthetic devices. 

 

 

Forbes reports: 

The hope is that with more self-powered prosthetics 'on hand,' amputees could hike up into the mountains or head out to sea– without having to lug along any extra external batteries for their limbs. And robots coated entirely in the touch-sensitive graphene skin could have a much easier time picking things up and dropping them off, too. As long as that touchy bot's not growing any human skin, a softer more sensitive robot... sounds like a good thing.

And in Japan, researchers at Keio University’s Faculty of Science and Technology revealed the GP-Arm --a general-purpose robotic arm with a delicate touch: 

GP-Arm includes a master controller arm and a slave arm that grasps things and performs other movements. A human operates the three fingers of the master to control the movements of the slave, which conveys the tactile sense of the objects gripped back to the master. For example, if the slave arm is moved to pick up a lemon, the fingers of the master will stop in a position corresponding to the size of the lemon and will not tighten further. Tactile force is communicated through the interaction between the gripping force of the slave arm and the elastic force of the object being gripped. 

 

Artifical Intelligence Brief 

Elon Musk launched a new brain-computer interface venture this week. Dubbed Neuralink, the new project will create brain implants with the ultimate aim of (as The Verge puts it) "helping human beings merge with software and keep pace with advancements in artificial intelligence." 

Musk has hinted at the existence of Neuralink a few times over the last six months or so. More recently, Musk told a crowd in Dubai, “Over time I think we will probably see a closer merger of biological intelligence and digital intelligence.” He added that “it's mostly about the bandwidth, the speed of the connection between your brain and the digital version of yourself, particularly output." On Twitter, Musk has responded to inquiring fans about his progress on a so-called “neural lace,” which is sci-fi shorthand for a brain-computer interface humans could use to improve themselves.

(The project was also featured in The Economist's Babbage podcast.)

OpenAI, a nonprofit research institute cofounded and funded by Elon Musk, announced that it has discovered an easier-to-use alternative to reinforcement learning that gets rival results when it plays games and performs other tasks. 

Meanwhile, researchers demonstrated that artificial intelligence can cooperate more effectively than humans, by enabling AIs to teach themselves themselves how to cooperate in games in which the objective is to reach the best possible outcome for all players. 

Science reports: 

The feat is far harder than training artificial intelligence (AI) to triumph in a win-lose game such as chess or checkers, researchers say. The advance could help enhance human-machine cooperation.

[...] by the end of the game, the machine-only teams worked together almost 100% of the time, whereas humans cooperated an average of about 60% of the time. “The machine-learning algorithm learned to be loyal,” Crandall says.

NASA AI.jpg

MIT Technology Review ran an interesting piece on Nvidia's "deep-learning chips," which are being used in medical deep-learning applications; the BBC featured Toronto's Vector Institute for Artificial Intelligence; and Space reported on how NASA's Autonomous Sciencecraft Experiment helped researchers monitor volcanic activity in Ethiopia earlier this year. 

Automation & Jobs Debate Redux

We covered this topic last week, but it's worth returning to as the debate grew even louder  over the past seven days. 

United States Secretary of the Treasury Steven Mnuchin told CNBC that robots replacing jobs is "not even on my radar screen." This prompted MIT Technology Review to publish "Actually, Steve Mnuchin, Robots Have Already Affected the U.S. Labor Market." 

PricewaterhouseCoopers report found that up to 30% of existing UK jobs could be impacted by automation by the early 2030s and a study from the U.S. National Bureau of Economic Research found that each new robot added to the workforce meant the loss of between 3 and 5.6 jobs in the local commuting area. 

The New York Times reported that robots are "winning the race for US jobs" and the Daily Star reported on potential losses in the bricklaying industry due to the arrival of a new bricklaying robot. Elsewhere, The Conversation argued that to "really help US workers, we should invest in robots." 

Trust Issues

A recent survey of Europeans conducted by the European Commission found that, overall, people have a positive attitude towards robots. 

 

 

However, as The Guardian reports "while most respondents were OK with robots being involved in space exploration or manufacturing, about 60% thought robots should be banned from looking after children, the elderly or the disabled. About 34% thought robots should be banned from education, while between 20 and 27% of those surveyed wanted them banned from healthcare and leisure activities." 

At what seems like the other end of the spectrum, Scottish researchers are working with a "socially intelligent" Pepper robot to see whether it could be used to tackle loneliness.

skynews.img.1200.745.jpeg

Via Sky News

Professor David Lane, director of the Edinburgh Centre for Robotics, told Sky News: 'Robots are helping us in the way that we work in manufacturing, in hazardous environments and in healthcare.'There are going to be lots of applications where robots will be working as assistants alongside people.'

As this little kid demonstrates, some people have no trust issues with "robots" at all (via Inverse "This Adorable Child Has Not Yet Learned to Fear the Machines"). 

 

 

 I'll be back next week with more news from the world of AI and robotics. Until then, I hope you enjoy these videos and links! 

 

 

 

 
 


 
 

 

 World’s First Machine Tool Robot Made from Carbon Fiber (Modern Machine Shop
How to make employees comfortable when you add robotics to your production facility (Control Design
Elbit offers multimission, unmanned naval robot (Defense News
Houses to be grown using plant-robot hybrids (Horizon Magazine)
Japanese authorities decry ongoing robot failures at Fukushima (TechCrunch
RISE wants to battle lionfish with robots (Mashable
These 6 Trends Are Retooling Manufacturing as We Know It (Singularity Hub
Minneapolis firm's Robot Fear Index shows little fear (Star Tribune
Delft University of Technology organizing first anti-drone race (Robohub)
Robot Economics - Justifying The Investment (Process and Control Today

grippers for collaborative robots

 
x

Subscribe to Robotiq's Blog

Leave a comment

Emmet Cole
Written by Emmet Cole
A freelance robotics writer since 2006, Emmet is an Economist contributor, and a regular contributor to Robotics Business Review and Robotics Trends. His writing on robots has also appeared in Wired, BBC Future, BBC Focus magazine, Space Quarterly, and numerous other outlets.
Connect with the writer:

Related posts

Why Humans Should Stop Worrying About Robots Taking Their Jobs

When the topic of robots in manufacturing comes up, the first thing people talk about is a fear of losing their jobs to robotic...

Mariane Davids
By Mariane Davids - June 19, 2017
What's New in Robotics This Week - Jun 16

Manufacturing & cobot roundup, the Tertill launch, Softbank-Boston dynamics deal, 2060: It begins and much more! We hope that...

Emmet Cole
By Emmet Cole - June 16, 2017
How Today's Collaborative Robots Are Cheaper Than Fenced Options

Until recent years, robots in manufacturing were limited to fenced options that were large, took up a lot of space on the...

Mariane Davids
By Mariane Davids - June 13, 2017

Yes, We Now Support Two Grippers on One UR Arm!

...actually, we support up to four Grippers on the same arm.Our new Gripper URCap software upgrade now includes multiple Grippers control. But that’s not all!Here is the list of new features and bug...Read more

Remote control of Universal Robots user interface

Hi. Has anyone tried to or does anyone know how to remote control Polyscope, the user interface of Universal robots? I’ve had the idea to install VNC server on a robot to be able to remote control...Read more

Improve cycle time when using the Robotiq Gripper

Hi Pros,In some applications where cycle time is critical, saving a few seconds here and there can be important. Here's a new program template that allows you to save a few tenths of seconds...Read more

Allighnment with integrated force sensing of UR5

In our application we have a UR5 with a Robotiq Gripper, Is it possible to use a force feedback to aid in aligning the palletizing program to the presented pallet or work surface. I began...Read more