Subscribe

Latest Blog Post

compare new collaborative robots

Playing with Legos just got a Boost to the Next Level !

Mathieu Bélanger-Barrette
by Mathieu Bélanger-Barrette on Jan 25, 2016 7:00:00 AM

Yesss, playing with Legos just got funner, well maybe not for your five year old, but for the AFOLs out there. In fact, the game that consists of creating different structures, shapes, cars and planes with blocs is now making its way into the future. We are now actually able to assemble Legos with a robotic arm. Such a thing was not possible a couple years ago for various reasons. Let's see what makes it possible now?

weblegofturag-1.jpg

But first, here are a couple of videos that show how things are done. 

ArtiMinds Christmas tree

Some of the videos have a Christmas theme. Since we are just out of the holidays, it makes sense, right? 

MIT students are playing with Lego during undergrad??

In one of the MIT labs, you can spot students playing with Legos... well, they are not actually playing, they are learning and who said learning had to be boring.

Robotiq Playing with Legos at Olympus Games

Here is a short video from one of our sales people who went to visit one of our distributors (Olympus Controls) and set up a robot arm to reconstruct a Christmas tree made of Legos. 

So how it is done?

All videos have common points. They all use:

  • force feedback to locate and fix the Lego block at the right spot.
  • Adaptive Grippers to grasp different types of blocks with the same Gripper. 
  • collaborative robots. 

Using Force Feedback

The force feedback is achieved with a Force Torque Sensor such as the FT 150 to able to sense what the robot is feeling. In fact, in this particular case, you need to know if one part is well aligned with the next part. To determine this, you cannot use vision, you need to feel it. The exact same way a human would recognize the clipping of the 2 blocks, the robot will recognize the exact same thing. Without this device, the robot would simply go to a requested position and wouldn't know if the block was inserted correctly or not. 

Adaptive Grippers

Such technology enables the user to grasp all the different Lego shapes and sizes with a single Gripper and with a single programming path. The fact that the Gripper can adapt to the width of the part, makes the operation a lot easier. Another nice feature of the Gripper is that it is force limited, in this case, you can put a small force setting and not crush the blocks. 

Collaborative Robots

It is not obligatory to use a collaborative robot like the UR5 for this type of application, but you should note that they are a lot safer than a regular industrial robot. This means that you can play Lego with or alongside the robot. :)

The other much appreciated aspect of these robots is the fact that they are easy to teach. In fact, using the teach by demonstration technique, you can easily show some path points to the robot and create a basic routine with the robot. It is a lot easier to program than a regular robot, so you have more time to build your Millennium Falcon! 

If you need more information on how to achieve a project with a Force Torque Sensor, I highly recommend to take a look at the eBook on Force Torque Sensor – An Introduction.

Download everything you need to know about collaborative robots

 

 

 

 

 
x

Subscribe to Robotiq's Blog

Leave a comment

Mathieu Bélanger-Barrette
Mathieu works as the production engineer at Robotiq, where he strives to constantly optimize the production line for Robotiq Grippers. Mathieu is always looking for new manufacturing processes to make operators as efficient as possible. He is also seeking out new robotic applications and their effect on improving our world, then keeps Robotiq’s blog readers updated on his finds.
Connect with the writer:

Related posts

What's the Difference Between Digital and Analog I/O?

Analog and Digital I/O is a fundamental concept in robotics. What is the difference between them? We answer a question from the...

Alex Owen-Hill
By Alex Owen-Hill - June 14, 2017
New Updates to Improve Your Wrist Camera's Speed and Accuracy

What's trending on DoF this week? Our new Wrist Camera URCap is now two times faster with our latest performance updates. We...

Amanda Lee
By Amanda Lee - June 8, 2017
Share Your Programming Hacks on Universal Robots

What's trending on DoF this week? Handy helper functions for UR, new teaching method sneak peek, Parker automation controller,...

Amanda Lee
By Amanda Lee - June 1, 2017

How to control 2-Finger Gripper via MODBUS RTU ?

I and using 2-Finger Gripper and I want to control its position, force speed using MODBUS RTU.The gripper is connected to a Windows PC via a USB port and uses a USB to RS-485 converter.I'm writing...Read more

50 Different pallet layouts

I have an application where a UR10 is palletizing boxes. There is about 50 different sizes which means 50 different pallet layouts. Multiple box sizes a day so it is always changing. I am...Read more

2 Finger Gripper(85) on a Universal Robot 5

I need to have in ROS Gazebo and MoveIt an UR5 robot who has the Robotiq 2 Finger Gripper(85) in the simulation models. At the moment all I have is the UR5 model only for simulations. How do I add...Read more

open source robot arm

Hi everyone,  how can I get a low cost open source robot arm for my final year projet.Thanks.PRINCEWILL Read more