Subscribe

Latest Blog Post

build your in-house robotic expertise program

Lowercase's 5-Day Integration Project

David Maltais
by David Maltais on May 31, 2017 7:00:00 AM

Two friends without any manufacturing background wanted to bring back eyewear production to the United States. They started their brand, Lowercase NYC, and automated their processes right from the beginning. In only five days, they’ve programmed a Universal Robot and Robotiq’s 2-Finger Gripper to operate the CNC machine by itself, allowing the three employees to focus on the countless things they have to do in this start-up business.


2-finger-cnc-machine-lowercase-6-657820-edited.jpeg

Since the 80’s, American eyewear manufacturers were all bought by foreign interests, stopping the domestic production in the process. Since then, most American eyewear brands sell products that are made overseas. Two years ago, an architect, Brian Vallario and his friend Gerard Masci, a finance worker, decided that the time has come to bring back something that was long gone in the American eyewear industry: the made in USA label.

Curious to see how they did that? Jump into the first of three videos from our latest case study!

 

“The main problem was that the integration cost of most robotic solutions was 3-4 times the cost of the solution itself.”

Since one of the co-founders came to the eyewear industry with a financial background, any equipment chosen to build the factory had to be worth every penny. Gerard Masci was willing to get started with collaborative robots, but he quickly realized that the price of a robot and the price of integration were two different things. 

In the case study's part 2, see how collaborative robots made financial sense for this young startup.

 

 

Building-Up Today’s Manufacturing Startups

Eyewear production is a very labor-intensive process and for a small team like Lowercase NYC, any improvement that can be made on overall efficiency is huge. Having a product that operates by itself allows every employee to sit at the computer and work on design or go work on the more labor intensive stuff that can’t be done by machines, for example.

Without seeing life through a pair of pink glasses, Brian Vallario and Gerard Masci definitely see great things coming for Lowercase. Automation is an important part of many of their future projects, not only regarding the addition of new robots in the factory, but also to raise hires.

In the third part of this case study, see why collaborative robots integration was a perfect match for Lowercase NYC from the beginning, but also for years to come. 

 

You can't be too small for cobots: It’s time for you to get started with your automation project today!

Request a FREE Quote Today!

 
x

Subscribe to Robotiq's Blog

Leave a comment

David Maltais
Written by David Maltais
After a few years working as a journalist, David switched to corporate communications and public relations. He focuses on spreading Robotiq's voice around the world via medias, partners and influencers of the automation and manufacturing industries.
Connect with the writer:

Related posts

CNCs in Decline? Nope. Manufacturers Are Getting Smart

Machine tool sales seem to be declining, but can it really be true? From our experience, CNC machines are as popular as ever....

Alex Owen-Hill
By Alex Owen-Hill - May 9, 2017
How the Role of CNC Operators Has Changed

Robotic machine tending could revolutionize CNC machine tending. But, where does that leave machine operators? Surprisingly,...

Alex Owen-Hill
By Alex Owen-Hill - April 11, 2017

Is it possible to save programs using a network connections rather than the USB key

Hi pros,anyone know if it is possible to save programs on our plant network directly from the UR rather than saving on a USB stick? Could we also load the programs from the network? Read more

Is it possible to process the image acquired from the wrist camera with a different img proc toolbox

Because of the camera's form factor and integration with Robotiq products, I'd like to use the wrist camera. However, I need to leverage some of the features and functions that Halcon Merlic offers....Read more

Updated specs for new FT300 sensor?

So I'm looking at this page in the FT300 manual and it says it was last updated April 2017.With the overhaul of the sensor that decreased signal noise, are the updated specs available anywhere...Read more