Subscribe

Latest Blog Post

compare new collaborative robots

How to Benefit from the Robotic Skill Shortage

Alex Owen-Hill
by Alex Owen-Hill on Mar 31, 2016 7:00:00 AM

Robotics is probably going to be one of the biggest job creators in modern history. But, are there enough qualified people to fill those jobs? As various sectors announce skill shortages, we look at how robotics is affected and which skills are the most important for employers.

10945708_s.jpg

Studies have shown that robotics is going to be a huge creator of jobs, despite scaremongering to the contrary from the media. However, those jobs require a particular set of skills, which the job market is struggling to provide.

Some sources within the industry say that there aren't enough skilled applicants to fill jobs in robotics and manufacturing. Plotr, a careers advice website, found that 52% of robotics engineering jobs in the UK are hard to fill, and almost all of these are due to skill shortages. A recent study by Deloitte predicted that 57% of US manufacturing jobs will be left unfilled over the next decade for the same reason.

What are Skill Gaps and Skill Shortages?

Skill gaps and skill shortages both refer to situations where there are not enough skilled people to fill the requirements of a job. However, although they are similar concepts, they are not exactly the same. A "skill gap" happens when a company's existing workforce does not have the required skills to fulfill the job. A "skill shortage" happens when the job can't be filled because there is a shortage of skilled applicants in the external job market.

Robotics can be affected by both of these situations. For example, bringing new robotic technology into the workplace can mean that existing workers don't have the skills needed to operate them. This produces a skill gap, which can be filled by training and/or hiring of new employees. However, due to a skill shortage in the wider job market, it may be difficult to find the right applicant.

40333135_s.jpg

Is There a Skill Shortage in Robotics?

Jobs in robotics require quite a wide range of skills. Robotics spans several different fields, including mechanical engineering and computer science. To be effective, applicants need skills like systems analysis, critical thinking and complex problem solving. As a result of this, working with robots is a “skilled job”, whereas in the past, jobs in the same workplace may have been “unskilled”. Employers have reported finding it difficult to fill jobs, because their applicants don't have the necessary level of technical skill needed to operate the robots.

A 2013 report by the International Federation of Robotics found that companies have been cutting back on low-paid, low-skill jobs since the beginning of the current global recession. This is apparently quite common during recessions. To replace these jobs, employers have been trying to improve the efficiency of their existing workforce, and robotics is one way to do this. However, this has led to the creation of skilled robotics jobs in many industries including manufacturing, electronics and the food industry. Unfortunately, this is often also combined with a skills gap in their existing workforce.

Skill shortages in the job market mean that many of these new positions are not being filled. A recent study by Deloitte Consulting and the Manufacturing Institute predicted that, of the 3.5 million US manufacturing jobs projected for 2015 to 2025, a huge 2 million of these positions will be left unfilled due to skill shortages.

Who is Affected?

The skills shortage is likely to affect everyone, including employers, job seekers and the existing workforce.

  • Employers need to provide training for their existing workforce, to ensure that a skills gap doesn't develop which can't be filled by hiring. The Deloitte study also found that involvement with local schools and community colleges can be effective, to ensure a future supply of engaged, skilled professionals.
  • Job seekers need to ensure that they are continually developing. Training can be costly for employers, so coming to a job interview with existing technical skills could greatly increase the chances of landing the job.
  • The existing workforce also needs to continually reeducate itself. Although robots are not replacing jobs directly, it does seem that many unskilled jobs are mutating into more skilled positions.

As Dan Kara, Practice Director of robotics at ABI Research, is quoted as saying: "You don’t want to be in a place where your job can be replaced by automation or technology. You want to be in a place where you’re the master of automation technology."

The answer, then, seems to be continual training for everyone involved. No longer is it the case that you can stop learning after you have finished your degree, apprenticeship or other training course. Robotics technology is continually developing and it is the responsibility of the entire workforce to keep up with technology, or risk skill shortages and skill gaps such as we are seeing now.

The Top Skill Which Robotics Employers Want

Although there are many technical skills required of robotics 40159456_s.jpgworkers, there is one skill which comes up again and again and again and again.

So, what is that skill? .... Programming.

Today, programming is required even for jobs which would previously have been low skilled. Factory workers who operate robots need to have at least a basic understanding of programming, even if they won't be writing lines of code.

But which programming language should you learn first? Check out our post to discover the Top 10 programming languages for robotics.

 

Have you struggled due to the skills gap? Do you think that the skills gap even exists? How do you ensure that you are continually trained? Tell us in the comments below or join the discussion on LinkedIn, Twitter or Facebook.

 

Risk Assessment with Collaborative Robots

 
x

Subscribe to Robotiq's Blog

Leave a comment

Alex Owen-Hill
Written by Alex Owen-Hill
Alex Owen-Hill is a freelance writer and blogger who writes about a large range of topics, including science, language, creativity and (of course) robotics. He completed a PhD in Telerobotics from Universidad Politecnica de Madrid as part of the PURESAFE project, in collaboration with CERN. As a recovering academic, he maintains a firm foot in the robotics world by blogging for gripper manufacturer Robotiq.
Connect with the writer:

Related posts

What's New in Robotics This Week - Aug 18

Manufacturing & cobot roundup, super self-healing soft bots, time to replace pets with bots?, A.I. set to reshape music and...

Emmet Cole
By Emmet Cole - August 18, 2017
How Cobots Promote Local Business

It’s a common misconception that as autonomy, AI and robotic systems become more commonplace, people will lose their jobs. Yes,...

Kayla Matthews
By Kayla Matthews - August 15, 2017
What's New in Robotics This Week - Aug 11

Manufacturing & Cobot Roundup; South Korea Ponders 'Robot Tax'; JPL's Clockwork Venus Rover; People Prefer Bots That Make...

Emmet Cole
By Emmet Cole - August 11, 2017

How to control 2-Finger Gripper via MODBUS RTU ?

I and using 2-Finger Gripper and I want to control its position, force speed using MODBUS RTU.The gripper is connected to a Windows PC via a USB port and uses a USB to RS-485 converter.I'm writing...Read more

50 Different pallet layouts

I have an application where a UR10 is palletizing boxes. There is about 50 different sizes which means 50 different pallet layouts. Multiple box sizes a day so it is always changing. I am...Read more

2 Finger Gripper(85) on a Universal Robot 5

I need to have in ROS Gazebo and MoveIt an UR5 robot who has the Robotiq 2 Finger Gripper(85) in the simulation models. At the moment all I have is the UR5 model only for simulations. How do I add...Read more

open source robot arm

Hi everyone,  how can I get a low cost open source robot arm for my final year projet.Thanks.PRINCEWILL Read more