Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

How To Reduce Wrist Camera Set-Up Time

Jérémy Martin
by Jérémy Martin. Last updated on Jul 06, 2017 7:01 AM
Posted on Jul 06, 2017 7:01 AM. 3 min read time

What's going on on DoF this week? An interesting question about the Wrist Camera that could be useful for lots of people, Center of Gravity calculus for end of arm tooling and most importantly, two new program templates from Annick Mottard and David Gariépy! A short read with lots of content, enjoy!

 Reduce The Set-Up Time for Your Wrist Camera

 This week, an interesting integration question from Sebastien Blanchette on DoF; How can we reduce the teaching time for the Wrist Camera when it is set-up on a mobile unit, where its position can change 1/2" between set-ups. 

Wrist Camera UR Best of UR Rsz1000 (101)-593475-edited.jpgBy using an advanced feature from the camera, allowing to locate parts on a workplane even if this workplane is higher or lower than the original one. Check out this program template to know how to use one of the camera's advanced feature!

Tool Center Point And Center of Gravity

Also popular on DoF this week, Colin and Gabrielle exchanged about how to calculate TCP and CoG depending on the end of arm tooling used. In the last post, Gabrielle shared with us all of the information needed to calculate the Center of Gravity when setting up different tools on your robot. Learn more about this conversation here.

Learn More About Two New Program Templates

This week again, DoF Pro and Robotiq's Annick_Mottard introduced a new program template, allowing to perform a torque tightening assembly application along UR wrist's Z axis. By using the FT300 Force Torque Sensor feedback to tighten parts up to a predefined torque, this allows repeatability in assembly lines, where precise torque tightening is required. Read more about this new program and upload it on our website to get started!

 

 

Another brand new program template from David Gariépy enables you to measure the dimension of an object by using the Robotiq 2-Finger Gripper with a precision of +/- 2mm. In this program template, you'll find a video demonstrating the application of the program template provided, a UR program template and a step-by-step detailed procedure. Check out this short video and learn more about it on DoF!

 

 

 Did we miss anything?  Ask the Pros on DoF!

 

grippers for collaborative robots

Leave a comment

Jérémy Martin
Written by Jérémy Martin
Connect with the writer:
http://robotiq.com/

Related posts

What's New In Robotics? 13.03.2020

Good morning. In this week's news mix: Universal Robots launches UR+ Application Kits, Kassow begins new cobot production and...

Emmet Cole
By Emmet Cole - March 13, 2020
10 Steps to Automate a Finishing Process

Looking back to only a year ago, automate finishing applications with a cobot was something that only robotics experts were...

David Maltais
By David Maltais - March 5, 2020
Why Partnerships Are Now the Future of Robotics

Collaboration is truly the future! A lot of robotics companies are partnering up now. Why are partnerships important and what...

Alex Owen-Hill
By Alex Owen-Hill - February 25, 2020