Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

White Paper: Flexible Automation of Machine Tending Operations

Nicolas Lauzier
by Nicolas Lauzier. Last updated on Jul 11, 2022 8:47 AM
Posted on Sep 10, 2012 4:45 PM. 2 min read time

Manufacturers doing machining are getting to a point where they need to automate machine tending: Statistics show that good machinists are hard to find and that it will not get any better in the years to come. So they want to get the most value of their skilled machinists. One way of doing this is having the machinists do the programming and the setups, then a robot do the loading and unloading of the parts.

For a lot of manufacturers, this is challenging because blanks can have different sizes and the machined parts can have any shape. This is one reason why several integrators and end users looked at taking advantage of the Robotiq Adaptive Gripper flexibility to handle a wide variety of parts. Still, precision of the machined parts must not be compromised.

You can see above a video of a study done in collaboration with ETS, a technical university based in Montreal. The work presents a robot control approach that can leverage the features of the Adaptive Gripper and the precision of the lathe tooling to obtain a flexible and precise robotic machine tending cell. The control uses compliance mode available today on most industrial robot controllers to enable free movement along given tool axis while maintaining constraints on others. Experiments were done on a cylindrical part turned back to back in a lathe. The part precision obtained by the robot was compared by the precision obtained by a human machinist. It is shown that the proposed approach could be used as the basis for flexible and precise robotic machine tending.

 

 

A robot feeding a CNC lathe using a 3-Finger Adaptive Gripper

A robot feeding a CNC lathe using a 3-Finger Adaptive Gripper

A white paper, which contains the experimental procedure and the detailed results, can be downloaded here

Banner of the Robotiq Machine Tending bundle

Leave a comment

Nicolas Lauzier
Written by Nicolas Lauzier
Senior Product Manager R&D
Connect with the writer:
http://www.robotiq.com

Related posts

How to Get More from the 3-Finger Gripper With ROS

The new Robotiq ROS package is now available! Here's what you need to know about the package. What is it? What does it include?...

Alex Owen-Hill
By Alex Owen-Hill - October 30, 2018
See Some Cutting-Edge Robotic R&D Projects

Robotiq provides a treasure trove of information to robotics developers and manufacturers, but it's also known for its Adaptive...

Mariane Davids
By Mariane Davids - April 30, 2018
Simplify Your Programming with These Force Torque Sensor Skills

What's happening on DoF this week?

Amanda Lee
By Amanda Lee - March 15, 2018