Subscribe

Latest Blog Post

What is ROS, and Can it Create a Universal Standard?

Mariane Davids
by Mariane Davids. Last updated on May 05, 2026
Posted on May 05, 2019 in
2 min read time

The biggest problem with robotics research is that everyone is working towards an individual goal. Industrial robotics is such a competitive field that numerous countries and companies prefer to keep their research a secret. As a result, advancements rarely make their way to the factory floor.

ROS, and by extension, ROS-Industrial, seeks to bridge this gap by creating pathways that are economical, so robotics can finally realize their full potential. Join us as we look at the strides ROS has made, and how it could contribute to a universal standard. 

 

Robotiq's 3-Finger Gripper is compatible with the latest version of ROS

 

A quick overview of ROS and ROS-Industrial

ROS is an open-source set of utilities and libraries for adding functions to robots. It's not a programming language, but it does work with a variety of them to make implementation easier.

The official website describes ROS as "an open-source meta-operating system for your robot." Many of the functions of an OS are present, such as hardware abstraction, low-level device control, and inclusion of standard functionality.

It provides tools and libraries for obtaining, building, and running code across multiple computers. It's similar to robot frameworks. The primary purpose of ROS is to facilitate code reuse in robotics research and development.

It is a distributed framework of processes, known as "nodes." These enable executables to be designed and coupled at runtime individually. To make things simpler, you can group the nodes into "packages" and "stacks," which are easy to share.

So, how does ROS differ from any other operating system? ROS supports a system of code repositories that allow you to distribute collaboration. The design, from the file system level to the community level, enables users to make independent decisions and bring everything together with ROS infrastructure tools.

This leads to several more goals of ROS as a whole:

  • Thin as Possible - Code written for ROS is usable with other robotic software frameworks. It's easy to integrate into other software frameworks as well.
  • Agnostic Libraries - The development model is to write ROS-agnostic libraries with clean function interfaces
  • Independent Language - The ROS framework is easy to implement into modern programming languages like Python, C++, and Lisp.
  • Scalable - ROS works with large runtime systems and development processes.

 

Can ROS become a universal standard?

ROS originally began as a small project at Stanford University, but it has since branched off into a separate branch known as ROS-Industrial. Robots in manufacturing have had largely the same functions for 20 years.

Advanced functionality has not been possible due to high costs. The research is being done, but applying to it to manufacturing floors is a complicated issue. There needs to be a return on investment for integrating and programming robots with agile processing.

ROS-Industrial seeks to bridge the gap by creating cost-effective solutions that allow robotic applications to reach their full potential without the extreme costs of integration.

It's highly possible that the goals of ROS will align with industrial standards sooner than we think. As a result, we could see it become a universal standard in the future for industrial robotics.

Do you think such a scenario is possible? Let us know in the comments!

Learn how to deploy Physical AI that works

Leave a comment