Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

RoboBusiness 2015 : Object Sensitive Gripping Panel

Samuel Bouchard
by Samuel Bouchard. Last updated on May 05, 2016 5:10 PM
Posted on Oct 06, 2015 5:01 PM. 3 min read time

RoboBusiness 2015 was held a couple of weeks ago. On top of the summary of the event that I published here, here is a summary of the Object Sensitive Gripping for Multi-Purpose Applications panel discussion I took part in with colleagues from the industry.

The panel was prepared and moderated by Tim DeRosett, Co-founder & CEO of Blue Ocean Robotics. Other participants were:

robobuisinessPic from YTenzer

Here are the main points that were discussed with summary answers from the panel.

Q1. What are the macro trends driving such a high-level of variability in manufacturing and logistics today?

Some of the trends include: shorter product life cycle, fickle customer demands and preferences, the desire for configurable products and the transition to e-commerce, as well as the continuous pressure to increase productivity.collaborative-robots-gripper

Q2. Gripping can be viewed as a technology that enables robots to do things they previous could not do. Can you provide real world examples of success in this area?

Technically, many high-mix applications in manufacturing are possible using standard grippers and tool changers. It's the ROI that did not make sense when very high flexibility was needed. Machine tending in SMEs is an example.

Q3. Are there particular application areas that demand flexibility that's not available in traditional gripping?

Picking for e-commerce, which deals with millions of different objects is absolutely impossible to perform using traditional gripping.

Assembly tasks are still limited by the gripper specifications. In the future, everything in the service robotics’ market in unstructured environments will require a new generation of gripper.

Q4. Perception is also thought of as an enabling technology. Yet today grasping & perception are viewed largely as separate technologies. Without divulging confidential information, can you envision a time when the two technologies converge? Please explain.

It's already happening. If you look at Fanuc, Rethink and Gomtec (now ABB), they are packaging whole solutions which include perception and gripping. This simplifies the integration and can increase the overall performance of the system. The challenge for them is to have something general enough in terms of perception and in terms of gripping so they can address a wide range of applications. This trend is a risk for gripper providers like us and an opportunity, we'll need to find a way to fit in with these packages. Other participants in the panel are going this way in their specific industries.

electronic-gripperQ5. Several factors drive decisions about the type of gripping technology to use for a particular application. How are you able to balance the need for flexibility, speed, reliability and ROI?

It's challenging, because speed and reliability data can be easily and directly integrated in a ROI calculation while flexibility can't. You really need to find those companies for which flexibility is causing big headaches for their operations..

Q6. How might gripping take advantage of recent advances in rapid prototyping and 3D printing?

3D printing can be used to make custom fingertips or fixtures quickly. This is just an intermediary step until we have truly flexible grippers that can adapt by themselves to the different parts. 3D printing could also be used in the manufacturing of grippers to integrate electronics and sensing.

Q7. Can you describe the trade-off between bullet-proof reliability and ‘consumable’ grippers?

In factories and distribution centers because of the demands placed on the grippers, and the fact that they can't afford to change the gripper every month even if it's really cheap... It needs to be reliable. 

CONCLUSION:

I really enjoyed taking part in this panel as everybody had a different and interesting point of view. It also struck me how the tooling manufacturers, just like the industry, are maturing in their business model. 

GET ROBOTIQ PACKAGE FOR UNIVERSAL ROBOTS

 

Leave a comment

Samuel Bouchard
Written by Samuel Bouchard
Samuel is CEO and co-founder of Robotiq. His mission is to free human hands from repetitive tasks. He is also the author of Lean Robotics: A Guide to Making Robots Work in Your Factory. He lives in Québec City with his wife and four children.
Connect with the writer:
http://robotiq.com

Related posts

What's New In Robotics?  07.12.2018

-UR celebrates 10 years since 1st sale-China robot production data -World's first automated ferry -Hello Bennu-Elowan the...

Emmet Cole
By Emmet Cole - December 7, 2018
Demo Week Highlights

What's trending on DoF this week? Demo week kick-off, circle move looped twice, security planes, use of Arduino to control...

Amanda Lee
By Amanda Lee - February 9, 2017
Trending on DoF This Week - Nov. 17

What's trending on DoF this week? Using one snapshot position to sort multiple parts, sampling rate for polishing, Revtech...

Amanda Lee
By Amanda Lee - November 17, 2016