Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

Be Warned When Colliding With Your FT 300 Force Torque Sensor

Amanda Lee
by Amanda Lee. Last updated on Nov 30, 2017 8:00 AM
Posted on Nov 30, 2017 7:00 AM. 2 min read time

What's happening on DoF this week?

  • We launched a brand new Skill for collision detection with the FT 300.
  • If you haven't heard about it yet, we released an updated free FT 300 URCap software.
  • To go along with the new URCap release, we have some retro-compatibility tips for you!
Learn more from automation Pros here!

Be warned when colliding with the FT 300

collision-detection-3.png

This week, Robotiq integration coach louis_bergeron shared a new Collision Detection Skill. You will be able to use the FT 300 Force Torque Sensor by preventing potential collisions between the end-effector and robot cell assets. This Skill uses the data measured by the FT 300 to define at which force and torque values a program will stop due to a potential collision. Don't wait and get it here!

Improve your FT 300 path recording with the new URCap

If you didn't know about it yet, we recently released an updated free FT 300 Force Torque Sensor URCap software to get the most out of every application. It enables the FT 300 to feed data to the Universal Robots force mode (available with Universal Robots CB3.1 controller only). It improves the path recording constant speed option and also unlocks the possibility to perform a wider range of high force control tasks such as sanding, polishing, grinding and deburring. Learn even more about it here.

 

Get access to a broader range of applications with retro-compatibility tips

As previously said, the new features of the FT 300 URcap make programming easier to fit a broader range of applications. However, in order to achieve this, here are a few retro-compatibility tips if you are using the 1.1.1 version of the URCap.

 

 Did we miss anything? Ask the Pros on DoF!

Get a quote for the FT 300

Leave a comment

Amanda Lee
Written by Amanda Lee
As an e-marketing coordinator, Amanda focuses on Robotiq's content management. With her background in marketing, she hopes to bring valuable, relevant, and consistent content to our audience through the blog, social media and video center.
Connect with the writer:

Related posts

How to Include a Force Sensing in a Robot Cell Design

You have decided to include force sensing in your robot application. Perhaps your task requires tactile feedback, flexibility,...

Alex Owen-Hill
By Alex Owen-Hill - May 17, 2021
9 Doubts to Clarify About Using a Force Sensing

Still unsure about using force sensing in your robotic application?

Even if you are convinced of the benefits of adding force...

Alex Owen-Hill
By Alex Owen-Hill - May 14, 2021
The 7 Best Robot Applications for a Force Sensor

Do you need a force sensor for your chosen robot application?

Some robot tasks benefit from the addition of force sensing....

Alex Owen-Hill
By Alex Owen-Hill - March 5, 2021