Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

The Oldest Robot

Samuel Bouchard
by Samuel Bouchard. Last updated on Jan 29, 2015 10:21 AM
Posted on Jul 09, 2007 3:54 PM. 1 min read time

 

The above New Scientist video shows a replica of a reprogrammable automaton from the 60s. Not the 1960s, the 60s, the design of a Classical Greek engineer named Hero.

A falling mass attached to a rope that separates into two provides the energy. Each rope end winds around an axle that turns a wheel. Pegs are used on the axles to program the movement (advance, back up, turn). By changing the amount of winding, they change the direction of the wheel’s motion. Adjustments to exactly where in the winding these changes of direction occur control the movement… until the mass reaches ground. Really ingenious, and pretty fascinating from where – and when – I stand, in 2007, working on robots activated by wires!

But is it really a robot? What is a robot, anyway? In the most general sense, a robot is a programmable machine. By that definition, Hero’s automaton is a robot. But not everyone would see it that way. Joseph Engelberger, widely considered the father of robotics, has said “I can't define a robot, but I know one when I see one.”

[via AI&R]

Leave a comment

Samuel Bouchard
Written by Samuel Bouchard
Samuel is CEO and co-founder of Robotiq. His mission is to free human hands from repetitive tasks. He is also the author of Lean Robotics: A Guide to Making Robots Work in Your Factory. He lives in Québec City with his wife and four children.
Connect with the writer:
http://robotiq.com

Related posts

Seven robots working for the health of our planet

Machines fueled by trash, super fast recycling sorters, and an invasive species zapper/vacuum: Here are a few of the robotics...

Philip Fine
By Philip Fine - September 10, 2019
The 3 Ways to Automate a Sanding Task

What's the best way to automate a sanding task? Material removal is vital for many manufacturing processes, but it take a lot...

Alex Owen-Hill
By Alex Owen-Hill - April 30, 2019
Let's Start a Conversation about Finishing...

 Catherine Elie showcases Robotiq's new Sanding Kit as we get ready to delve into the world of sanding, polishing, deburring...

Emmet Cole
By Emmet Cole - April 25, 2019