What's New In Robotics This Week - 18.05.2018
![Emmet Cole](http://blog.robotiq.com/hubfs/images/emmet-cole-220x220.jpg)
Posted on May 18, 2018 7:00 AM. 9 min read time
- Manufacturing & cobot roundup
- News from Universal Robots, AUBO, Techman, and Omron
- From human intelligence to automation design, "less is more"
- The wireless flying insect bot and octopus bot
- "Mindless" robots?
- And much more!
Manufacturing & cobot roundup
Japan's Omron Corp. and Taiwanese cobot firm Techman Robot Inc. announced the formation of a "strategic alliance on collaborative robots."
Continental is using cobots from Universal Robots and safety solutions from SICK to replace "inflexible testing and assembly lines"...
Writing in Forbes ("Robots: The Automation Juggernaut That Manufacturers Need"), Rethink Robotics' COO Jim Lawton shared some important questions to ask when deciding on a cobot solution:
- Who trains the cobot?
- How quickly can cobots be put to work?
- How many tasks can one cobot do?
- What kinds of tasks can cobots do?
- How much does innovation cost me?
- How smart is the cobot?
Fanuc's cobot was spotted helping with some fenceless 3D metrology inspection...
Meanwhile, according to Seeking Alpha, cobots "are the PCs of the Robot Era." An article in Harvard Business Review argued that "tomorrow's factories will need better processes, not just better robots," and Bloomberg profiled Japanese startup Preferred Networks Inc., which aims to apply deep learning techniques to manufacturing.
One of AUBO's cobots was spotted helping humans out with a progressive metal forming process...
Yaskawa plans to build a new factory in Slovenia (as reported by Japan Times).
Researchers at Université Laval are developing a "low impedance human-robot interaction" system for manufacturing applications...
Demand for automated guided vehicles and autonomous mobile robots used in manufacturing is "exploding," with global sales set to reach nearly $1.5 billion this year, and revenues from AMRs expected to grow by almost 75% during 2018, according to a new report (H/T Drives & Controls).
ABB's YuMi cobot was spotted on TV...
Engineers at the University of Sheffield Advanced Manufacturing Research Centre are "leading the way in collaborative robotics research in a drive to help SMEs integrate the technology onto factory floors" (H/T PES Media).
When cobots whisper "Relax. It's Friday"...
Elsewhere...
On the surface, the next story isn't directly related to robotics or AI, but check out the parallels between efficient biological design and efficient automation design. You have to wonder "How widely can this principle be applied?"
Researchers at Ruhr-Universität Bochum published imaging findings in Nature Communications this week that show "the more intelligent a person, the fewer connections there are between the neurons in [their] cerebral cortex."
Bear in mind that previous research has shown that intelligent people have larger brains and also that they display less neuronal activity than others when performing an IQ test.
So, putting all these findings together, the Ruhr-Universität Bochum team concluded that "intelligent brains possess lean, yet efficient neuronal connections. Thus, they boast high mental performance at low neuronal activity."
The chain reaction of Lean Robotics.
The parallels between these findings and the principles of Lean Robotics are intriguing. Less is more – at least in smart, effective automation projects.
In fact, throwing lots of effort into automation in the absence of lean design can lead to overkill and rapid project failure (the automation equivalent of how overthinking leads to cognitive inefficiencies). Lean robotics aims to cut out that waste.
Based on the principles of lean manufacturing, Lean Robotics shows you how to quickly design, integrate, and operate robotic cells that boast high performance for a minimal initial investment of time and money. It's smart manufacturing design that mirrors the best in biological design.
Biology sometimes sets efficiency standards that roboticists can only dream of replicating with current materials and power sources.
(Image: Wikipedia.)
The natural world displays this "less is more" principle in abundance. Through millions of years, nature has produced some incredibly efficient designs for locomotion, flight, vision, physical endurance, location mapping, energy consumption and intelligence.
And so roboticists constantly look to the natural world for inspiration, hoping to capture the incredible efficiency of biological systems.
For example, this week in the world of bio-inspired robotics, researchers from the University of Washington revealed RoboFly, which they say is the "world's first wireless insect-sized flying robot." The main engineering challenge? Powering the flapping system in an energy-efficient way.
Here things take a turn away from biology, as the team eventually decided to power the bot using a "narrow, invisible laser beam" to excite a photovoltaic cell that then converts the laser light into electricity...
Over at ICRA, researchers revealed a "bio-inspired octopus robot based on [a] novel soft fluidic actuator"...
And researchers at Cornell revealed a cute, partly bio-inspired prototype bot that can express its emotions through touch, "sending out little spikes when it’s scared or even getting goosebumps to express delight or excitement." The team compared the system to “human goosebumps, cats’ neck fur raising, dogs’ back hair, the needles of a porcupine, spiking of a blowfish, or a bird’s ruffled feathers.”
And a team from the University of Graz, Austria shared their research into the development of "robot spies" that can be used to study biological swarms, such as colonies of bees...
Despite all this talk of "intelligence" – and yet still in tune with the insight that "less is more" – tiny, self-powered, "mindless" vibrating robots are able to work together to move a corral, as demonstrated by researchers at the University of Bordeaux in France.
Intriguing stuff, even if you have to wonder to what extent a "mindless" robot can be called a "robot" at all.
Collections of small, simple bots may someday perform useful tasks like exploration, so researchers want to learn about their basic principles of operation. Credit: A. Deblais et al., Phys. Rev. Lett. (2018) (Via PhysOrg).
I'll be back next week with more robotics news. Until then...
Five vids for Friday
1. NASA announced plans to launch the first-ever helicopter on Mars in July 2020. The miniature, unmanned drone-like chopper, dubbed "The Mars Helicopter," weighs less than 1.8 kilos (4 lbs) and is about the size of a softball.
2. A team at MIT’s Little Devices Lab revealed a set of modular blocks that can be put together in different ways to produce diagnostic devices for testing blood glucose levels, detecting viral infections, and performing other functions.
3. Italian researchers unveiled a "lighter, cheaper robotic hand."
4. CNBC spent some time with Sharp’s humanoid bot, RoBoHoN, an automated travel companion for humans.
5. Boston Dynamics announced that it will start selling its SpotMini robot in 2019.
Leave a comment