Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

Start Using Force Feedback Loops for Insertion Applications

Amanda Lee
by Amanda Lee. Last updated on Jan 26, 2017 11:01 PM
Posted on Jan 26, 2017 7:00 AM. 3 min read time

What's trending on DoF this week? Spiral search using FT300 Sensor, UR10 risk assessment, increasing the sensitivity of the Gripper, gear insertion using FT300 Sensor and much more. Get the latest news from automation Pros!

Spiral Search Using FT300 Sensor

Screen Shot 2017-01-25 at 9.28.59 AM.png
Did you know that the sensor can also be used in a force feedback loop for insertion or assembly type applications? Tyler_Berryman wrote a subprogram to use a spiral search to find a hole. This type of subprogram is very useful for applications that require a precise insertion or that have a vision component integrated with the cell. Take a look at the demo video here.

UR10 Risk Assessment

A Pro who is quite new to collaborative robotics and the TS 15066 norm needs your expertise. He must conduct a risk assessment on a particular application to determine necessary controls. Do you have an example of a risk assessment previously completed that you could share with Aaron?

Increasing the Sensitivity of the Gripper

increasing-sensitivity-gripper.jpg

Another Pro who is very new to robotics needs your help! She's working with a UR10 in combination with Robotiq's 2-Finger Gripper and FT150 Sensor. She extended the Gripper's fingertips and has difficulties detecting the object when picking it up. This is why she wants to figure out if there is another way to control the sensitivity, such as communicating with the the FT150 sensor directly. Do you have any suggestions?

Gear Insertion Using FT300 Sensor

Screen Shot 2017-01-25 at 10.28.50 AM.png

Tyler_Berryman worked on a proof of concept for a potential customer that might useful for similar applications that you may be working on. This potential customer wants to insert gears into a Go-NoGo jig using the FT300 Sensor. The fit between the gear and the jig is fairly tight, this is why the Force Torque Sensor is used to match the teeth of both the gear and the jig. Discover how he accomplished this here

Standard Icons or Symbols for Robot Status

Can you help Karine_Simard? She is searching for a standard set of icons to represent different robot states, such as running, protective stop, emergency stop, etc. Let her know where she can find it!

 

building in-house robotic expertise program

Leave a comment

Amanda Lee
Written by Amanda Lee
As an e-marketing coordinator, Amanda focuses on Robotiq's content management. With her background in marketing, she hopes to bring valuable, relevant, and consistent content to our audience through the blog, social media and video center.
Connect with the writer:

Related posts

Trending on DoF This Week - Jan. 19

What's trending on DoF this week? Unstacking using UR's built-in Seek function, manual tool changer, getting a UR on WIFI,...

Amanda Lee
By Amanda Lee - January 19, 2017
Top Manufacturers of Robotic Tool Changers

Robotic tool changers are useful devices when you only have one robot station to carry out different processes. This short...

Mathieu Bélanger-Barrette
By Mathieu Bélanger-Barrette - October 28, 2014