Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

How Palletizing Cobots Relieve the Manual Strain at Ornua Dairy

Nicolas Lauzier
by Nicolas Lauzier. Last updated on Aug 07, 2024 8:53 AM
Posted on Aug 07, 2024 8:36 AM. 3 min read time

Ornua, a leading Irish dairy cooperative, wasn't churning out the efficiency they desired. Their manual palletizing process, involving a variety of heavy dairy products, was a recipe for employee strain and reduced productivity.

Ornua palletizing


The headache of manual palletizing

Manual palletizing of dairy products, from 6kg blocks of cheese to 12kg packs, took its toll on Ornua's employees. Constant bending, stretching and lifting meant a high risk of repetitive strain injury (RSI) and fatigue. This was not only impacting on employee well-being, but also hampering overall production. It was vital to find a solution that would meet these physical demands while retaining flexibility for a variety of products.

 

 

 

Smoother operation: The Robotiq solution

Ornua found the answer in Robotiq's Palletizing Solution with the UR20 cobot. This collaborative robot integrated seamlessly into their existing operations, eliminating the need for isolated, cumbersome automation systems. The user-friendly interface made it easy for employees to collaborate with the cobot, maintaining the human element that was crucial to their production environment.

 

Transforming the bottom line

Implementing an automated palletizing solution at Ornua brought these results:

  • Reduced RSI: Physically demanding tasks were taken over by the cobot, significantly reducing the risk of injury.
  • Increased productivity: A 30% boost in palletizing efficiency resulted in a smoother, faster production flow.
  • Happier Employees: Freed from the physical strain, employees reported increased satisfaction and morale.          

"We looked at palletizing as the first area to explore automation due to the number of human resources needed. If we can automate that task, then those resources can be used elsewhere."
Jack Cotton, Ornua's Continuous Improvement Lead
                   


The takeaway: A win-win for efficiency and employee well-being

Ornua's success story demonstrates the power of collaborative automation. By adopting Robotiq's Palletizing Solution, the company has not only improved efficiency, but also created a safer and more pleasant working environment for its employees. It's a win-win situation for productivity and employee satisfaction, proving that sometimes the best way to succeed is to let robots do the heavy lifting.

ornua case study banner

Leave a comment

Nicolas Lauzier
Written by Nicolas Lauzier
Senior Product Manager R&D
Connect with the writer:
http://www.robotiq.com

Related posts

The Secret Ingredient of Nutriset's Success: Palletizing Cobots

Nutriset Group, a pioneer in the fight against malnutrition, is committed to both employee well-being and operational...

Nicolas Lauzier
By Nicolas Lauzier - August 22, 2024
Investing in Automated Palletizing: A Strategic Move for 2024

As we navigate through 2024, forward-thinking manufacturers are setting their sights on the horizon, anticipating the economic...

Nicolas Lauzier
By Nicolas Lauzier - July 17, 2024