Subscribe

Latest Post written about

robot-grippers

Grippers for Collaborative Robots

When putting a collaborative robot cell together, many design decisions have to be made. First of all, the robot itself, its different functionalities and specifications. Then the controller, the programming methods, the emplacement on the work floor have to be considered. Finally, you must make a choice of robot grippers to be used. Most robotic cell design underestimates the importance of the gripper choice for collaborative applications. I would compare the right gripper to the right tires on a race car. This may be underestimated too, since the tires are the only contact the race car has with the ground, where it gets all its traction. A race car with bad tires, results in a bad race. Same thing for a gripper, it is the only peripheral of the robotic cell that will touch the part you are manufacturing. A cell with a bad gripper will probably result in bad cell performance. 

Mathieu Bélanger-Barrette
By Mathieu Bélanger-Barrette
on Mar 09, 2015 in Robot Grippers. 7 min read time
Grippers for Collaborative Robots

When putting a collaborative robot cell together, many design decisions have to be made. First of all, the robot itself, its...

Read more 7 min read time
How Does a Parallel Robot Gripper Work?

Choosing a robot gripper can sometimes be confusing. As there are a wide choice of different grippers out there, you really...

Read more 5 min read time
How to Design Custom Fingertips for Your Application?

When designing any kind of mechanical device, you need to consider the context where it will work. Designing custom fingertips...

Read more 5 min read time
Why Did MIT Choose the 3-Finger Robot Gripper from Robotiq?
I get asked very often, "Who is typically using the robotic hand from Robotiq?". Well, it is very hard to describe a specific...
Read more 3 min read time
How to Design Gripper Fingertips

Designers of robotic grippers are always trying to enhance the gripping performance of their product. Some will increase force...

Read more 4 min read time
Fast Integration of 2-Finger 85 Adaptive Gripper on Universal Robots

Using robots is often associated with complexity and programming time sinks. With the introduction of collaborative robots,...

Read more 3 min read time
Top 5 Applications using Universal Robots

The popularity of Universal Robots is undeniable. You may ask yourself why this robot is so popular in the robotic market. The...

Read more 5 min read time
Contactless Robot Teleoperation at Arts et Métiers ParisTech

Robotic collaborative applications are mostly related to robots working autonomously alongside humans. The robot is helping...

Read more 3 min read time
How to Install the 2-Finger 85 Adaptive Gripper on Universal Robots

Our goal at Robotiq is to facilitate the integration of robotic grippers in automation processes. As integration includes...

Read more 3 min read time

Leave a comment