Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

Adjustable Safety Features on Universal Robots

Mathieu Bélanger-Barrette
by Mathieu Bélanger-Barrette. Last updated on May 05, 2016 4:15 PM
Posted on Sep 13, 2015 9:10 PM. 2 min read time

The safety of collaborative robots is sometimes put in doubt because of the fact that it is a new concept. In fact, just because it can work alongside humans, doesn’t mean that people are comfortable working alongside robots. To avoid such concerns, manufacturers have develop ways to reduce or eliminate the possibility of impact. In fact, by reducing the speed of the robot while the worker is working beside it reduces the possibility of contact with the worker. 

collaborative-robot-safety

Fixed Safety Zone

Many collaborative robot manufacturers have develop ways to reduce the speed of the robot arm when the robot is in a certain zone. The first way to do this is to establish fixed reduced speed areas where the robot will reduce its speed while in this zone. An area established by planar points is virtually placed in the robot workspace and once the robot enters this virtual space it will reduce its speed for the next operation it is programmed to perform. The following video explains how this can be done with a Universal Robots

Video from Cross Automation

This kind of safety feature would be close to the 'Safety-rated Monitored Stop' as described in the ISO 10218 standard. This new term applies to the robot drive system where it has limitations built-in to ensure safe speeds and/or torques as explained above.

Variable Safety Zone

If you want to go a step further in your safety features you can add a vision or laser system that can monitor the robot’s surroundings. By doing this you can establish different safety zones for different robotic functions and program the robot react to these zones. In fact, in this video, if a worker is entering the reduced speed safety zone the robot will reduce its speed but will still continue to achieve its task. If you enter the next zone which is closer to the robot, the robot will fall into the stop safety zone, where the robot will brake completely and stop all its motions. Once the worker exits this zone, the robot will resume its motions and continue its program from where it left off. Notice that the robotic cell is equipped with a light that broadcasts the state of the robot. Orange for reduced speed, red for safety stop and green for full speed ahead. You should also notice that the robot has a fourth mode which is an emergency stop. This is the same as any other robot where the robot will stop all its motions and will need a reset before going back to its program. 

Video from Axis Systems

This kind of safety feature would be closer to the 'Speed and Separation Monitoring' as described in the ISO 10218 standard. 

If you need further information on how to realize a safe robotic cell you may want to look at the following document that goes into more detail on collaborative robots and the risk assessments necessary when implementing a robotic cell. 

GET THE EBOOK ON COLLABORATIVE ROBOT RISK ASSESSMENT

Leave a comment

Mathieu Bélanger-Barrette
Mathieu is a production engineer at Robotiq, where he constantly strives to optimize the production line for Robotiq Grippers. He enjoys discovering new robotic applications and sharing what he learns on Robotiq's blog.
Connect with the writer:
http://robotiq.com

Related posts

8 Benefits of Palletizing Cobots in the Coffee and Tea Packaging Process

The coffee industry is very competitive. If you're looking for a way to solve labor shortages, speed up your processes, reduce...

Nicolas Lauzier
By Nicolas Lauzier - November 16, 2022
Improve Your Efficiency in Logistics Operations With Robots

Is it possible to improve the efficiency in logistics with robotics?

Unlike in other areas, it's not always obvious how robots...

Alex Owen-Hill
By Alex Owen-Hill - November 12, 2021
Packaging in Logistics: How to Streamline Packaging With Cobots

Packaging is a core task in logistics. But, a lot of packaging processes are inefficient. They are not well suited to the...

Alex Owen-Hill
By Alex Owen-Hill - October 29, 2021