Subscribe

Latest Blog Post

Sweet success: How a world-renowned candy manufacturer in Germany scaled palletizing across multiple lines

Piotr Tyburzec
by Piotr Tyburzec. Last updated on Mar 26, 2026
Posted on Mar 26, 2026 in Palletizing
5 min read time

Automation rarely starts with a full factory transformation.

More often, it begins with a single line. One challenge, one opportunity, one team ready to try something different.

What matters is what happens next.

amit-lahav-LU_fCezP9-o-unsplashPhoto by Amit Lahav on Unsplash 

Tackle a real constraint, not the whole plant

At a major confectionery site in Germany, end-of-line palletizing had become a recurring bottleneck: inconsistent pallets, heavy manual handling and throughput pressure during seasonal peaks. Rather than automating the whole factory, the team asked a practical question: where can we create immediate, repeatable impact? The answer was a single, reusable palletizing cell.

Design the pilot for reuse and for people 

The pilot focused on three practical goals: stabilize end-of-line operations, raise pallet consistency and reduce manual strain for operators. Key design choices made the cell replicable across lines:

  • Configurable pallet patterns for common box formats
  • Handling standard Euro pallets (800 × 1,200 mm) and pallet heights up to ~2.4 m
  • Reliable pick performance in the 6–10 picks/min range and an intuitive operator HMI

Because the cell was built as a template rather than a bespoke one-off, it was straightforward to adapt to other lines.

From pilot to program -- fast

The pilot produced measurable gains in consistency, ergonomics and throughput stability. Those results changed the conversation: automation shifted from a theoretical improvement to an operational capability.

Within roughly a year of the first deployment the site had deployed lines 1 and 2 and was preparing to roll out lines 3 and 4 — a clear signal the pilot had become a repeatable model. Reused tooling, pallet patterns and commissioning checklists shortened design and commissioning times for follow-on cells, so benefits arrived sooner across the site.

Why the ROI worked 

Their ROI wasn’t a single headline figure — it came from several reliable, repeatable improvements:

  • Labor & ergonomics. Stations that needed two operators moved to one for routine operation, delivering predictable recurring savings and lower ergonomic risk.
  • Throughput stability. Repeatable pallet patterns and predictable pick rates removed hidden capacity losses and let the upstream line run at designed speeds.
  • Fewer rework events. More consistent pallets reduced rebuilds, manual interventions and unplanned downtime.
  • Faster future rollouts. Standardized templates reduced engineering and commissioning effort, accelerating the realization of plant-wide benefits.

Two early projects reached payback in under 12 months; a third was scoped with an expected 1–2 year payback — outcomes driven by operational improvements rather than a single dramatic saving.

What to measure for a defensible ROI 

Capture these before/after inputs to build a clear ROI case:

  1. Net FTE change and hours saved per week per station
  2. Throughput uplift or reduced variability (cases/hr, fewer stops)
  3. Rework & scrap reductions (pallet rebuilds per week)
  4. Downtime & maintenance impacts (manual interventions, changeover time)
  5. Weeks saved on subsequent installs due to standardization

Translate those into annualized savings and compare them to your expected annual benefit to estimate payback in months.

Quick checklist for a reusable palletizing pilot

  • Choose modular tooling that covers your box formats and pallet heights.
  • Build a small, selectable library of pallet patterns accessible from the HMI.
  • Keep changeovers short and document SOPs.
  • Stock common spares locally and provide a one-page troubleshooting guide.
  • Involve operators and maintenance in commissioning so the system isn’t “worked around.”

Results at a glance

  • Site: world-renowned candy manufacturer (Germany)
  • Project set: 3 projects for one site (2 closed, 1 in project-identification)
  • Rollout pace: Lines 1 & 2 deployed; lines 3 & 4 preparing for deployment within ~1 year of the pilot
  • Payback: 2 projects under 1 year; 1 project 1–2 years
  • Pick rate: 6–10 picks/min
  • Pallet format: 800 × 1,200 mm; heights up to ~2.4 m
  • Packaging: cardboard boxes
  • Approach: configurable palletizer + standardized tooling and templates

Related case studies 

For more examples of the same repeatable approach in other food & beverage settings, see: a bread palletizing success story, Hack AG and a vodka palletizing implementation. These show how a reusable approach and simple templates speed deployments in different product categories.
Eckerts distillery

Top 5 key takeaways

  1. Start small, design for reuse. A focused pilot that is modular and templateable creates the fastest path to scaling.
  2. Measure the right things. Labor (FTEs), throughput variability, rework, downtime and deployment efficiency drive a defensible ROI.
  3. Make operators part of the solution. Simple HMIs, short training and maintenance involvement prevent the system from being “worked around.”
  4. Standardize to accelerate rollout. Reusable tooling, pallet patterns and commissioning checklists dramatically shorten design and commissioning for follow-on cells.
  5. ROI is the sum of many parts. Payback often comes from multiple modest, repeatable improvements (ergonomics, throughput stability, fewer rebuilds and faster deployments) rather than a single headline saving.

Bottom line: palletizing ROI in high-volume confectionery is the cumulative effect of reduced labor, improved throughput stability, less rework and the ability to replicate a flexible pilot quickly. Start with a well-scoped cell, measure the right KPIs, and use those wins to build a repeatable rollout plan.

👉 Try the Palletizing Fit Tool to get a quick, personalized read on your palletizing potential and the inputs you need to model ROI.

Screenshot 2025-09-08 at 9.41.29 AM

Leave a comment

Related posts

How IQ Gives Manufacturers a Faster, More Predictable Path to a Running Palletizing Workcell

Getting a palletizing project done right has always depended on having the right information at the right time. Product specs,...

Robotiq Team
By Robotiq Team - June 12, 2026
Robotiq Launches IQ to Make Palletizing Automation Faster and More Predictable

Most manufacturers who want to automate palletizing face the same problem. Getting a straight answer on whether it fits their...

Robotiq Team
By Robotiq Team - June 2, 2026
Why Do Palletizing Automation Projects Fail? 5 Pitfalls and How to Fix Them

Palletizing automation is one of the clearest wins in end-of-line operations. The ROI is real, the labor savings are immediate,...

Amanda Lee
By Amanda Lee - May 27, 2026