Subscribe

Latest Blog Post

Robotiq Improves the 2F-85 and 2F-140 Adaptive Grippers

David Maltais
by David Maltais. Last updated on Dec 12, 2024
Posted on Nov 08, 2018 in Robot Grippers
1 min read time

Robotiq has released the next generation of adaptive grippers for collaborative robots: the 2F-85 and 2F-140. Both models feature many new updates, while retaining the same key benefits that have inspired thousands of manufacturers to choose them since their launch 6 years ago.

Video time!

 

The new Adaptive Grippers are less exposed to factory air, dust, and fluids. Their finger bases have been redesigned to simplify fingertip changeover and ensure a reliable grip. The overall design is smoother and rounder, with every sharp edge removed. Each one also includes an accessories holder near the base. The new 2F-85 and 2F-140 are connected to Universal Robots’ safety function, making them more collaborative than ever.

“We kept the basics of our winning recipe, but improved the final taste,” explains Robotiq CTO Jean-Philippe Jobin. “Our patented finger design, which enables both internal and external parallel gripping, as well as a unique encompassing grip mode, is key to making these grippers the most flexible on the market. This launch builds on the release of our Hand-E Gripper in June. Manufacturers can now choose the best up-to-date Robotiq Adaptive Gripper for their needs.”  

The 2F-85 remains the top choice for applications involving heavy objects and high pinch force, while the 2F-140 is ideal for picking objects of almost any size and shape. Finally, Hand-E is perfect for high-precision tasks and harsh industrial environments.

Talk to an expert

Leave a comment

Related posts

Hand-E Now Reaches 100 mm Without Giving Up an Ounce of Precision

If you've been using Hand-E Adaptive Gripper on your production line, you already know why it's earned its reputation: a...

Robotiq Team
By Robotiq Team - July 16, 2026
How Sennheiser increased PCB testing by 33% with a Robotiq 2F-85 gripper

At Sennheiser Manufacturing USA in Albuquerque, precision is non-negotiable.

Every week, the facility assembles 30,000 printed...

Linnea Bruce
By Linnea Bruce - February 11, 2026
Robotiq brings the sense of touch to Physical AI

Physical AI has reached a critical point. Robots can see, plan, and decide better than ever—but manipulation in the real world...

Jennifer Kwiatkowski
By Jennifer Kwiatkowski - January 27, 2026