Subscribe

Latest Blog Post

Tech giants choose Robotiq

Linnea Bruce
by Linnea Bruce. Last updated on Jun 03, 2025
Posted on Jun 03, 2025 in Robot Grippers
2 min read time

When the biggest names in tech choose a tool, the industry takes notice.

Recently, Robotiq Adaptive Grippers have been spotted in action at Amazon and NVIDIA Robotics. And no, we’re not just talking about behind-the-scenes speculation; these cameos showed up on their own social media feeds. From fast-paced fulfillment centers to next-gen robotic labs, the message is clear: when you need a reliable, versatile gripper, Robotiq delivers.

Why are Amazon and NVIDIA using Robotiq Adaptive Grippers?

Let’s start with what sets these grippers apart. Robotiq’s Adaptive Grippers aren’t just plug-and-play. You can plug, play, and adapt.
Whether it’s handling fragile products in a dynamic warehouse or assembling components with micrometer precision, these grippers give robots the flexibility and control they need to excel in real-world environments.

🦾 3 fingers? 2 fingers? Either way! Robotiq’s Adaptive Grippers conform to the shape of what they’re picking up without the need to change tools.
🔁 Repetitive or high-mix tasks? No problem. These grippers adjust on the fly, making them ideal for modern automation where product variety is high.
🤝 Tight integration with many top Robot brands means minimal coding, quick deployment, and rock-solid performance.

linkedin hand-e gripper

NVIDIA: AI meets adaptive gripping

When NVIDIA Robotics recently showcased their work on AI-enabled robotic systems, a familiar gripper made an appearance: the Robotiq 2F-140.

In their video, the gripper performs assembly-like movements with impressive precision—exactly the kind of task where traditional parallel grippers fall short. It’s another example of how our tools help bring real intelligence to robotic hands.

These moments show what’s possible when hardware and intelligence align.

NVIDIA Robotics

Amazon: Fulfillment that doesn’t miss a beat

Over at Amazon, robots work in high-speed, high-variability environments. And in their recent footage, you can see our Adaptive Grippers handling packages of various shapes and sizes.

Why is that important? Because no two packages are exactly the same. And no two shifts go exactly as planned. That’s where adaptability is mission critical.

Amazon

What this means for manufacturers like you

If Robotiq Adaptive Grippers are solving challenges for some of the most advanced robotic teams in the world, they can solve yours, too.

Whether you’re picking irregular parts, stacking delicate goods, or automating tough-to-staff jobs, these grippers are built to keep up.

Ready to see how adaptive gripping fits your factory?

 👉 Explore Robotiq’s Adaptive Grippers

Leave a comment

Related posts

Hand-E Now Reaches 100 mm Without Giving Up an Ounce of Precision

If you've been using Hand-E Adaptive Gripper on your production line, you already know why it's earned its reputation: a...

Robotiq Team
By Robotiq Team - July 16, 2026
How Sennheiser increased PCB testing by 33% with a Robotiq 2F-85 gripper

At Sennheiser Manufacturing USA in Albuquerque, precision is non-negotiable.

Every week, the facility assembles 30,000 printed...

Linnea Bruce
By Linnea Bruce - February 11, 2026
Robotiq brings the sense of touch to Physical AI

Physical AI has reached a critical point. Robots can see, plan, and decide better than ever—but manipulation in the real world...

Jennifer Kwiatkowski
By Jennifer Kwiatkowski - January 27, 2026