Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

Top 5 Applications for Robotic Electric Grippers

Mathieu Bélanger-Barrette
by Mathieu Bélanger-Barrette. Last updated on May 05, 2016 5:10 PM
Posted on Oct 14, 2014 8:28 PM. 3 min read time

Electric servo grippers offer a different set of functionality than pneumatic grippers. They trade speed and force for flexibility. In fact having specifications such as programmable; stroke, force and speed can make your applications a lot easier. To figure out for which applications is this useful, read on.

1. Grippers for Assembly

For assembly tasks an electric gripper can be really useful. In fact, most assembly tasks are done at a single spot in the production line. This means the gripper that is positioned there must be flexible and be able to grasp different parts. There is absolutely no time for tool changing and this is why a flexible electric gripper should be used. 

Also, grippers such as our 3-Finger Adaptive Gripper that have a programmable stroke can reduce the cycle time of the robot considerably. Especially since if you can set the stroke, the gripper doesn't need to run through its whole stroke before closing back on the object. The gripper can be set a little wider than the part and this can reduce the cycle time of the robot by reducing the gripper's motion. 

Another interesting aspect of the electric gripper is that it can have embedded sensing. This means you can have direct feedback as to whether or not the part has been grasped by the gripper. This can determine the difference between a productive assembly and a badly integrated assembly. 

2. Grippers for Machine Tending

machine tending gripperThe advantage of using an electric gripper in machine tending applications is that some grippers can handle a lot of different shapes. In fact often the shape of the part will change from before and after the machining operation. This is why you should have a gripper that can grasp both the raw part and the finished part. Otherwise you might be stuck using a tool changer and this can be complicated as well as time consuming. 

Another aspect that is often overlooked is your environment. In machining operations, there could be a lot of fluids involved. Since this can effect the functionality of your robot gripper, you have to choose a tool that can work well under your conditions. Irregardless of the type of gripper you choose, the IP rating should be known to make sure your gripper can handle your working environment. 

3. Grippers for Clean Rooms

Laboratories or metrology rooms might require clean air environments. By using pneumatic grippers, the air can be contaminated. Some grippers are specifically clean room rated and are designed to be installed in these kinds of rooms. A good alternative to the pneumatic gripper might be an electric on-off gripper. This kind of gripper has the same functionality without the disadvantage of air contamination. 

4. Grippers for Lab Automation

In the same way grippers that are used in laboratories might have to handle fragile parts such as tubes and trays. This means that the gripper probably requires programmable force, which can be done with an electric gripper. In fact, force is just a setting that can be changed in the gripper program to select the gripper grasping force which can be slight or firm depending on the part. In the case where the lab is using a pneumatic gripper, the force has to be set by adjusting the air pressure. However, if the pressure is not constant throughout the actionable time, then force could be higher or lower than necessary which could cause problems for the application.

5. Grippers for Mobile Robots

mobile robot gripperPneumatic grippers always have to be fed by their air lines which makes it pretty hard to drive around with a hose as a tether. Electric grippers can run on batteries. Even if the electric grippers are more useful than a pneumatic gripper with certain kinds of applications, the Adaptive Grippers are even more efficient. In fact, since the Robotiq Grippers are equipped with self-locking fingers, there is no need to power the gripper while the part is grasped. This means, the gripper can be powered for its movement and then lock itself on the part and doesn't require any further energy input until it deposits the part. This can be a good choice for saving valuable energy. 

For more in-depth information on the advantages of electric servo grippers take a look at this ebook.

How to choose the right robotic gripper for your application?  Learn more here

Leave a comment

Mathieu Bélanger-Barrette
Mathieu is a production engineer at Robotiq, where he constantly strives to optimize the production line for Robotiq Grippers. He enjoys discovering new robotic applications and sharing what he learns on Robotiq's blog.
Connect with the writer:
http://robotiq.com

Related posts

How to Use Lean Robotics to Automate Your CNC Machine

CNC machines are amazing tools for creating high-quality parts and products quickly. Some machines are very sophisticated with...

Alex Owen-Hill
By Alex Owen-Hill - November 29, 2022
My 8 Takeaways from Automate 2022

Three years ago, I was given by our friends at A3 a cool looking “Automate - Detroit 2021” t-shirt. Just like the caps they...

Samuel Bouchard
By Samuel Bouchard - June 10, 2022
What's New In Robotics?  17.01.2020

Good morning. In this week's news mix: Universal Robots launches cobot leasing program, Bossa Nova's massive Walmart deal and...

Emmet Cole
By Emmet Cole - January 17, 2020