Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

Robotiq Updates FT 300 Sensitivity For High Precision Tasks With Universal Robots

David Maltais
by David Maltais. Last updated on Nov 13, 2017 3:02 PM
Posted on Nov 13, 2017 7:00 AM. 2 min read time

Robotiq launches a 10 times more sensitive version of its FT 300 Force Torque Sensor. With plug and play integration on all Universal Robots, the FT 300 performs high precision force control tasks such as finishing applications, product testing, assembly and precise part insertion.

It comes with an updated free URCap software to get the most out of every application. It enables the FT 300 to feed data into Universal Robots Force mode (Available with Universal Robots CB3.1 controller only). This new feature allows the user to perform precise force-insertion assembly and many finishing applications where force control with high sensitivity  is required.

 

Plug + Play Calibration Procedure

The URCap also includes a new calibration routine. Robotiq integrated a step-by-step calibration procedure which guides the user through the process that takes less than 2 minutes. A new dashboard also provides all 6-axis real-time force and moment readings. Moreover, pre-built programming functions are now embedded in the URCap for intuitive programming.

 


Plug + Play calibration procedure

Many free Skills were also developed to accelerate robot programming of specific force control tasks. Every Universal Robots user now has access to the following ready-to-use, downloadable robotic programs:

 

 

Demo: Search for X,Y,Z with FT 300

Path recording remains an important feature of the FT 300. We've improved speed consistency for a more precise result which will result in a greater quality index.

 

 Demo: FT 300 path recording

For more info, take a look at the FT 300 FAQ.

Get a quote for the FT 300

Leave a comment

David Maltais
Written by David Maltais
David is a PR specialist at Robotiq, where he focuses on sharing Robotiq's voice worldwide. David brings several years' experience as a journalist to his work. He enjoys interacting with partners and influencers in the automation and manufacturing industries.
Connect with the writer:

Related posts

Pioneering Cobot Force Control: Louis Bergeron’s Story

Until recently, programming force-sensitive tasks on any kind of robot was a job for experts. And then someone made it simpler....

David Maltais
By David Maltais - November 6, 2019
How the RUC 2018 Changed the World of Cobots

It's hasn't been a month since the Robotiq User Conference 2018 ended and we at Robotiq already feel this event's major...

David Maltais
By David Maltais - September 26, 2018
Robotiq Makes Force Control Easy with Force Copilot

Robotiq is launching Force Copilot, an intuitive software to operate Universal Robots e-Series’ embedded force torque sensor....

David Maltais
By David Maltais - September 5, 2018