Subscribe

Latest Blog Post

Case Study: Universal Robots in Volkswagen Facilities

Catherine Bernier
by Catherine Bernier. Last updated on Dec 19, 2024
Posted on Oct 29, 2013 in Case Study
3 min read time

UR5-Universal-robots-volkswagen-collaborative robotsThe car manufacturer, Volkswagen, is renown to be an innovative company. The manufacturer proves it again, not by its products, but by its production methods. It decided to install a collaborative robot from Universal Robots, UR5, on its production line.

The company now sends an important message to industry: this is a new era for robotics. The time where robots were working on their own in safety cages is about to end. The new technologies in robotics allow for human-robot collaboration.

UR5 enters the automotive industry

The car manufacturer decided to work with the Danish robot manufacturer, Universal Robots and Faude Automatisierungstechnik, the distributor of UR5 in Germany, to equip its motors manufacturing plant which is situated in Salzgitter, Lower Saxony. The implementation lasted two years. The factory is spread over 2.8M square meters and builds 7,000 diesel and gas cars per day. There are 6,000 employees and, now, a UR5.

The UR5 is the smallest robot from Universal Robots and weighs about 18 kg. It is a six-axis arm that can also detect collisions by monitoring the current used in its joints. If a collision occurs, the robot will automatically stop to avoid any injuries or damage. Here is a video presenting this collaborative robot:


For more information about this robot, you can also take a look at the article: Collaborative Robots Series: Universal Robots

By using these new types of industrial robots, the company wants to automate monotonous and repetitive jobs to preserve its employees. The task of the robot will be to slide glow plugs into cylinder heads of motors. To do so, the robot will have to lift a 5 kg part, which is not possible with some other collaborative robots.

Another reason why the company chose Universal Robots is that they are the only robots to respect the ISO/TS 15066  standard, which allows the robot to work without a safety cage around it. This standard is not yet published but it will specify the limits of force and speed that will not harm a human in a collaborative task.

Jürgen Häfner a project manager at the plant explained why they introduced the UR5 to their production line:

“We would like to prevent long-term burdens on our employees in all areas of our company with an ergonomic workplace layout. By using robots without guards, they can work hand-in-hand together with the robots. In this way, the robot becomes a production assistant in manufacture and as such can release staff from ergonomically unfavorable work.”

However, working around collaborative robots is not risk-free. The programming and the movements of the robot should always be under surveillance. Moreover, the environment of the collaborative zone is also important to consider for safety.

Universal Robots' Success

Universal Robots already had important clients such as packaging, tobacco and car manufacturers (BMW). Yet, it has enlarged its place in the car industry, which before was reserved for big robotics manufacturers such as KUKA.  Universal Robots was, at first, considered by small and medium companies, but, now, it has made its way into the big league. Who knows what’s next?

Compare 19 collaborative Robots here >>

Leave a comment

Related posts

Small Team, Big Output: The Wine Bottler Bulles Création Automates Its End-of-Line with Robotiq Cobot Palletizing

In the heart of Provence, a small French bottling company is proving that automation isn't just for large manufacturers. Bulles...

Amanda Lee
By Amanda Lee - July 9, 2026
How an Italian Flour Producer Automated End-of-Line Palletizing in 5 Days

Manual palletizing is one of the most common, and most overlooked, inefficiencies in food manufacturing. It happens at the end...

Amanda Lee
By Amanda Lee - June 30, 2026
How SEL Eliminated Ergonomic Injuries and Automated 1.4 Million Screws a Year with Robotiq

What does it look like when a single cobot workcell solves a real problem, earns full ROI in under a year, and quietly grows...

Amanda Lee
By Amanda Lee - June 18, 2026