Subscribe

Latest Blog Post

How to Install a Robotic Gripper in 5 Easy Steps

Catherine Bernier
by Catherine Bernier. Last updated on Dec 19, 2024
Posted on Sep 12, 2013 in Robot Grippers
3 min read time

Robotiq’s 2-Finger Adaptive Robot Grippers are products that offer great value due to their adaptability and their other features such as grip detection, speed and position control. Moreover, they are simple to use, compatible with other industrial robots and their installation can be done in only 5 easy steps. These steps can be applied to the 2-Finger Adaptive Robot Gripper - 85 (for 85mm stroke) and the 2-Finger Adaptive Robot Gripper - 200 (for 200mm stroke).

First of all, here are the principal components you should received with your Adaptive Gripper:

  • Adaptive Gripper

  • Robotiq Device Cable

  • Controller

  • Mechanical Coupling

  • Wrist Adapter Plate (used only for some robot models)

 

Installation steps

robot-gripper-end-effector-universal-robots

Step 1. Installing Adapter Plate and/or Mechanical Coupling

Without Wrist Adapter Plate - Screw the Mechanical Coupling to your robot arm 

With Wrist Adapter Plate - Screw the Wrist Adapter Plate to your robot arm 

Then, screw the Mechanical Coupling to the Wrist Adapter Plate with the supplied screws and pins.

Step 2. Installing the Robot Gripper on the Mechanical Coupling

Attach the Robot Gripper to the Mechanical Coupling with the supplied screws or pins according to Gripper model.

Step 3. Connecting the Controllers Together

According to your communication protocol, use your Communication Cable to connect your communication master device to the controller.

controller-end-effector-gripper-2-finger-robotiq

Step 4. Connecting the Robot Gripper

Use the Robotiq Device Cable to connect the Gripper to its controller.

robotiq-2-finger-gripper-end-effector

Step 5. Turn On the End Effector!

Turn on your Gripper by connecting the power supply to the controller.

robotiq-gripper-2-finger-end effector

Now, you are ready to use your Robotiq’s 2-Finger Adaptive Gripper. For more information on Robotiq's products and requirements, take a look at our Product List. Or for a turnkey solution contact one of our distributors.

GET THE EBOOK: Electric Robot Gripper Advantages

Leave a comment

Related posts

How to choose the right standard gripper for your cobot projects

In robotics integration, every hour saved means a more profitable project. Yet one of the biggest time drains integrators face...

Michelle Vallée
By Michelle Vallée - November 5, 2025
Tech giants choose Robotiq

When the biggest names in tech choose a tool, the industry takes notice.Recently, Robotiq Adaptive Grippers have been spotted...

Linnea Bruce
By Linnea Bruce - June 3, 2025
Meet PowerPick Multi: The gripper built for flexible palletizing

If your production line handles a wide variety of box sizes, you know the frustration—constant gripper changeovers, manual...

Michel Beauchemin
By Michel Beauchemin - March 31, 2025