Subscribe

Latest Blog Post

DLR & KUKA: Grasp Planning & Control with the 3-Finger Robot Gripper

Catherine Bernier
by Catherine Bernier. Last updated on Feb 27, 2025
Posted on Sep 04, 2013 in Robot Grippers
3 min read time

Many companies are interested by the adaptability of Robotiq’s Grippers. They want to experiment with it, and integrate it into their own product. Like the German Aerospace Center, DLR, which is working with KUKA to use the 3-Finger Adaptive Gripper as an end effector for the KUKA LWR arm to integrate grasp planning and control. 

Partnership

DLR-Robotics-end-effector-grasping-control-gripperThe collaborative robot was first developed by the German Aerospace Center (DLR). The Light-Weight Robot (LWR) was originally designed to be used in space. However, with a technology transfer agreement, KUKA was allowed to use this technology and commercialize it for industrial purposes - read more on these new types of industrial robots here. Even if the LWR is now known as KUKA’s product, the DLR still works on the robot in collaboration with the company and different integrations have been made with Robotiq's product.

About their work

The control framework developed by KUKA for the LWR enables great integration with Robotiq’s 3-Finger Adaptive Robot Gripper through a plugin. To complement the control framework of the LWR and our robotic hand, DLR uses a grasp planner based on the openrave simulation environment (http://openrave.org/).

kuka,DLR, LWR, 3-Finger Adaptive Gripper, end effector

First, a CAD model of the object is needed, then the geometrical shape of the object is analyzed. Based on the curvature and geometrical features, good locations are selected for potential grasping. Different grasp strategies can be implemented to allow the simulation to plan all the operating modes for the Robot Gripper such as Basic, Pinch, Wide or Scissor modes. With the simulation software, sequential closing of the fingers around the object allows for a simulation of the adaptability of the end effector. Then, when all the fingers are closed, the contact points are obtained and the quality of the grasp is evaluated. This method creates a grasp database for the known CAD model.

The same procedure is used for meshes of objects acquired from a vision system. However, the results obtained by a machine vision system can produce non-watertight meshes, but a good grasp can still be selected by avoiding regions where there is no information available.

To complete the simulation and prove that the grasp is a good one, a dynamic simulation using Bullet, as a physics engine, can produce real environmental effects such as gravity, friction forces and control strategies. This last step evaluates the robustness of the grip before it is tried with a real industrial robot.

kuka,DLR, LWR, 3-Finger Adaptive Gripper, end effector

These developments will help with further integration of Robotiq’s 3-Finger Robot Gripper and the KUKA LWR. This will also give some sort of intelligence to the Gripper, which will increase its adaptability, even though it is already one of the best.

GET THE EBOOK: Electric Robot Gripper Advantages

Leave a comment

Related posts

Robotiq brings the sense of touch to Physical AI

Physical AI has reached a critical point. Robots can see, plan, and decide better than ever—but manipulation in the real world...

Jennifer Kwiatkowski
By Jennifer Kwiatkowski - January 27, 2026
How to choose the right standard gripper for your cobot projects

In robotics integration, every hour saved means a more profitable project. Yet one of the biggest time drains integrators face...

Michelle Vallée
By Michelle Vallée - November 5, 2025
Tech giants choose Robotiq

When the biggest names in tech choose a tool, the industry takes notice.Recently, Robotiq Adaptive Grippers have been spotted...

Linnea Bruce
By Linnea Bruce - June 3, 2025