Subscribe

Latest Blog Post

Two-arm teleoperation robot with Kinect and electric grippers

Guillaume Robert
by Guillaume Robert. Last updated on Feb 27, 2025
Posted on Mar 19, 2013 in Robot Grippers
2 min read time

Maybe some of you have seen the following video from the guys at Rensselaer Polytechnic Institute (RPI) where a robot replicates the movements of somebody by using Kinect. It was very interesting to see how a Kinect could perform on an industrial robot.





Today, guys from this robotics research lab are going a step further by integrating a Kinect, electric grippers, force/torque sensors and Firewire cameras to do teleoperation through motion detection. The robot uses vision and Alvar tags to align with the surfaces of the box, then applies squeeze control (using position accommodation) for a secure grasp. The user stands in front of the Kinect (with simulation and Kinect skeletal command shown) to provide motion input to the box. The robot autonomously applies the required force to prevent the box from falling.




Robot raconteur kinect RPI web

The key of this integration is the Robot Raconteur (RR). Robot Raconteur is an open-source project intended to provide a solution to distributed control and component interfaces. It is precisely designed for the scenario of an engineer wanting to control a component from a high level language (refer to this blog post to learn more about Robot Raconteur). So this team of researchers has built a RR service for the Motoman High Speed Controller to handle its peripherals. Here is the overall architecture:

Robot raconteur RPI web

Using Kinect frees users from all the constraints related to mechanical interfaces, such as a joystick, keyboard, etc. It is much more natural and intuitive that way.

Laws for control have also been implemented to make sure the box doesn't slip or fall. The arms "squeeze" the box with 10N force towards each other (the other degrees of freedom are under position control). Since the robot position is the only command, the robot's position accommodation control can be used to emulate a generalized damper (essentially integral force feedback).  The robot motion is also limited to avoid excessive motion induced force from causing the robot to lose its grip.

 

GET THE EBOOK: Electric Robot Gripper Advantages

Leave a comment

Related posts

Hand-E Now Reaches 100 mm Without Giving Up an Ounce of Precision

If you've been using Hand-E Adaptive Gripper on your production line, you already know why it's earned its reputation: a...

Robotiq Team
By Robotiq Team - July 16, 2026
How Sennheiser increased PCB testing by 33% with a Robotiq 2F-85 gripper

At Sennheiser Manufacturing USA in Albuquerque, precision is non-negotiable.

Every week, the facility assembles 30,000 printed...

Linnea Bruce
By Linnea Bruce - February 11, 2026
Robotiq brings the sense of touch to Physical AI

Physical AI has reached a critical point. Robots can see, plan, and decide better than ever—but manipulation in the real world...

Jennifer Kwiatkowski
By Jennifer Kwiatkowski - January 27, 2026