Subscribe

Latest Blog Post

Adaptive Gripper Teaching on ABB Touch Screen Pendant

Samuel Bouchard
by Samuel Bouchard. Last updated on Dec 12, 2024
Posted on Jul 18, 2011 in Robot Grippers
1 min read time

The Robotiq Adptive Gripper was recently implemented on an ABB robot using an ABB touch screen teach pendant. This project utilizes an ABB robot for a machine tending application with a Robotiq Gripper as the end-of-arm-tooling. Like any integration project, one of the first steps is programming the robot and its end-of-arm. A custom GUI (Graphical User Interface) on the touch screen pendant was created to simplify the usage of the teach pendant as demonstrated in this video:

The GUI has three main screens:

  • Control: open & close commands, grip modes

  • Satus: position of each finger

  • Define: speed and force

The GUI also has an integrated acquisition interface used to monitor the current in each servo of the Adaptive Gripper. The architecture consists of using an ABB robot (IRB 120M2004) with an IRC5 Compact Controller and its touch screen pendant.

The main advantages of using this custom GUI are to:

  • Simplify and reduce the total teaching time required for the robot

  • Provide easy visual and portable control

  • Have a tool dedicated to the Adaptive Gripper

  • Use the GUI with any ABB robot with an IRC5 controller

The development of the touch screen GUI was done at the CoRo (Command and Robotics) Laboratory of Montreal by graduate Yanick Noiseux, under the supervision of Vincent Duchaine, Scientific Advisor at Robotiq and Professor at ETS.

Get the eBook on: Robot Grippers for Collaborative Robots

Leave a comment

Related posts

Hand-E Now Reaches 100 mm Without Giving Up an Ounce of Precision

If you've been using Hand-E Adaptive Gripper on your production line, you already know why it's earned its reputation: a...

Robotiq Team
By Robotiq Team - July 16, 2026
How Sennheiser increased PCB testing by 33% with a Robotiq 2F-85 gripper

At Sennheiser Manufacturing USA in Albuquerque, precision is non-negotiable.

Every week, the facility assembles 30,000 printed...

Linnea Bruce
By Linnea Bruce - February 11, 2026
Robotiq brings the sense of touch to Physical AI

Physical AI has reached a critical point. Robots can see, plan, and decide better than ever—but manipulation in the real world...

Jennifer Kwiatkowski
By Jennifer Kwiatkowski - January 27, 2026