Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

10 Solutions to Improve Robot Vision With Shiny Objects

Alex Owen-Hill
by Alex Owen-Hill. Last updated on Mar 07, 2019 4:30 PM
Posted on Mar 07, 2019 11:02 AM. 6 min read time

Lights, camera, … and then reflections on the surface of your shiny objects! Suddenly your flawless robot vision setup can't detect objects. How do you deal with these annoying lighting problems? Here are ten great solutions.

The Robotiq Wrist Camera URCap version 1.7 is now the fastest and most intuitive vision system for Universal Robots.

Shiny objects are possibly the most challenging objects for a robot vision system. All it takes is one annoying reflection on the surface of the material and the reliability of the entire robot's task can be compromised.

Robot vision (and the more general "computer vision") is all about lighting. Whatever type of sensor you are using, the lighting will have a huge effect on whether or not it will be possible to detect the objects. Pick the wrong type of light and you could end up not being able to detect anything at all.

This is why shiny materials can be such trouble. The lighting you choose can completely change the appearance of the objects. This whitepaper from Microscan shows how a shiny ball bearing looks entirely different under 7 different lighting conditions. As Robotiq's Catherine Bernier explains, light reflections are seen by the robot's vision system as "features" (i.e. things that should be detected) but they aren't real physical features so they confuse the whole detection process.

How can we overcome these challenges and improve the detection of shiny objects?

Thankfully, there are some great solutions out there. Here are 10 solutions to improve robot vision with shiny objects.

wrist-camera-urcap-update-cta

1. Use a backlight

A backlight is one which sits underneath the object. We've used them before in our trade fair demos as they are a good way to control the light when the ambient lighting is unpredictable. They provide the vision sensor with a very clear outline of the object, which will show up as dark in the image.

Backlights are particularly useful with shiny objects because the light is coming from behind the object. This reduces chance of reflections on the object's surface.

2. Use infra-red lighting

Not all frequencies of light will interact with a surface in the same way. For example, ultraviolet (UV) light has a short wavelength which means that it will reflect strongly off the material's surface. Infra-red (IR) light, on the other hand, has a long wavelength and so will reflect less strongly. With some materials, it's even possible to "look through" the material with IR light. It is for this reason that IR light is often used for inspection applications.

Robotiq-wrist-cameraAdding a camera to your cobot is key to pick objects that lie in unstructured environments.

3. Change the light color

Of course, you don't need to change the type of light completely. Sometimes you can reduce the effects of light reflections by simply changing the color of the lighting. For example, visible-spectrum red light will interact less strongly with shiny surfaces than white light. An easy way to change lighting color is to cover the light with a colored "gel" (a thin, transparent film).

Changing the light color can also improve detection in other ways. For example, if your robot vision system uses monochrome images for detection, as many systems do, adding a blue light will make blue features lighter in the monochrome image and orange features darker. This effect happens because orange is the opposite color to blue on a color-wheel.

4. Use polarized light

Normal white light contains light waves which are oriented in many different planes. Polarization is a process by which only light waves in one plane are allowed to pass through a polarizing filter.

Polarized light is often used in computer vision applications as shining a polarized light onto the shiny surface can reduce the reflections. However, polarized light is not always the best solution. You have to precisely position the polarized light or the reflections can get much worse.

5. Change the flash

If your vision system uses strobed lighting, this can have an effect on the reflections from shiny objects. Sometimes flashed light can reduce the reflections by "overwhelming" the glare caused by ambient lighting. Other times, the flash can make the reflections worse.

The solution is to test out your own setup and see whether changing the properties of the flash solves your problem.

6. Add ambient lighting

Often, a reflection on the surface of a shiny object  is caused by a single light source — e.g. a strip-light in the ceiling, a window, etc. It can seem a strange idea to add more light sources in an attempt to reduce the problem, but this is actually a good solution.

As with adding a flash, additional ambient lighting can "overwhelm" the reflections from individual light sources. Of course, you need to make sure that the light that you add doesn't create more reflections.

7. Diffuse the existing light

Imagine someone shines a torch in your eye. It's hard to look at the bright light, right? Now imagine a bright, grey sky on a very cloudy day. Even though the sky is bright, it's easier to look at than the torch, isn't it?

This is an example of the difference between a hard lighting source (the torch) and diffuse/soft lighting source (the overcast sky). The worst reflections on shiny objects are caused by harsh, single point light sources. By diffusing this light, you can drastically reduce the reflections. One common way to diffuse light is to add a diffuse dome.

8. Use advanced sensors

Robot users sometimes think that more advanced (and costly) sensors will solve their problems. For dealing with shiny objects, the assumption is often that 3D laser scanners and 3D vision will not have the same problems as 2D vision.

However, although advanced sensors are necessary in some cases, they aren't immune from the problems caused by shiny objects. Researchers from Huazhong University of Science and Technology explain that even 3D laser scanners are affected by spurious reflections — they had to develop an entire new algorithmic solution to overcome these issues. Sometimes, more advanced technology just means more complex problems!

9. Reduce reflections when teaching

One of the real secrets to improving vision detection of all objects — not just shiny ones — is to make sure that your teaching phase is good. The detection phase can be quite robust to lighting changes as long as the vision system has a good model (aka template) of the object it needs to detect.

To ensure your system has a good template of your object, you should reduce reflections to a minimum when you are teaching the robot vision system. You may find that the system is able to detect the objects better even in the presence of reflections.

10. Use the secret unusual trick

How do you improve the teaching phase? One way is to use our favorite "secret trick" for creating a flawless object template. You can learn about this trick in our article An Unusual Trick That Improves Robot Vision Teaching

 New Call-to-action

What lighting problems have you encountered with robot vision? Tell us in the comments below or join the discussion on LinkedIn, Twitter, Facebook or the DoF professional robotics community.

Leave a comment

Alex Owen-Hill
Written by Alex Owen-Hill
Alex Owen-Hill is a freelance writer and public speaker who blogs about a large range of topics, including science, presentation skills at CreateClarifyArticulate.com, storytelling and (of course) robotics. He completed a PhD in Telerobotics from Universidad Politecnica de Madrid as part of the PURESAFE project, in collaboration with CERN. As a recovering academic, he maintains a firm foot in the robotics world by blogging about industrial robotics.
Connect with the writer:
http://alexowenhill.co.uk/

Related posts

How to Use Robot Vision With Big or Awkward Objects

What if your objects are too big or awkward to teach to a robot vision system?

Is robot vision only suitable for small, regular...

Alex Owen-Hill
By Alex Owen-Hill - August 21, 2020
Do Robots Need 3D Vision? One Insect Says No

To use 3D or not to use 3D? That's the question. Which properties are the most important for robot vision? The natural world...

Alex Owen-Hill
By Alex Owen-Hill - March 28, 2019
Bin Picking the Easy Way vs the Hard Way With Robot Vision

It's one of the trickiest robotic tasks in the world. But, you don't need a complex solution to solve it. There's a hard way to...

Alex Owen-Hill
By Alex Owen-Hill - March 21, 2019