Subscribe

Latest Blog Post

Why Physical AI isn't scaling yet, and what's holding it back

Linnea Bruce
by Linnea Bruce. Last updated on Apr 21, 2026
Posted on Apr 21, 2026 in Physical AI
6 min read time

Physical AI is advancing quickly.

AI models can now recognize objects, plan actions, and adapt to new tasks. But despite this progress, most systems still struggle to scale in real-world environments.

Two core challenges explain why:

  • Limited real-world dexterity
  • High cost and complexity of deployment

Until these are solved, Physical AI will remain difficult to scale beyond controlled applications.

What is Physical AI?

 

Physical AI refers to AI systems that can perceive, decide, and act in the real world through physical interaction.

Unlike digital AI, Physical AI must handle:

  • Uncertainty in the environment
  • Variability in objects and materials
  • Real-time feedback during physical contact

To work reliably, Physical AI systems must combine:

  • Perception (vision, sensors)
  • Decision-making (AI models)
  • Action (robot motion)
  • Adaptation (force and tactile feedback)

Why isn’t Physical AI scaling today?

Physical AI is not scaling because most systems:

  • Struggle to handle real-world variability
  • Require complex and costly integration
  • Depend on precise conditions to function
  • Lack real-time adaptability during interaction

In short, they work in demos, but not consistently in production.

The gap between Physical AI demos and real-world deployment

In controlled environments, everything is predictable.

In real-world applications, variability is constant:

  • Parts are slightly different
  • Lighting changes
  • Objects shift during handling
  • Contact forces are uncertain

This gap between controlled conditions and real environments is where most Physical AI systems fail.

Bottleneck #1: Real-world dexterity in robotics

What is robotic dexterity?

Robotic dexterity is the ability to manipulate objects reliably despite variation in shape, position, and physical properties.

This includes:

  • Picking different objects
  • Handling uncertain orientations
  • Adjusting grip during motion
  • Managing friction and deformation

Why is dexterity hard to achieve?

Most systems rely on:

  • Precise positioning
  • Detailed planning
  • Limited feedback during contact

This makes them fragile when conditions change.

Common (but limiting) approach: more complexity

To improve dexterity, some systems add:

  • Multi-fingered robotic hands
  • Advanced grasp planning algorithms
  • High-dimensional control

The problem:
More complexity often leads to:

  • Higher cost
  • Longer deployment time
  • Lower robustness in production

A better approach: Simplifying robotic manipulation

Instead of increasing complexity, scalable systems simplify interaction.

Adaptive grippers and compliant designs help by:

  • Conforming to object shapes
  • Absorbing positioning errors
  • Reducing reliance on precise planning

Key idea:
Shift complexity from software to hardware.

This improves reliability without increasing system burden.

Bottleneck #2: Scaling Physical AI across deployments

Even when a system works once, scaling it is difficult.

Why is scaling robotic systems hard?

Because every deployment introduces variation:

  • New product types
  • Different layouts
  • Changing lighting
  • Operator differences

If each setup requires reprogramming or expert tuning, scaling becomes too expensive.

What makes a Physical AI system scalable?

A scalable system is one that can be deployed repeatedly with minimal effort.

Key characteristics of scalable robotics systems:

  • Works across variation without major changes
  • Requires minimal expert intervention
  • Maintains consistent performance
  • Has predictable deployment time and cost

Why repeatability matters more than capability

A system that works once is not enough.

The real value comes from systems that:

  • Work consistently
  • Can be replicated across sites
  • Require little customization

Scalability = repeatability at a sustainable cost.

How to make Physical AI systems more scalable

To enable scaling, systems must be designed differently.

Best practices for scalable Physical AI:

  • Design for variability, not perfect conditions
  • Use sensing to adapt instead of pre-programming everything
  • Reduce system complexity wherever possible
  • Use hardware to absorb uncertainty

The goal is not to eliminate variability, but to handle it effectively.

The role of force and tactile sensing in Physical AI

Why is sensing critical for Physical AI?

Force and tactile sensing allow robots to:

  • Detect contact in real time
  • Adjust grip dynamically
  • Handle uncertainty without reprogramming

This enables systems to adapt during execution—not just before.

How sensing improves scalability

With proper feedback, robots can:

  • Generalize across different setups
  • Reduce dependency on precise inputs
  • Minimize manual adjustments

This is essential for scaling across applications.

From one successful robot cell to many

A scalable Physical AI solution is not defined by a single success.

It’s defined by how easily that success can be repeated.

If each deployment requires starting over, the system doesn’t scale.

The future of Physical AI: Simpler systems that scale

The next phase of Physical AI won’t be driven by more complex AI alone.

It will come from:

  • Simpler, more robust system design
  • Better integration of sensing and hardware
  • Reduced dependency on ideal conditions

The systems that scale will be the ones that:

  • Handle variability
  • Deploy quickly
  • Deliver consistent results

Closing thought: Physical AI must scale to deliver value

Physical AI has the potential to transform robotics.

But impact won’t come from isolated successes.

It will come from systems that scale across real-world environments.

From:
“What can this system do?”

To:
“Can this system scale?”

Because real impact comes from repeatable deployment rather than one-time performance.

Ready to make your robotics application scale?

If you're working on a robotics application and facing challenges with reliability, variability, or deployment at scale, you're not alone.

Talk to a Robotiq expert to explore practical ways to simplify your system, improve robustness, and move from a working concept to a scalable solution.

👉 Get in touch with our team to discuss your application

Leave a comment

Related posts

Robotiq Releases New 2F-85 Isaac Sim Asset on Newton

If you have put a Robotiq 2F-85 into an NVIDIA Isaac Sim scene and closed it on an object, you have probably seen the fingers...

Robotiq Team
By Robotiq Team - September 22, 2026
Robotiq Releases ROS 2 Packages for Adaptive Grippers

If you run a Robotiq gripper in the Robot Operating System (ROS) 2 workspace today, you are almost certainly running PickNik...

Robotiq Team
By Robotiq Team - August 26, 2026
Robotiq Releases an Open-Source C++ SDK for Adaptive Grippers

As physical AI moves from research into real applications, developers need a solid primitive that meets them where they work:...

Robotiq Team
By Robotiq Team - August 12, 2026