Subscribe

Latest Blog Post

AI can decide. But can it act? The missing layer in Physical AI

Louis-Alexis Demers
by Louis-Alexis Demers. Last updated on Apr 16, 2026
Posted on Apr 16, 2026 in Physical AI
5 min read time

Artificial intelligence has made impressive progress.

Models can classify images, generate text, and even plan complex sequences of actions. But when you take AI out of the digital world and place it into a factory, a warehouse, or any physical environment, something breaks.

The AI can decide.

But it can’t reliably act.

This is the gap that defines Physical AI—and it’s where most real-world robotics projects succeed or fail.

 

The gap between thinking and doing

Tactile Sensors Highlight-1

In simulation, everything is clean and predictable.

Objects are perfectly modeled. Lighting is ideal. Physics behaves exactly as expected.

In the real world, none of that is true.

  • Parts vary slightly from one batch to another
  • Surfaces reflect light differently throughout the day
  • Objects shift, slip, or deform during handling
  • Contact forces are uncertain

An AI system might correctly identify an object and decide how to pick it. But without the ability to adapt during the interaction, that decision often fails in execution.

This is why many AI-driven robotics demos look impressive—yet struggle when deployed on the factory floor.

 

Perception isn't enough

Most AI development in robotics has focused on vision.

And vision is important. It helps robots locate objects, understand scenes, and plan actions.

But vision alone doesn’t close the loop.

Humans don’t rely only on sight to manipulate objects. We use touch, force, and feedback continuously:

  • We adjust our grip when something starts slipping
  • We feel contact before applying force
  • We adapt instantly to small variations

Without this feedback, even simple tasks become unreliable.

The same is true for robots.

Physical AI requires a full loop: sense → decide → act → adapt

AgileRobots_web

To operate reliably in the real world, robots need more than intelligence. They need a closed-loop interaction system.

That loop looks like this:

  1. Sense – Vision, force, and tactile inputs
  2. Decide – AI models or control logic determine the action
  3. Act – The robot executes the motion
  4. Adapt – Real-time feedback adjusts the action during execution

Most current systems stop short of this loop.

They sense and decide, but don’t adapt effectively once contact begins.

That missing “adapt” step is where failures happen.


Why manipulation is still the hardest problem

Moving a robot arm from point A to point B is a solved problem.

Interacting with the real world is not.

Grasping, inserting, aligning, or handling objects introduces uncertainty that AI alone cannot resolve.

The challenge isn’t just planning the motion. It’s handling what happens during the motion:

  • Slight misalignment during insertion
  • Unexpected resistance when pushing a part
  • Object slipping during a pick
  • Variations in material stiffness or friction

Without feedback, the robot either fails or requires extremely tight control of the environment.

And tightly controlled environments don’t scale.


The role of hardware in making AI work

There’s a tendency to treat AI as the primary driver of progress.

But in Physical AI, hardware plays an equally critical role.

Adaptive grippers, force-torque sensors, and compliant mechanisms don’t just execute actions; they make those actions more robust.

They reduce the precision required from AI models by absorbing variability physically.

Instead of needing perfect perception and planning, the system can rely on:

  • Mechanical compliance
  • Force feedback
  • Simpler grasp strategies

This is what enables real-world reliability.

Not perfect AI, but systems designed to handle imperfection.

From demos to deployment

The difference between a demo and a deployed system often comes down to one question:

Can the robot recover from small errors on its own?

In many AI-driven demos, the answer is no.

Everything works because the environment is controlled.

In production, variability is constant. And systems that can’t adapt require:

  • Frequent human intervention
  • Complex reprogramming
  • Tight process constraints

That’s where projects stall.

Physical AI isn’t just about making robots smarter. It’s about making them more resilient to reality.

 

What this means for robotics teams 

If you’re building or deploying robotic systems, this shift has practical implications:

  • Don’t evaluate AI in isolation; evaluate the full interaction loop
  • Prioritize systems that can adapt during contact, not just before
  • Use hardware to simplify the problem whenever possible
  • Design for variability, not perfection

The goal isn’t to eliminate uncertainty.

It’s to handle it effectively.


Closing the gap

AI has reached a point where decision-making is no longer the main limitation.

Interaction is.

Physical AI is about closing that gap: connecting intelligence to the real world through sensing, action, and adaptation.

Because in robotics, the question isn’t just:

“Does it work?”

It’s:

“Does it still work when reality gets messy?”

Ready to take the next step?

If you're working on a robotics application and running into challenges with reliability, variability, or deployment at scale, you're not alone.

Talk to a Robotiq expert to explore practical ways to simplify your system, improve robustness, and move from a working concept to a scalable solution.

Leave a comment

Related posts

Robotiq Releases New 2F-85 Isaac Sim Asset on Newton

If you have put a Robotiq 2F-85 into an NVIDIA Isaac Sim scene and closed it on an object, you have probably seen the fingers...

Robotiq Team
By Robotiq Team - September 22, 2026
Robotiq Releases ROS 2 Packages for Adaptive Grippers

If you run a Robotiq gripper in the Robot Operating System (ROS) 2 workspace today, you are almost certainly running PickNik...

Robotiq Team
By Robotiq Team - August 26, 2026
Robotiq Releases an Open-Source C++ SDK for Adaptive Grippers

As physical AI moves from research into real applications, developers need a solid primitive that meets them where they work:...

Robotiq Team
By Robotiq Team - August 12, 2026