Subscribe

Latest Blog Post

Scaling Physical AI: Why grippers and sensors matter for real-world robotics

Marc Giguère
by Marc Giguère. Last updated on Apr 09, 2026
Posted on Apr 09, 2026 in Physical AI
6 min read time

Physical AI is evolving quickly.

From imitation learning to foundation models, robotics teams are making real progress toward systems that can adapt, generalize, and improve over time.

But there’s a gap.

Many of these systems work well in controlled environments… yet struggle when faced with the variability of real production.

If you’re a robotics OEM, product leader, or engineering team, you’ve likely felt this firsthand.

The challenge isn’t just building smarter robots.
It’s building robots that work reliably in the real world.

End-of-arm tooling is a key part of the equation.

 

The challenge in Physical AI: Real-world interaction

Tactile Sensors Highlight-1

Physical AI robotics relies on multiple sources of learning: real-world interaction, simulation, and multimodal data.

But when systems move into production, one challenge becomes especially clear: the real world is messy.

  • parts aren’t perfectly positioned
  • surfaces vary
  • objects slip, shift, or deform
  • vision systems introduce uncertainty

This is where many systems start to struggle.

Because even with strong models and simulation pipelines, performance in production depends on how well the robot can interact with its environment.

The quality of grasping, the ability to handle variation, and the consistency of execution all come down to what happens at the point of contact.

If your robot can’t reliably grasp, sense, and adapt, your AI won’t scale.

Why end-of-arm tooling matters in robotics AI

In traditional automation, a robotic gripper is selected for a single task.

In physical AI, that assumption no longer holds.

Robots are expected to:

  • handle variation
  • perform multiple tasks
  • learn from real-world feedback
  • improve over time

That means your end-of-arm tooling (grippers and sensors) needs to do more than just pick a part.

It needs to:

  • generate consistent, high-quality interaction data
  • handle uncertainty without failure
  • support both testing and scalable deployment
  • integrate into simulation and real-world workflows

This is why end-of-arm tooling is becoming a core part of the AI stack, not just a mechanical component.

Choosing the right robotic gripper for Physical AI 

There’s a lot of attention on highly dexterous robotic hands.

And while they show promise, today they are often:

  • fragile
  • complex to integrate
  • expensive to scale
  • difficult to maintain

The reality is that most industrial applications don’t need that level of complexity.

Many tasks can be solved with:

  • reliable pinch grasps
  • adaptive gripping
  • simple manipulation strategies

This is where adaptive robotic grippers stand out.

With built-in mechanical intelligence, they can:

  • perform both parallel and encompassing grasps
  • adapt to part variation automatically
  • introduce compliance during contact

All while remaining simple and durable.

For robotics OEMs and product teams, this means:

  • faster time to deployment
  • lower system complexity
  • reduced maintenance costs
  • better long-term reliability

And most importantly: a solution that scales with your applications.


How force-torque sensors improve robotic precision 

  • Even with the right gripper, vision alone isn’t enough.

    As soon as tasks involve contact like insertion, alignment, or assembly, robots need another layer of feedback.

    A force-torque sensor gives robots a sense of touch at the wrist.

    It enables them to:

    • detect contact
    • adjust in real time
    • compensate for variation
    • complete precision tasks reliably

    For engineering teams, this reduces dependence on perfect positioning.

    For business leaders, it expands what can be automated—without redesigning the entire environment.

    And in physical AI workflows, force sensing becomes a key input for learning and adaptation.

What tactile sensors unlock for robotic manipulation 

Force sensing is powerful.

But tactile sensors in robotics bring feedback even closer to the fingertips.

This is where robots start to understand not just that they picked something, but how they picked it.

Tactile sensing enables:

  • pressure distribution mapping
  • slip detection through vibration
  • fingertip orientation awareness

With this data, robots can:

  • detect bad grasps instantly
  • adjust grip dynamically
  • handle fragile or variable objects more effectively
  • improve learning-based manipulation

For AI/ML teams, this means richer, multimodal data.

For OEMs, it means unlocking applications that were previously too complex or unreliable.

From research to scalable robotics deployment 

The biggest shift happening now is this:

Physical AI is moving from research to real-world deployment.

But scaling requires more than a successful demo.

It requires systems that can:

  • run millions of cycles
  • handle variation consistently
  • maintain performance over time
  • operate in real production environments

This is where proven hardware matters.

Field-tested robotic grippers and force-torque sensors provide the reliability needed today—while tactile sensing opens the door to what’s next.

The winning approach is not choosing one or the other.

It’s combining:

  • proven, reliable hardware
  • learning-ready sensing technologies

What this means for robotics OEMs and engineering leaders 

If you’re building or scaling robotics systems, here’s what matters:

  • Durable hardware is crucial to get your system from research to scalable deployment
  • Your hardware is part of your AI system
  • Better sensing leads to better performance
  • Simpler, robust designs often outperform complex ones
  • Data quality starts at the point of contact

The companies that scale physical AI fastest won’t be the ones with the most complex robots.

They’ll be the ones with robots that work consistently, reliably, and at scale.

Ready to scale Physical AI in your applications? 

Before optimizing your models, start with what matters most:

Can your robot reliably grasp, sense, and adapt in the real world?

That’s where real performance begins.

👉 Download our Physical AI white paper to learn how leading robotics teams are scaling from research to deployment.
👉 Talk to a Robotiq expert to explore the right grippers and sensors for your application.

Giving Physical AI a hand-1

Leave a comment

Related posts

Robotiq Releases New 2F-85 Isaac Sim Asset on Newton

If you have put a Robotiq 2F-85 into an NVIDIA Isaac Sim scene and closed it on an object, you have probably seen the fingers...

Robotiq Team
By Robotiq Team - September 22, 2026
Robotiq Releases ROS 2 Packages for Adaptive Grippers

If you run a Robotiq gripper in the Robot Operating System (ROS) 2 workspace today, you are almost certainly running PickNik...

Robotiq Team
By Robotiq Team - August 26, 2026
Robotiq Releases an Open-Source C++ SDK for Adaptive Grippers

As physical AI moves from research into real applications, developers need a solid primitive that meets them where they work:...

Robotiq Team
By Robotiq Team - August 12, 2026