Subscribe

Latest Blog Post

Robots that feel: why touch is the next frontier in Physical AI

Jennifer Kwiatkowski
by Jennifer Kwiatkowski. Last updated on Feb 06, 2026
Posted on Feb 06, 2026 in Physical AI
5 min read time

Physical AI has moved past proof-of-concept. Large models, better simulation, and faster hardware have pushed embodied intelligence forward—but real-world manipulation is still the limiting factor.

Not perception.
Not planning.
Manipulation.

Robots can see the world with increasing clarity, yet still struggle to interact with it reliably. The reason is simple: vision-only systems don’t experience contact. And without contact, learning stalls.

Physical AI matters because it closes that gap. It connects sensing, decision-making, and action in the real world—where objects slip, deform, collide, and behave in ways simulation still cannot fully capture.

Touch is no longer optional. It’s the missing signal.

What physical AI actually changes

Physical-AI-title-01

Physical AI is not traditional automation with a neural network bolted on. It is a shift in how robots learn and operate.

Instead of executing predefined trajectories, Physical AI systems:

  • Perceive the world through different data - vision, tactile, proprioception and force

  • Adjust behavior dynamically during interaction

  • Learn from real-world outcomes rather than scripted success cases

This matters most at the moment of contact—when fingers meet an object, when force distributes unevenly, when slip begins.

Those milliseconds define whether a grasp succeeds, fails, or generates usable training data.

Without tactile feedback, robots guess. With it, they learn.

Physical AI vs traditional automation

Traditional automation was built for repeatability. Known objects. Known poses. Known forces.

That model breaks down when:

  • Objects vary in shape, stiffness, or surface
  • Contact dynamics are non-linear
  • The task space is large and underconstrained

To compensate, teams often add complexity upstream: tighter fixturing, constrained environments, or custom end-effectors designed for narrow tasks.

Physical AI flips that equation.

Instead of simplifying the world for the robot, it equips the robot to handle the world as it is.

That requires:

  • Real-time contact awareness
  • Continuous force feedback
  • The ability to recover from partial failure rather than reset

The result is not just higher task success. It’s systems that learn from every interaction (success or failure) and become more capable over time.

Why vision-only manipulation has hit a ceiling

Vision excels at pre-contact reasoning: object detection, pose estimation, scene understanding. But once contact occurs, vision plateaus.

Occlusion increases.
Lighting changes.
Micro-slips and contact are invisible.

This is where many manipulation pipelines fail—not because the model is wrong, but because it’s blind at the most critical moment.

Tactile sensing provides signals vision cannot:

  • Contact geometry
  • Force distribution
  • Slip onset
  • Object compliance

For Physical AI teams, this isn’t about incremental improvement. It’s about unlocking learning regimes that were previously unstable, data-starved, or too costly to scale.


Digital AI vs physical AI in robotics programs

Digital AI has already transformed robotics development:

  • Faster simulation
  • Better planning
  • Improved model training and evaluation

But digital AI operates one step removed from reality.

Physical AI is where models are stress-tested against physics, friction, noise, and uncertainty. It’s where sim-to-real gaps are exposed—and closed.

Digital AI helps decide what should happen.
Physical AI determines what actually happens.

Physical AI faces a challenge digital doesn’t: high quality real-world data.

Why tactile-enabled manipulation changes the economics

As fleets scale, new constraints emerge:

  • Cost per robot
  • Cost per datapoint
  • Reliability across hundreds of identical stations

Custom grippers and bespoke tactile solutions often become bottlenecks. They fragment systems, slow deployment, and divert engineering effort away from core AI work.

A fleet-ready manipulation system does the opposite:

  • Standardized hardware across stations
  • Increased uptime
  • Reduced maintenance costs and time
  • Known performance envelopes
  • Repeatable data characteristics

Adding tactile fingertips to proven industrial grippers shifts the trade-off. Teams gain access to rich contact data without absorbing the cost, fragility, and maintenance burden of fully custom hands.

Tactile Sensors Highlight-1

For humanoids, the benefit is immediate:

  • More stable grasps
  • Better slip recovery
  • Useful contact feedback without anthropomorphic complexity

For Physical AI labs, the impact compounds over time:

  • Higher data throughput per robot
  • More consistent learning signals
  • Faster iteration cycles

What this means for Physical AI teams

Physical AI is not about building the most human-like hand. It’s about building systems that can learn reliably in the real world.

Touch enables that learning.
Consistency enables scale.
Robust hardware enables both.

As Physical AI programs move from isolated demos to fleets, the question is no longer can this robot grasp an object?

It’s:

  • Can it do it thousands of times a day?
  • Can it generate consistent, usable data?
  • Can the system scale without collapsing under its own complexity?

That’s where tactile-enabled manipulation stops being a research feature—and becomes infrastructure.

Leave a comment

Related posts

Robotiq Releases New 2F-85 Isaac Sim Asset on Newton

If you have put a Robotiq 2F-85 into an NVIDIA Isaac Sim scene and closed it on an object, you have probably seen the fingers...

Robotiq Team
By Robotiq Team - September 22, 2026
Robotiq Releases ROS 2 Packages for Adaptive Grippers

If you run a Robotiq gripper in the Robot Operating System (ROS) 2 workspace today, you are almost certainly running PickNik...

Robotiq Team
By Robotiq Team - August 26, 2026
Robotiq Releases an Open-Source C++ SDK for Adaptive Grippers

As physical AI moves from research into real applications, developers need a solid primitive that meets them where they work:...

Robotiq Team
By Robotiq Team - August 12, 2026