Subscribe

Latest Blog Post

Robotiq Presents Hand-E, the First UR+ Gripper Ready for the e-SERIES

David Maltais
by David Maltais. Last updated on Feb 20, 2025
Posted on Jun 19, 2018 in Robot Grippers
2 min read time

We kept you in suspense, but the day has finally come! 

The latest product in Robotiq's line-up of Adaptive Grippers is Hand-E,  the first UR+ electric gripper ready for the new e-SERIES generation of Universal Robots.

Hand-E’s high accuracy and 50 mm parallel stroke make it perfect for precision assembly tasks, while its sealed design ensures reliability in the toughest manufacturing conditions.

How can we simplify collaborative robot applications? Well, after 10 years in the industry, we've come up with the perfect formula.

It starts with an easy-to-install gripper and the ability to create custom fingertips. Then, we add intuitive programming software combined with great precision, pinch force, and payload specifications. This brings us to Hand-E, the ultimate gripper for collaborative robots.

Meet Hand-E!

As our CTO Jean-Philippe Jobin explains,  “We wanted to create a product that fits any manufacturer’s needs and allows them to start production faster. Hand-E comes with a 3-fingertip kit so automation engineers can easily integrate the gripper in their application. Its compact and ergonomic shape makes collaborative robot hand-guiding safe and easy.”  

Along with the popular 2F-85 and 2F-140, Hand-E completes Robotiq’s product line of Adaptive Grippers, which all connect directly to the e-SERIES wrist. They all operate with the same intuitive programming software, which enables full control over the gripper’s position, force, and speed. A new grip check feature allows the robot to validate its grip with the part's dimensions before starting the cycle. 

A new feature: validate grip with the part's dimensions.

Hand-E also unlocks many industrial applications by integrating seamlessly with the Robotiq Wrist Camera and FT 300 Force Torque Sensor. 

Not sure which Robotiq Adaptive Gripper is best for your application? The following chart gives an overview of how each gripper complements the others.

Capture d’écran 2018-06-19 à 10.57.43

 

Get the full specifications

Leave a comment

Related posts

Hand-E Now Reaches 100 mm Without Giving Up an Ounce of Precision

If you've been using Hand-E Adaptive Gripper on your production line, you already know why it's earned its reputation: a...

Robotiq Team
By Robotiq Team - July 16, 2026
How Sennheiser increased PCB testing by 33% with a Robotiq 2F-85 gripper

At Sennheiser Manufacturing USA in Albuquerque, precision is non-negotiable.

Every week, the facility assembles 30,000 printed...

Linnea Bruce
By Linnea Bruce - February 11, 2026
Robotiq brings the sense of touch to Physical AI

Physical AI has reached a critical point. Robots can see, plan, and decide better than ever—but manipulation in the real world...

Jennifer Kwiatkowski
By Jennifer Kwiatkowski - January 27, 2026