Subscribe

Latest Blog Post

Physical AI: The DARPA Legacy & the Road Ahead — From Face-Plants to Foundation Models

Samuel Bouchard
by Samuel Bouchard. Last updated on Jul 28, 2026
Posted on Jul 28, 2026 in Physical AI
13 min read time

Part 1 of 2, Physical AI: The DARPA Legacy & the Road Ahead. What the DARPA Robotics Challenge Actually Built—and Why It Still Matters

In March 2011, a massive earthquake and tsunami triggered a nuclear disaster at the Fukushima Daiichi power plant in Japan. Radiation and structural damage made parts of the facility too dangerous for people to enter, yet the available robots could do little more than observe from a distance.

DARPA Robotics Challenge

Robots already existed for bomb disposal, reconnaissance and industrial automation. What they could not reliably do was enter a damaged building designed for humans, climb stairs, open doors, move debris, operate valves and use ordinary tools.

That failure helped motivate the U.S. Defense Advanced Research Projects Agency to launch the DARPA Robotics Challenge in April 2012. Its objective was not to build a fully autonomous humanoid. DARPA asked something more practical: could a human supervise a robot from a distance while the machine handled enough perception, balance and motion locally to operate through degraded or intermittent communications?

The competition culminated in the June 2015 Finals in Pomona, California. Twenty-three teams attempted eight tasks that included driving a vehicle, opening a door, turning a valve, cutting through a wall, traversing debris and climbing stairs. Robots had to carry their own power, operate without physical support and cope with intentionally unreliable communications. Only three teams completed all eight tasks.

The falls became internet entertainment. The deeper legacy was less visible.

The DRC forced robotics researchers to integrate locomotion, manipulation, perception, communications, human-machine interfaces, power systems and field repair into complete machines. It exposed the difference between a laboratory capability and an operational system. It also created a generation of researchers, software tools, components and companies that now form part of the industrial foundation of physical AI.

 

1. The First Lesson: There Was No Winning Body Plan

It is tempting to conclude that the DRC proved hybrid mobility was superior to pure bipedalism. The actual result was more interesting.

The three leading teams represented three very different engineering philosophies.

KAIST, the winner, used DRC-HUBO. The robot could walk on two legs but could also kneel and move on wheels mounted near its knees. Walking allowed it to negotiate stairs and irregular obstacles. Wheeled motion gave it a wider base, greater speed and more stability during portions of the course.

IHMC, which finished second, used Boston Dynamics’ Atlas—a conventional biped without wheels or tracks. IHMC’s achievement was demonstrating that a large humanoid could complete all eight tasks through a combination of sophisticated balance control, footstep planning, whole-body motion and an effective operator interface.

Tartan Rescue, which finished third, took the opposite approach. Carnegie Mellon’s CHIMP moved on tracks built into its four limbs and was designed to remain statically stable rather than continuously balance like a person. It also completed all eight tasks, in 55 minutes and 15 seconds.

The competition therefore did not identify one universally superior morphology. It demonstrated that reliability comes from matching the machine’s physical architecture to its task and controlling the resulting risks.

A biped can move through spaces built for humans. Wheels can make common surfaces faster and safer. Tracks and multiple contact points can reduce the consequences of a loss of balance. The right answer depends on terrain, speed, payload, fall tolerance and the cost of failure.

That remains true today. The question is not whether every robot should look human. It is which parts of the human form create economic value for a particular job.

 

2. The Manipulation Lesson: Dexterity Is Worthless Without Reliability

The DRC also served as a severe test of robotic hands.

A disaster-response robot has to grasp irregular objects, hold vibrating tools, manipulate controls built for human fingers and survive collisions or falls. These demands created a difficult trade-off.

Anthropomorphic hands offered greater theoretical dexterity, but they also introduced more actuators, joints, cables, sensors and possible failure points. Simpler grippers offered fewer grasp configurations but were easier to control, repair and protect.

The result was not the disappearance of dexterous hands. It was a stronger appreciation for underactuation, mechanical compliance and modularity.

Eight of the 25 qualifying teams for finals planned to use our three-finger adaptive gripper — a fact I still think about. MIT researchers later emphasized the qualities they valued during the competition: durability, underactuation and the ability to regulate fingertip force.

The iRobot i-HY hand, another prominent DRC end effector, was designed around a similar compromise: enough dexterity to perform useful tasks, but with underactuated mechanisms intended to be durable and relatively economical. Atlas teams were provided with hand options developed by iRobot and Sandia National Laboratories.

Mechanical compliance mattered because it reduced the precision demanded from software. When a finger could passively conform around a valve, handle or tool, the perception and control system did not need a perfect geometric model of every contact.

This remains an important principle for physical AI:

Intelligence does not have to live entirely in software. It can also be embedded in the geometry, compliance and mechanics of the machine.

Today’s dexterous hands are returning with better tactile sensors, actuators and learning methods. That does not invalidate the DRC lesson. It raises the bar. Additional dexterity must produce enough useful capability to justify its cost, fragility and control complexity.

 

3. The DRC Was a Shared-Autonomy Challenge

Descriptions of the DRC sometimes imply that the robots autonomously understood the environment and completed tasks on their own.

They did not.

DARPA intentionally reduced communications quality so operators could not continuously joystick every movement. But humans still played a central role. They interpreted sensor data, selected objects and goals, approved actions and intervened when plans failed.

The robots handled pieces of the problem locally: maintaining balance, generating footsteps, planning trajectories and controlling joints. The operator handled ambiguity, strategy and exception management.

IHMC called its approach coactive design: instead of treating the robot as either autonomous or teleoperated, the team designed the human, interface and robot as one operational system.

This may be the most relevant DRC lesson for current physical AI deployments.

The near-term alternative to full autonomy is not necessarily crude remote control. It is a graduated system in which:

  • the robot executes known skills autonomously;
  • a person gives goals or resolves ambiguous situations;
  • remote assistance handles exceptions;
  • the system records interventions as training data;
  • autonomy expands as recurring exceptions are learned.

That architecture now appears in warehouse robots, autonomous vehicles, delivery systems and emerging humanoid deployments. The operator gradually moves from controlling one robot to supervising a fleet.

 

4. What Was Still Missing in 2015

The DRC established that complex mobile manipulation was possible. It also revealed how far the field remained from scalable autonomy.

Perception was geometric and task-specific

Teams relied heavily on depth cameras, LiDAR point clouds, geometric registration and operator-selected regions of interest. These methods worked when the object, scene and expected action were known. They were brittle when the environment differed from the model.

Modern systems can add learned visual representations, language-conditioned models and policies trained across broader datasets. Yet geometric estimation has not disappeared. Successful systems increasingly combine learned perception with conventional estimation, planning and safety constraints.

Behaviours were engineered more than learned

DRC teams created state machines, motion planners and task-specific behaviours. A door-opening routine did not automatically become a general skill for handling every articulated object.

Current imitation learning, reinforcement learning and vision-language-action models promise greater transfer. But demonstrations are still easier than dependable deployment. Policies must handle contact variation, calibration drift, wear, changing payloads and recovery after partial failure.

Data was scarce and fragmented

Each team generated its own demonstrations, maps, models and test results. There was no large, shared corpus of robot interaction comparable with the data available for language or images.

That remains one of physical AI’s central bottlenecks. Robot data is expensive because it must include not just observations, but also actions, embodiment, timing, forces, failures and outcomes.

Contact sensing was limited

Many systems inferred contact from joint torque, hydraulic pressure or motor current. Rich tactile sensing was not a central part of most competition stacks.

Current tactile technologies can measure pressure distributions, vibrations, contact location, slip and local geometry. The next challenge is turning those measurements into datasets and policies that transfer across objects, grippers and robots.

Recovery remained difficult

A robot could complete an impressive planned action and still be defeated by a small deviation. A foot could land several centimetres away from its expected position. A tool could shift in the gripper. A door could resist differently than anticipated.

Modern physical AI often focuses on task success. Production systems will increasingly be judged by something harder: whether they can detect failure, recover and continue without human intervention.

 

5. What DARPA Actually Created in Industry

DARPA did not single-handedly create the humanoid industry. ROS existed before the DRC. Rainbow Robotics had already been founded. Boston Dynamics and many of the participating laboratories had decades of prior work.

What the DRC created was an industrial acceleration mechanism.

It aligned researchers and suppliers around a public benchmark, funded shared infrastructure, made failure visible, trained complete systems teams and gave companies evidence that the technology could eventually leave the laboratory.

A common humanoid development platform

DARPA funded Boston Dynamics to develop Atlas as a shared platform for several teams. Seven teams emerging from the Virtual Robotics Challenge received Atlas robots, allowing researchers to work on a common machine rather than each spending years building a humanoid from scratch.

For the 2015 Finals, Atlas was upgraded with onboard power, wireless operation, improved limbs and greater durability. The robot became a development platform on which numerous teams advanced state estimation, whole-body control, manipulation and operator interfaces.

That lineage continues. Boston Dynamics’ current electric Atlas is a fundamentally new commercial machine, not the hydraulic DRC robot. But it inherits the accumulated organizational knowledge of building, controlling, falling, repairing and operating full-sized humanoids. In 2026, Boston Dynamics announced initial product deployments with Hyundai and a research collaboration with Google DeepMind.

The direct legacy is not one unchanged robot. It is more than a decade of embodied engineering knowledge.

Open-source simulation infrastructure

The Virtual Robotics Challenge required teams to develop and test robot software in simulation. DARPA’s contract with the Open Source Robotics Foundation helped establish the organization now known as Open Robotics and funded several years of work on Gazebo and related infrastructure. Open Robotics itself describes the DRC as a catalyst for the organization’s formation and growth.

The DRC did not create ROS. What it did was strengthen the institutions and simulation tools around the open-source robotics ecosystem.

That contribution was strategically important. Shared simulation lowered the cost of entry, let geographically distributed teams reproduce scenarios and helped establish simulation as part of the normal robotics-development workflow.

Modern GPU simulators are vastly more capable. They support parallel environments, photorealistic rendering, domain randomization and reinforcement learning. But the organizational model—shared robot descriptions, common interfaces and repeatable virtual tests—was already visible in the DRC.

Validation for a new generation of robotics companies

The competition also acted as a credibility engine.

Rainbow Robotics was founded by KAIST researchers in 2011, before the DRC. The 2015 victory did not create the company, but it gave the team an internationally visible proof point. Rainbow later commercialized collaborative and mobile robots, listed publicly in South Korea and became strategically tied to Samsung, which increased its ownership position to 35 percent.

NASA’s Valkyrie program created another important talent and technology lineage. Apptronik describes its humanoid Apollo as rooted in experience accumulated through Valkyrie and more than ten previous robot platforms developed by its team.

IHMC’s work on Atlas helped form a continuing lineage in legged robotics, including Boardwalk Robotics and its electric humanoid Alex. The important industrial transfer was not a single algorithm; it was a group of people experienced in integrating controls, mechanics, interfaces and field operations under pressure.

SCHAFT, created by alumni of the University of Tokyo’s JSK laboratory, dominated the 2013 Trials before withdrawing from the Finals to focus on commercial development. Its acquisition by Google was an early signal that advanced humanoid capabilities had become strategically interesting to major technology companies.

A talent network spanning academia and industry

DARPA challenges concentrate exceptional researchers around a common deadline. After the event, those people disperse—but they carry shared experience, relationships and technical assumptions with them.

Gill Pratt, the DRC program manager, later became chief scientist at Toyota and CEO of the Toyota Research Institute. Russ Tedrake, who led Team MIT, became vice-president of robotics research at TRI. Scott Kuindersma, a key member of Team MIT, went on to lead robotics research at Boston Dynamics.

In 2024, Boston Dynamics and TRI announced a collaboration combining TRI’s large behaviour models with the electric Atlas platform. The project reunited several researchers with direct Team MIT and DRC lineage, including Tedrake, Kuindersma, Pat Marion and Lucas Manuelli.

That is how challenge programs influence industry. They create cohorts of people who have already solved difficult integration problems together and who later recombine inside companies, laboratories and startups.

A commercial component ecosystem

The DRC also demonstrated that advanced robotics did not require every team to build every component.

Teams incorporated common robot platforms, commercial grippers, cameras, force sensors, computers and open-source middleware. Suppliers received unusually demanding field feedback. Researchers learned which components survived impact, vibration, electrical noise, calibration errors and repeated integration.

This helped move robotics toward a more modular industrial ecosystem. The same pattern is now visible in physical AI: foundation-model builders, robot manufacturers, actuator suppliers, gripper companies, simulation providers and deployment specialists can each own a layer of the stack.

A culture of useful public failure

Perhaps DARPA’s most important contribution was making failure acceptable—and informative.

Most industrial demonstrations are designed to hide uncertainty. The DRC did the opposite. Robots failed in public, under a common set of rules, with no marketing edit.

A fall exposed weaknesses in balance and recovery. A dropped tool exposed problems in grasping and perception. A stalled robot exposed weaknesses in power, communications or operator workflow.

Because every team confronted similar tasks, the failures became comparable. The field could see which problems were individual implementation mistakes and which represented broader technological limits.

 

6. The Real Connection to Today’s Physical AI

The current physical AI wave is not simply placing neural-network brains inside DRC-era bodies.

The hardware is changing. Electric actuators are improving. Sensors are cheaper. Compute is denser. Simulation can generate millions of training episodes. Models can connect language, vision and action. Robot fleets can collect data and improve over time.

But the DRC’s systems lessons remain intact:

  • Embodiment matters.
  • Mechanical design can reduce the learning problem.
  • A complete system is limited by its weakest subsystem.
  • Human supervision is not binary; it can be designed and progressively reduced.
  • Recovery matters as much as nominal task execution.
  • Simulation is essential, but reality remains the final test.
  • Reliability is created through integration, not through one breakthrough model.

The DRC did not solve physical AI. It defined the systems problem that physical AI is now attempting to solve at scale.

Its greatest legacy is therefore not a particular robot, controller or winning team. It is an industrial and intellectual community that learned—often through very public falls—what it takes for software and hardware to act reliably in the physical world.

Learn how to deploy Physical AI that works

Leave a comment

Related posts

Robotiq Releases New 2F-85 Isaac Sim Asset on Newton

If you have put a Robotiq 2F-85 into an NVIDIA Isaac Sim scene and closed it on an object, you have probably seen the fingers...

Robotiq Team
By Robotiq Team - September 22, 2026
Robotiq Releases ROS 2 Packages for Adaptive Grippers

If you run a Robotiq gripper in the Robot Operating System (ROS) 2 workspace today, you are almost certainly running PickNik...

Robotiq Team
By Robotiq Team - August 26, 2026
Robotiq Releases an Open-Source C++ SDK for Adaptive Grippers

As physical AI moves from research into real applications, developers need a solid primitive that meets them where they work:...

Robotiq Team
By Robotiq Team - August 12, 2026