Subscribe

Latest Blog Post

5 Unusual Vacuum Grippers Which Innovated Robotics

Alex Owen-Hill
by Alex Owen-Hill. Last updated on Dec 12, 2024
Posted on Jun 20, 2019 in Robot Grippers
7 min read time

In March 2019, a group of researchers from MIT and Harvard announced their latest unusual robot gripper… made of origami! But, theirs is not the first unusual vacuum gripper that we've seen in the world of robotics. Here are 5 unusual vacuum grippers which innovated robotics.

EPick-RobotiqSay bonjour to AirPick and EPick the newest products from the creators of the world's best-selling grippers!

Researchers from the Massachusetts Institute of Technology (MIT) and Harvard University recently announced a new robot gripper that they've been developing. It's a vacuum-based gripper but with a difference…

Instead of using standard rubber vacuum cups — as is the case with most vacuum grippers — they used 3D printed "origami." This produced a rather unusual looking gripper which lifts objects in a very different manner to most vacuum grippers.

This is not the first unusual vacuum gripper that we've seen. Below, we provide a list of 5 unusual grippers that we've seen over the years.

But first… why do researchers build these unusual grippers at all?

New call-to-action

Why unusual grippers are useful

Every few years, a new "unusual" robot gripper appears in the robotics news, usually the result of some new research. At first, these developments might seem frivolous. Just a way to develop a new headline-grabbing gripper which will grab people's attention (and there may be a grain of truth in that).

However, sometimes these new technologies change the way that we think about robot gripping at a fundamental level. As we'll see, many are inspired by nature and biology and bring brand new gripping strategies to the world of robotics. Some — like the coffee granule gripper — are so popular, they inspire roboticists all over the world to make their own versions of the gripper.

5 Unusual Vacuum Grippers Which Innovated Robotics

1. The MIT-Harvard origami gripper

unusual-gripper-origami-gripper-mit-csailOrigami Robot Gripper by the MIT-Harvard / Image: Jason Dorfman/MIT CSAIL

This year's "rock star" vacuum gripper is the development I've already mentioned from MIT and Harvard. The unusual thing about this gripper is that was inspired by origami and looks a bit like a Venus flytrap plant — or so says the MIT News, myself I think it looks like a flower.

The gripper underwent 3 different prototypes before the team arrived at the final design. It was made by 3D printing a cast out of ABS plastic, which was then filled with silicone rubber. At the core of the gripper is a flexible "skeleton" which is covered in the silicone skin.

When the vacuum is activated, the air is sucked out of the gripper's skin. This distorts its shape around the object, providing a strong lifting force without squeezing the object too much. As a result, the gripper is well suited to lifting soft, irregularly shaped items such as fruit.

2. Festo's octopus tentacle

unusual-vacuum-grippers-tentaclegripperTentacleGripper / Source: Festo Corporate

I first encountered Festo back in 2010 when I saw a video of their Air-Ray balloon, modeled on a Manta Ray fish, flying through the air. Since then, I've been intrigued again and again by the air-based robotic technologies that Festo has released.

Festo's TentacleGripper is another example of an unusual vacuum gripper which turned robotic gripping on its head when it slithered onto the scene in 2017. Made of soft silicone, the gripper can wrap around the shape of objects and suck itself onto them in a manner that mimics an octopus tentacle.

This gripper uses its vacuum technology in two distinct ways:

  1. The vacuum changes the shape of the tentacle to wrap around the object.
  2. The small suction cups that line the inside of the tentacle provide extra suction onto the surface of the object, in a similar manner to standard vacuum grippers.

3. Starfish soft robotics

vacuum-gripper-Starfish-footSoft Robotics for Chemists

Another sea-creature-inspired vacuum gripper was announced in 2011. This starfish-like gripper was the work of Prof. George Whitesides from Harvard University, who is a strong proponent of soft robotics.

Made from soft polymer rubber, the gripper is sort of the opposite of a vacuum. Instead of sucking the air out of the gripper, it uses pneumatics to inflate air sacks inside the gripper's fingers. This causes the fingers to bend their shape around the object, providing an evenly-distributed force without crushing the object.

Since then, Prof. Whitesides and his research group have gone on to further remove hard components from robotic gripping. Last year they produced soft valves which allow the entire gripping mechanism to be made from soft components.

4. Shape memory alloy "artificial muscles"

Here's a very interesting one. In 2018, researchers from Saarland University in Germany announced that they had created a vacuum gripper that doesn't need compressed air or a vacuum generator!

The gripper works using a shape memory alloy, a type of flexible metal which returns to its original shape when an electrical pulse is passed across it. The researchers used this material property to provide a new way to generate a vacuum.

The gripper functions like this:

  1. The suction cup is placed onto a flat, non-porous surface.
  2. The shape memory alloy wires are activated with electricity.
  3. This creates a strong, stable vacuum under the suction cup.

The researchers describe their mechanism as "artificial muscles."

5. Balloons and coffee granules

vacuum-gripper-coffee-beans

Universal robotic gripper based on the jamming of granular material / Source : Cornell University

Possibly the most popular unusual vacuum gripper of the last decade is the balloon and coffee gripper.

This gripper design burst onto the scene in 2012, when researchers at Cornell University announced their Universal Jamming Gripper — "universal" because it can pick up pretty much any oddly shaped object.

The gripper is made of granular material inside a flexible rubber skin. When the vacuum is applied, the granules jam into position, which grasps them tightly around the contours of the object.

The design has been very popular among hobbyists because it is so easy to make at home. You simply need to fill a rubber balloon with coffee grounds and attach it to a plastic funnel. Tutorials to make your own universal gripper can be found from Make: magazine, which uses a vacuum cleaner to provide the suction, or from Instructables, which uses a syringe for the suction.

What if you just want a reliable vacuum gripper?

These unusual vacuum grippers are certainly fun. They can change the way we think about gripping. They provide new gripping strategies which allow us to pick up even more objects using vacuum grippers.

However, although it's interesting to see these unusual grippers, most of us don't need them for our own applications.

For most of us, we just need an easy-to-use, reliable vacuum gripper which integrates seamlessly with our robots. Thankfully, there are some great solutions for vacuum grippers.

 

What do you need from a vacuum gripper? Tell us in the comments below or join the discussion on LinkedIn, Twitter, Facebook or the DoF professional robotics community.

New Call-to-action

Leave a comment

Related posts

Hand-E Now Reaches 100 mm Without Giving Up an Ounce of Precision

If you've been using Hand-E Adaptive Gripper on your production line, you already know why it's earned its reputation: a...

Robotiq Team
By Robotiq Team - July 16, 2026
How Sennheiser increased PCB testing by 33% with a Robotiq 2F-85 gripper

At Sennheiser Manufacturing USA in Albuquerque, precision is non-negotiable.

Every week, the facility assembles 30,000 printed...

Linnea Bruce
By Linnea Bruce - February 11, 2026
Robotiq brings the sense of touch to Physical AI

Physical AI has reached a critical point. Robots can see, plan, and decide better than ever—but manipulation in the real world...

Jennifer Kwiatkowski
By Jennifer Kwiatkowski - January 27, 2026