Subscribe

Latest Blog Post

11 Useful Tips When Deploying Decentralized Palletizing

Alex Owen-Hill
by Alex Owen-Hill. Last updated on May 12, 2022
Posted on Jun 04, 2021 in Palletizing
5 min read time

Want to speed up your palletizing deployment? Decentralized palletizing can offer some important benefits for your business. But, you need to ensure that you do it right.

Palletizing is often the first task to be automated by a business. It's a repetitive, boring, and non-value added operation that can be easily given to a robot… as long as you set it up correctly.

Automating a palletizing task can improve worker safety (thanks to the ergonomics benefits), ensure consistent handling of palletized items, and regulate the flow of product through your facility.

Decentralized palletizing provides added benefits compared to centralized palletizing. Each palletizing robot serves just one or a few product lines, giving you better flexibility and control over your whole operation and reducing the impact of incidents on your entire workflow.

In this article, we'll provide a few tips on how to deploy your decentralized palletizing robot more effectively and how to get the most from collaborative robots for this task.

 

Collaborative robot taking boxes from a conveyor and placing them on a pallet.

 

What makes deploying decentralized palletizing different?

Deploying decentralized palletizing is a little bit different from deploying other robot applications.

For one thing, the real benefits of it come when you have multiple palletizing robots performing the same task at once. Instead of just deploying one robot and seeing how it goes before deciding to deploy more — as you would with another application — you are likely starting with the intention to deploy multiple robots soon.

Our usual advice when deploying a new robot is to just start with a single, simple cell.

This is still true with palletizing. However, you will make your life easier if you focus on creating a robot cell that is easy for you to copy-paste when you are ready to deploy your next cell.

For this reason, it can be very helpful to start with a pre-designed palletizing cell.

6 useful tips when using decentralized palletizing

Deploying a robot for decentralized palletizing is slightly different from just deploying a single palletizing cell.

Here are some specific tips for decentralized palletizing:

1. Decentralize palletizing responsibility

With decentralized palletizing, each palletizing robot is assigned to one or a few product lines. Therefore, it the makes most sense to assign the responsibility of the robot to whoever is responsible for the product line itself.

This makes the approach different from centralized palletizing where one person can be responsible for all palletizing operations in a facility.

2. Use easy-to-operate robots

One potential difficultly with decentralizing the responsibility over the robots is that not everyone is skilled in robot programming.

This is why easy-to-operate robots (such as collaborative robots) are so effective for decentralized palletizing. If anyone can operate the robot, it's much easier to make changes.

3. Group similar palletizing tasks

Depending on your setup and needs, you might not want to have a different palletizing robot for every single product line. You can keep a decentralized palletizing approach by grouping similar palletizing tasks together and using one robot with a few product lines.

This is also suitable when you don't have a high enough throughput to justify using one robot per product line.

4. Create copy-paste cells

You will make your life much simpler by creating a palletizing cell that can easily be copy-pasted when you want to deploy your second palletizing robot.

Focusing on easy replicability will affect how you deploy the first cell.

5. Go with smaller robots

With centralized palletizing, it might make sense to opt for a large industrial palletizing robot if your throughput is very high. However, this is less feasible with decentralized palletizing.

Smaller collaborative robots are a more flexible, cost-effective solution that works much better for a decentralized approach.

6. Track the right KPIs

The only way you can tell how well your palletizing robots are performing is by measuring their performance with the right metrics. Choose those metrics that align with your wider business metrics.

Three good metrics to track with palletizing include:

  • Ergonomy — e.g. track musculoskeletal injuries associated with the repetitive task of manual palletizing.
  • Capacity of the cell — e.g. box per minute or pallets per hour.
  • Employee turnover — e.g. employee turnover rate affected by the boring task.

5 useful tips when deploying a cobot for palletizing

Thanks to their small size and easy operation, collaborative robots are a great option for palletizing, especially if you use a pre-designed palletizing solution.

Here are some tips for getting the most from cobot palletizing:

1. Go for simple projects first

It's best to start with a palletizing task that is both simple and will have high value for the business. Examples of simple palletizing tasks that are ideal for cobots are those with no mixed pallets and that have a reasonably low throughput.

2. Start with a manual task mapping

Cobots are best suited to tasks that were previously performed manually by humans. For this reason, it's best to start your robot deployment by creating a manual task map, where you plot the operator's actions for the manual palletizing task.

3. Consider the payload and center of mass

With huge industrial palletizing robots, the weight of the items to be palletized is often well within the robot's payload capacity. With cobots, you will have to pay more attention to the payload capacity of the robot and the center of mass of the items to ensure they can be handled by the robot.

4. Consider the robot's reach

Cobots also have a more limited reach than most conventional palletizing robots. The benefit of this is that they take up less space. However, it does mean you need to be careful that everything in the palletizing cells is within the robot's reach when you design the cell.

5. Use a palletizing configurator

You can significantly speed up the deployment of your palletizing cobot by using a dedicated palletizing configurator. This allows you to prepare and program your robot quickly and easily.

To learn more about how to deploy your own palletizing cobot, check out our free eLearning course.

How to get started with your decentralized palletizing

Interested in learning how you could use cobots for decentralized palletizing in your business?

You might be interested in our Robotiq Palletizing Solution. It provides a quick-to-deploy solution that is suitable for many palletizing tasks.

Watch the Palletizing Demo

What tasks could you do more effectively with a palletizing robot? Tell us in the comments below or join the discussion on LinkedIn, Twitter, Facebook, or the DoF professional robotics community.

Leave a comment

Related posts

How IQ Gives Manufacturers a Faster, More Predictable Path to a Running Palletizing Workcell

Getting a palletizing project done right has always depended on having the right information at the right time. Product specs,...

Robotiq Team
By Robotiq Team - June 12, 2026
Robotiq Launches IQ to Make Palletizing Automation Faster and More Predictable

Most manufacturers who want to automate palletizing face the same problem. Getting a straight answer on whether it fits their...

Robotiq Team
By Robotiq Team - June 2, 2026
Why Do Palletizing Automation Projects Fail? 5 Pitfalls and How to Fix Them

Palletizing automation is one of the clearest wins in end-of-line operations. The ROI is real, the labor savings are immediate,...

Amanda Lee
By Amanda Lee - May 27, 2026