Subscribe

Latest Blog Post

get help with your robotic project

How to Quickly Integrate Your New Collaborative Robots

Mariane Davids
by Mariane Davids on Sep 5, 2017 7:00:00 AM

Collaborative robots are a massive new trend that makes life easier for businesses by providing safe and easy to program option that works alongside human worker. Once you’ve purchased a cobot, the next step is to integrate it. There are several things to consider when working on integration.

universal-robots-collaborative-robots-940637-edited.jpg

 

Today’s information comes straight from Robotiq’s eBook on this subject. You can find this book, and many more here. This particular eBook starts with a look at collaborative robots and what they are used for. The top applications, as described in the book, are as follows:

● Machine Tending

● Material Handling

● Assembly Tasks

● Packaging

These tasks are easy for integration. You simply connect your cobot, teach it through hand guiding, and you’re ready to go. Furthermore, these tasks are easy to work hand-in-hand with humans. Assembly tasks can be done efficiently without putting your employees at risk.

The eBook also describes the soft design nature of cobots, covering points like soft geometry and minimal pinch points. There’s a drastically reduced chance of impact or crushing due to impact. Collaborative robots are programmed to stop moving if they collide with a person.

The next portion of the eBook places specific information about how to quickly integrate your collaborative robots. Some of these highlights include the following:

Robot Fixture - For starters, you should seek to anchor the robot in place as much as possible, and set a reference point on the factory floor. You need to ensure that there’s no slipping or sliding as this will throw off the efficiency and functionality. Anchors should be used to keep robots with wheels in place, for example.

Part Input - There are multiple ways to locate parts. An array for example, is the simplest way to organize parts. Other options like an inclined plane can be used to bring parts to the same position every time a robot needs to grab them. Drawers can also be used, or the option for vision systems paired with encoders on the conveyor belt can be used. Force torque sensing is another option to consider as it gives the robot the ability to “touch” and feel out where the parts are located.

Part Output - You’ll need to consider the operations on the parts and how it can be properly tracked for quality assurance.

Robot Positioning - The actual robot should be placed within your workflow based on safety and performance. Keep it out of the way, but also where you typically have bottlenecks so it can properly integrate and improve your efficiency.

Machine to Robot Interface - The status of a robot and a machine needs to be communicated properly. The eBook lists out several signals that can be used to understand the principles behind these connections.

Robot Tools - The tools that the robot will use are important as well. They should be considered in regards to the gripper you’ll be using to manipulate the tool.

Final Thoughts

This Robotiq eBook offers some excellent insight into the integration of collaborative robots in the workplace, and should be referenced by any manufacturer looking to integrate as quickly a possible.

COLLABORATIVE ROBOT TIPS FOR FAST INTEGRATION   DOWNLOAD THE EBOOK HERE

 
x

Subscribe to Robotiq's Blog

Leave a comment

Mariane Davids
Written by Mariane Davids
Mariane Davids is a social media marketer with over a decade of experience in the industry. She's now bringing her decade of experience to others so they can better connect with their communities.
Connect with the writer:

Related posts

What's New in Robotics This Week - Sep 08

 - Manufacturing & cobot roundup- John Deere acquires Blue River Technologies- Meet Musio - India's Ganpati bot and much more....

Emmet Cole
By Emmet Cole - September 8, 2017
How Procter and Gamble Is Leading the Way With Cobots

The consumer goods industry is starting to accept collaborative robots. Procter and Gamble is leading the way, and has been for...

Alex Owen-Hill
By Alex Owen-Hill - September 6, 2017

Is it possible to save programs using a network connections rather than the USB key

Hi pros,anyone know if it is possible to save programs on our plant network directly from the UR rather than saving on a USB stick? Could we also load the programs from the network? Read more

Is it possible to process the image acquired from the wrist camera with a different img proc toolbox

Because of the camera's form factor and integration with Robotiq products, I'd like to use the wrist camera. However, I need to leverage some of the features and functions that Halcon Merlic offers....Read more

Updated specs for new FT300 sensor?

So I'm looking at this page in the FT300 manual and it says it was last updated April 2017.With the overhaul of the sensor that decreased signal noise, are the updated specs available anywhere...Read more