Subscribe

Latest Blog Post

Servo-Electric Gripper: How Does It Work

Samuel Bouchard
by Samuel Bouchard. Last updated on Dec 12
Posted on Apr 05, in Robot Grippers
2 min read time

This article presents an overview on how a servo-electric gripper works. The image below shows the main components of an electric gripper and how it interfaces with a robot.

Here is how servo grippers works:

  1. An Input command is sent to the gripper from a robot control unit. This unit is usually pre-programmed by an operator via a teach pendant. With most electric grippers, the command can be a position, a speed or a grip force. The robot can send commands to the gripper using digital I/O's, or by using any of the available robot communication protocols.

  2. The command from the robot is received by the gripper control module responsible for driving the gripper motor(s). This gripper module is sometimes embedded in the gripper but most of the time it consists of a box sitting between the robot controller and the gripper.

  3. The servo-electric motor reacts to the signal. The shaft will then rotate to the commanded position, speed or force. To enable closed-loop control, feedback from the motor position is usually necessary at the gripper level. Until there is a signal change, the servo will hold the position (and resist change).

  4. Some servo grippers can also send a status (jaw position, speed, grip detection) back to the robot control unit.

2-Finger-85-Adaptive-Robot-Gripper-encompassingFlexible Programming Options

The servo-electric gripper can be programmed via an interface integrated to the robot control or on it's own control unit. For example, Robotiq's Adaptive Gripper can be controled via a very simple Touch-Screen GUI where teaching the gripper is done the same way (and same timeframe) as using the robot teach mode.

If you're wondering what gripper to choose for your application, read this article on the advantages of servo electric grippers and this one on how to choose the right gripper for your application.

Download this Free Guide on  How to Choose your Gripper Now

Leave a comment

Samuel Bouchard
Written by Samuel Bouchard
Samuel is CEO and co-founder of Robotiq. His mission is to free human hands from repetitive tasks. He is also the author of Lean Robotics: A Guide to Making Robots Work in Your Factory. He lives in Québec City with his wife and four children.
Connect with the writer:
http://robotiq.com

Related posts

7 Things I Learned From Marketing Cobot Grippers

In the three years I’ve been working at Robotiq, I’ve been responsible for marketing several products, including the Robotiq...

Christine Giguère
By Christine Giguère - June 2, 2021
Robotiq Improves its Hand-E Adaptive Gripper

Challenges in automation continue to grow as robotics evolve over time, which leads to opportunities for improvement. Critical...

Valérie Lavoie
By Valérie Lavoie - June 11, 2020
10 Packing Jobs That Cobot Vacuum Grippers Can Do

Manual packing can be arduous and inefficient. A cobot with a vacuum gripper can improve the productivity of packing, but it...

Alex Owen-Hill
By Alex Owen-Hill - October 17, 2019