Blog | Robotiq

Notes from the 2015 International Collaborative Robots Workshop

Written by Samuel Bouchard | Oct 22, 2015 2:15 PM

I am just back from the 2015 International Collaborative Robots Workshop where I spoke about grippers for collaborative robots. This forum brings together users, suppliers and researchers interested in the field. I’m thankful to RIA for the opportunity to discuss these important topics. I am also glad that they decided to organize this last workshop in Pittsburgh, because there is a tremendous robotics community there that I haven’t had the chance to visit for some time. Here are my notes from the event.

The basics

Everybody agrees that collaborative is an application, not a robot type. Everyone agrees that there are 4 types of human-robot collaboration in manufacturing. But in the end, nobody in the audience really cared about the first 3 types; what people are really interested in are power and force limited robots that are easy to use and don’t need guarding.

As usual, safety was one of the main topics in every talk. Then again, everybody agrees : Safety is about the application and you must do a risk assessment. How?... That’s the big fuzzy open question.

Millennials, manufacturing and collaborative robots

Henrik Christensen from Georgia Tech made the point again that young people entering the workforce have played more than 3 full years of video games and we should try to leverage this skillset. We should also check which type of console people use nowadays to play, it’s not only about the game controller.

Jim Lawton from Rethink Robotics also mentioned the disinterest of millennials in traditional manufacturing. Easy to use and productive robots have the potential to interest younger people with the maker mentality. They could even be interested enough to want to use robots to build stuff as a job. Totally agree again!

Collaborative Robots - Vendor Roundup

RIA invited many robot suppliers to present their take on the technology, its applications and market.

Rethink Robotics - The Software Company

Jim Lawton, Technology Executive - Rethink Robotics

Jim Lawton surprised the audience by stating that he works for a software company that makes robots. He explained the usual impetus behind the cobot wave (demography, cost of labor, enabling technologies). Now that we (almost) have safe, cheap and easy to use robots, what is coming up? First, Jim underlined the low price or fast ROI of the collaborative robots. He also agrees with the fact that millennials are not interested in manual tasks and that bringing robots to the manufacturing chain is stimulating for them. Robots such as Baxter and Sawyer work like people do, they can carry human sized parts and do pretty much what a human can do. Finally, he said that robots can adapt to variability through machine learning and that they can be repurposed to a different application quickly. 

UR - The Robots of the People

Scott Mabie, General Manager - Americas - Universal Robots

I was wondering about the number of Universal Robots on the market and Scott Mabie told us that more than 5,000 Universal Robots have been sold so far. It is quite impressive to see how fast collaborative robots are growing. Some major manufacturers such as Maytag even feature the robot in their commercial.

ABB - The Volvo of Collaborative Robots

Phil Crowther, Global Product Manager Small Robots - ABB Robotics

If a 3-point safety belt would exist in robotics, ABB would invent it. Mr. Crowther presented their rigorous (and complex) approach to safety which they obviously take very seriously. I could finally play with YuMi in the exhibition area. The booth personnel seemed a little stressed by everybody touching the robot as if something might go wrong. That is the joy of robots for non-experts! For the little that I saw, it worked perfectly well. 

It was the first time I got a look at their clean, user friendly interface to program the YuMi. Other large end users who tried it also liked the idea of leveraging the existing know how of the more powerful and proven ABB tools if they needed to do more complex tasks. Just like Volvo cars, it is a very nice piece of engineering designed with the human in mind. As a gripper manufacturer, I can really appreciate the tight combination of the technology in their arm, the compact packaging of power, air and even embedded vision in the end effector. Mr. Crowther also talked a bit about the future of robot teach pendants, where smart phones and cloud computing would take the place of industrial PCs and large pendants. We have an interesting article on this subject by the way.

FANUC - The Lord of Robots

Paul Santi, General Manager - Powertain Systems Group - FANUC America Corporation

FANUC has been a reigning industrial robotics company in North America for years, winning the battle for market share by leveraging solid technology and top system integrators. You can clearly see that the FANUC presentation was colored by their history with their most important customer base : the automotive industry.

I agree with Paul that some things don’t change. You still need reliability and productivity increases. If I take the point of view of most automakers, I also agree that you still need integration for interfacing with machines and controlling the process. Their high payload, full featured, integration heavy approach for their new CR-35iA makes complete sense for the automotive industry. It makes no sense for SMEs who don’t need all the features and can’t get a competitive ROI if they can’t do most of the integration themselves. 

Precise Automation - The Underdog

Brian Carlisle, CEO - Precise Automation

I was quite impressed by Precise’s presentation and I really think that they have a great, underestimated potential in the market. One reason is probably because we don’t know them as well as the other players. Mr. Carlisle presented the general idea that they are used to making safe robots; leveraging the intimate knowledge of the physics of robots and software. They now have a very interesting lineup of Linear, SCARA and 6-axis robots. With targeted applications for a low payload (<3 kg); their robots are well suited for parts handling, laboratory automation and other lightweight applications. We have recently featured them in our eBook on Collaborative Robots.

Collaborative Robot User Panel

RIA invited three different collaborative robot users to share their experience in choosing, implementing and leveraging collaborative robots.

GM – The Expert User

Marty Linn, Robotic Principal Engineer - General Motors

Since General Motors was an early adopter of industrial robots (let's say they almost invented them) you would think that such company would have bunch of collaborative robots working alongside humans to cover all the difficult or redundant tasks. We're not there yet. In fact, with applications requiring a big payload, it is hard to incorporate a robot with a 5 kg payload to do a heavy task. Another disadvantage of collaborative robots is their relatively small reach. With the new Fanuc CR-35iA, GM is getting one step closer to the introduction of collaborative robots in the automotive industry. They have been testing the CR-35iA for almost a year now in 2 different applications. The fact that the robot can carry heavy parts (up to 35 kg) and has a long reach makes the robot pretty interesting. Compared to SMEs, GM does not need the intuitive programming platform that most collaborative robots are promoting, as they have the in-house knowledge and the repeatability volume to program the robot with standard programming methods. This is why the Green Fanuc is great for them, they are a traditional user. 

Glidewell Laboratories – The High Mix / Low Volume Process

Daniel Phee, Mechanical Design Engineer - Glidewell Laboratories

Glidewell Laboratories also shared their experience of using a collaborative robot. Glidewell is manufacturing custom dental crowns in California. With a production of 3,000 to 3,500 crowns per day, they decided to introduce Universal Robots into their process to do the machine tending. Using nine UR robot arms, the company is saving 150 human hours per week. Watch the video to have a better idea of their installation.

 

Sepcoe Erie - The Job Shop

Chris Pedersen, Operations Manager and Mechanical Engineer, Sepcoe Erie

Chris and his team installed a Universal Robots in a month and a half, got a ROI of 6 months, doubled capacity and reduced scrap by half. Moreover, they improved the workers morale by eliminating a station that was stressful, dirty and highly redundant. That is a great success story on how collaborative robots can increase the productivity of SMEs.

This panel included a wide spectrum of users; illustrating the differences between large and small companies with respect to collaborative robots. GM stuck to their preferred supplier to keep the same programming and interface to resolve ergonomic issues and smaller companies deployed new platforms on their floors to enhance productivity. Between all these factors the deployment time should also be considered, a few months for the smaller companies, a few years for GM who needed to do a lot of up front work. For all of them, one concern was employees’ perceptions of the new robots before installation. All agreed that after installation and training, the employees loved the robots who would do the redundant jobs. That is what collaborative robots are all about.

To have a better idea of the different collaborative robot models, take a look at the document we have put together. It contains all the latest collaborative robots on the market including the Fanuc CR-35iA.