Subscribe

Latest Blog Post

Industrial robots: What are the different types?

Samuel Bouchard
by Samuel Bouchard. Last updated on Dec 19, 2024 4:33 PM
Posted on Mar 13, 2014 9:04 AM. 5 min read time
motoman fanuc robot types of robot

An industrial robot commonly refers to a robot arm used in a factory environment for manufacturing applications. Traditional industrial robots can be classified according to different criteria such as type of movement (degrees of freedom), application (manufacturing process), architecture (serial or parallel) and brand. Then there is also a new qualifier for industrial robots that can be collaborative or not. This article presents the different classifications with some examples.

Industrial robots with different types of movements

Cartesian robots

Cartesian robots are robots that can do 3 translations using linear slides.  

cartesian robots axiscartesian robots

Scara robots

Scara robots are robots that can do 3 translations plus a rotation around a vertical axis.

scara robot w axis

6-axis robots

6-axis robots are robots that can fully position their tool in a given position (3 translations) and orientation (3 orientations)

6 axis robots

Redundant robots

Redundant robots can also fully position their tool in a given position. But while 6-axis robots can only have one posture for one given tool position, redundant robots can accommodate a given tool position under different postures. This is just like the human arm that can hold a fixed handle while moving the shoulder and elbow joints.

Kuka LWR electric gripper resized 600

Dual-arm robots

Dual-arm robots are composed of two arms that can work together on a given work piece.

dual arm motoman with electric robotic hand

The type of movement is dictated by the arrangement of joints (placement and type) and linkages.             
                                

Cable management on UR

Industrial robots for different applications

The application is the type of work that the robot is designed to do. Robot models are created with specific applications or processes in mind. Different applications will have different requirements. For instance, a painting robot will require a small payload but a large movement range and be explosion proof. On the other hand, an assembly robot will have a small workspace but will be very precise and fast. Depending on the target application, the industrial robot will have a specific type of movement, linkage dimension, control law, software and accessory packages. Below are some types of applications:

Welding robots
motoman welding robot 1

Material handling robots

delta robot adeptPalletizing robot
palletizing robotMeet the Palletizing SolutionPainting robot
painting robot abb 1

Assembly robot
assembly robot kuka 1

Serial or parallel industrial robots

Serial robots are the most common. They are composed of a series of joints and linkages that go from the base to the robot tool. 

Parallel robots come in many forms. Some call them spider robots. Parallel industrial robots are made in such a way that you can close loops from the base, to the tool and back to the base again. It's like many arms working together with the robot tool. Parallel industrial robots typically have a smaller workspace (try to move your arms around while holding your hands together vs the space you can reach with a free arm) but higher accelerations, as the actuators don't need to be moved: they all sit at the base.

2 finger robot gripper and parallel robot 1

Industrial robot brands

There are many industrial robot brands. The largest ones will have a complete range of robots for different applications and at different sizes. The smallest companies usually target a specific size or application range. Examples of industrial robot brands are:

To summarize all of the above, it is possible to have for instance:

  • Scara movement, packaging, parallel, ABB robot
  • 6-axis, welding, serial, Motoman robot

The latest generation: Collaborative industrial robots

There is a new qualifier that has just recently been used to classify an industrial robot, that is to say if it can collaborate with its human co-workers. Collaborative robots are made in such a way that they respect some safety standards so that they cannot hurt a human. While traditional industrial robots generally need to be fenced off away from human co-workers for safety reasons. Collaborative robots can be used in the same environment as humans. They can also usually be taught instead of programmed by an operator. Examples of collaborative robots are:

 

Leave a comment

Samuel Bouchard
Written by Samuel Bouchard
Samuel is CEO and co-founder of Robotiq. His mission is to free human hands from repetitive tasks. He is also the author of Lean Robotics: A Guide to Making Robots Work in Your Factory. He lives in Québec City with his wife and four children.
Connect with the writer:
http://robotiq.com

Related posts

Industrial Robots: 5 Most Popular Applications

Industrial robots have been in use for about 50 years. The first industrial robot was used for material handling in a General...

Jean-Philippe Jobin
By Jean-Philippe Jobin - December 19, 2024
How to Combat The Great Resignation and Keep Talent with Robots

As the dust is settling on the 2020 global pandemic, many workers are finding themselves in a unique position. An abundance of...

Alex Owen-Hill
By Alex Owen-Hill - January 6, 2023
How to Convince Employees to Accept Robot Workers

When a company like yours first wants to adopt robots into the workplace, there can be resistance from employees.

Some people...

Alex Owen-Hill
By Alex Owen-Hill - October 25, 2022