Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

NeuroArm: a Robot Brain Surgeon

Samuel Bouchard
by Samuel Bouchard. Last updated on Jan 29, 2015 10:23 AM
Posted on Apr 23, 2007 8:08 AM. 2 min read time

neuroarm

Brain surgery can have an immeasurable effect on a patient’s life. Just ask my friend Jean. His epilepsy is gone since such an operation, and his life has changed for the best. Obviously, such operations are risky. The recent announcement of the NeuroArm promises more accurate and safer brain surgeries. The impact on human lives is impressive: so is the technology behind this ambidextrous robot.

Inside a magnetic resonance imagery (MRI) machine

The idea driving the NeuroArmis is to be able to work inside an MRI machine. We can “see” inside a human body using these machines. Seeing inside a brain in real-time during an operation is a major advance in neurosurgery.

As its name indicates, the MRI uses a magnetic field to image the body. This provides significant technical challenges to roboticists. They must avoid all sensors and activators that generate magnetic fields. In addition, they must select materials that will not interfere with the magnetic field. This is why the NeuroArm is made mainly of titanium and PEEK, a plastic composite.

The surgeon’s immersion
In addition to receiving 3D imaging from the MRI, the stereoscopic cameras film the instruments in action. Everything is projected in stereo in the surgeon’s eyewear.

The doctor works two levers controlling the robotic instruments. They look like modified Phantoms. They provide tactile feedback so that the doctor feels like he is working on human tissue using real instruments. The user’s vibrations are filtered out, making the tools perfectly steady and making operations at the 50-micron precision level of individual cells possible. The best surgeons used to be able to operate at no less than 1-2 mm (1000-2000 microns).

The Canadarm in your head
Calgary University researchers carried out the project.Financing came from petroleum industry philanthropists at first, then from various provincial and federal research funds. Canadarm builder, MDA, built the robot. In space robotics as in medical robotics, safety and reliability are reaching incredible levels. Lives are at stake here. MDA was therefore able to transfer its experience from space to medicine. When you see the NeuroArm, you’d think it was the little landlubber brother of Dextre, who will be installed on the arm of the international space station.

Leave a comment

Samuel Bouchard
Written by Samuel Bouchard
Samuel is CEO and co-founder of Robotiq. His mission is to free human hands from repetitive tasks. He is also the author of Lean Robotics: A Guide to Making Robots Work in Your Factory. He lives in Québec City with his wife and four children.
Connect with the writer:
http://robotiq.com

Related posts

The Human View of Robot Workers: What Do Employees Really Think?

Robot workers are transforming the way we work. There is no denying that they are here to stay… but this raises some...

Alex Owen-Hill
By Alex Owen-Hill - February 21, 2023
7 Exciting and Effective Applications for Robotics in Retail

Robotic technology is transforming the retail industry. With robots, retailers of all sizes can automate and streamline...

Alex Owen-Hill
By Alex Owen-Hill - February 17, 2023
10 Robotics Predictions for Trends That Will Dominate 2023

Robots have come a long way since their early days as big, clunky machines that took up vast spaces in factories.

Today, robots...

Alex Owen-Hill
By Alex Owen-Hill - December 20, 2022