Subscribe

Latest Blog Post

Why Do Palletizing Automation Projects Fail? 5 Pitfalls and How to Fix Them

Amanda Lee
by Amanda Lee. Last updated on May 27, 2026
Posted on May 27, 2026 in Palletizing
6 min read time

Palletizing automation is one of the clearest wins in end-of-line operations. The ROI is real, the labor savings are immediate, and the technology is mature. Yet many manufacturers stall out, spending months on projects that should take weeks, or deploying systems that work in the demo but struggle on the production floor.

The good news: most of these failures follow predictable patterns. Here are five pitfalls we see repeatedly, and how to avoid them, illustrated by how Molino Merano, a historic Italian flour producer, turned a tight floor, a staffing problem, and a growing product line into a 14-month payback.

Moliono-merano-palletizing-end-of-line
Pitfall #1: Overestimating installation complexity

A lot of manufacturers never start a palletizing project because they're convinced it will mean months of production downtime, deep integration work, and a long commissioning process. That expectation, more than anything else, is what keeps manual palletizing in place long after it stops making sense.

When the solution is pre-engineered and standardized to connect with an existing line, deployment looks very different. Training is part of the package. The conveyor integration is straightforward. The commissioning period shrinks from months to days. The belief that automation is inherently slow to deploy is worth questioning before it shapes your decision. Part of what makes that possible is having the project information well organized from the start: customer requirements, site constraints, throughput targets, and layout realities all in one place, rather than scattered across emails and spreadsheets. When that groundwork is done upfront, the path from decision to running system gets much shorter.

Pitfall #2: Designing for perfect conditions

Real production floors have tight spaces, ceiling limits, layout constraints, and equipment that was installed a decade ago with no thought for what might come next. A solution engineered for a clean, open layout will always struggle when it meets a real factory.

Hardware that adapts to compact footprints and software that handles changing SKUs are not nice-to-haves. They are what determines whether a system still works two years after installation.

Pitfall #3: Not planning for variability

Many manufacturers rarely run one product. They run dozens, and that number tends to grow. A system that handles this year's SKU mix cleanly may struggle badly when a new format gets added or a customer changes their pallet specification.

Building for today's conditions without accounting for tomorrow's variability is a setup for re-engineering costs down the line. Choosing a system with flexible pattern programming, one where operators can make changes on their own, keeps the production line scalable as the business evolves.

Pitfall #4: Starting with the most complex operations

There's a logic to tackling the most complex line first. The biggest bottleneck, the highest labor cost, the most compelling ROI case. But starting with complexity adds complexity. Timelines stretch, scope grows, and the project loses momentum before it ever delivers.

A single, well-scoped project on a line with clear constraints and a realistic payback period does something a complex rollout rarely does: it finishes. This is the foundation of Lean Palletizing — start simple, build operator confidence, create the internal expertise that makes the next deployment faster and easier to approve. Start simple, prove it and then scale.

Pitfall #5: Over-engineering the solution

Customization can feel like thoroughness. The more the system is tailored to your operation, the better it should perform. In practice, highly customized systems take longer to deploy, are harder for operators to understand, and create a long-term dependency on external support for every change.

Standardized automation and proven solutions deliver faster. Operators learn them more quickly, maintain them more confidently, and own them more completely. When someone on the floor can adjust a pallet pattern or troubleshoot a fault without escalating, the system pays back more every single day. The same principle applies to the integration process itself: when the workflow for scoping, validating, and deploying a Workcell is repeatable and structured, partners can move faster and manufacturers face fewer surprises.

How Molino Merano avoided all five

Molino Merano has been producing flour products in the historic town of Merano, in Trentino Alto Adige in northern Italy, since 1985. The company had a floor space problem, a staffing problem, and a product line that kept growing. What they didn't have was time for a 12-month automation project. Here is how they worked through each of these challenges.

What pushed them to act

As the product line expanded, the end-of-line operation started showing the strain. Manual palletizing, where operators lifting and placing every box, shift after shift was slowing throughput and wearing people down. Finding staff for that kind of work was getting harder. And the production floor simply didn't have the space to bring in a traditional palletizer.

What they needed wasn't a large-scale automation project. They needed something that would fit where they had space, go in fast, and work reliably from day one.

What they deployed

Robotiq's cobot palletizing Workcell fit the floor where a conventional system couldn't. No fencing, no area scanners, just a collaborative Workcell that worked safely within the constraints of the existing layout, respecting the actual line rather than requiring the line to change around it. The solution handled multiple SKUs, allowed pallet changes without stopping production, and came with operator training built into the deployment.

What changed

The Workcell was in production within a week of installation.

As the product range had grown, so had the pressure on the team. Automating palletizing meant that pressure didn't have to grow with it. Staffing the end of the line stopped being a recurring problem. Operators moved to other parts of the operation where their time had more value.

But the change that stands out most isn't about throughput or headcount. Before the cobot, the end-of-line team was lifting every box onto every pallet, hundreds of times a day. Back pain was routine and that manual work is gone now. The physical environment at the end of the line is genuinely better, and the team feels it.

Molino Merano even reached a full return on investment in 14 months, across a footprint that fit the floor they actually had.

Molino Merano solution

Questions manufacturers ask before getting started

How long does a palletizing project actually take? Weeks, not months, and the gap is closing. Molino Merano went from installation to live production in under a week. With the right information organized upfront and a structured workflow from scoping to deployment, what used to take months is becoming a matter of days. The timeline depends far more on how well the project is prepared than on the technology itself.

What if our floor doesn't have much space? That's one of the most common constraints, and a good reason to look at cobot solution specifically. They're designed for compact footprints, work without safety fencing, and can be configured around existing equipment rather than requiring the line to move around them.

We run a lot of different products. Can one system handle all of them? Yes, if the system is built for it. The key is flexible pattern programming that operators can manage themselves. If changing a pallet configuration requires a service call, that's a problem at scale.

How quickly will we see a return? It depends on volume, labor costs, and how much downtime the current operation is absorbing. For Molino Merano, with a busy multi-SKU line and real difficulty finding staff, the return came in 14 months.

What happens when something goes wrong? That depends heavily on the system you choose. Standard, pre-engineered solutions are easier to troubleshoot because operators recognize what's happening. Highly customized systems tend to create dependency on vendor support for even basic interventions. Ease of maintenance should be part of the selection criteria from the start.

EN_Fit-Tool_Web_Screenshot


Get a clear answer instantly:

✔️ Check if your application is compatible
✔️ Estimate ROI based on your inputs
✔️ Get a recommended configuration

👉 Start your evaluation now with the Palletizing Fit Tool

Leave a comment

Related posts

How IQ Gives Manufacturers a Faster, More Predictable Path to a Running Palletizing Workcell

Getting a palletizing project done right has always depended on having the right information at the right time. Product specs,...

Robotiq Team
By Robotiq Team - June 12, 2026
Robotiq Launches IQ to Make Palletizing Automation Faster and More Predictable

Most manufacturers who want to automate palletizing face the same problem. Getting a straight answer on whether it fits their...

Robotiq Team
By Robotiq Team - June 2, 2026