Subscribe

Latest Blog Post

New Robotiq Vision System Breaks Down Integration Barriers

Karine Simard
by Karine Simard. Last updated on Dec 19, 2024
Posted on Jun 21, 2016 in Vision Systems
2 min read time
 

We are proud to launch Camera, our new vision-guided pick and place solution for Universal Robots that shortens setup time to 5 minutes and makes vision easy to integrate.2F85__FT300__Camera_on_UR_2_2.png

Early users of the system say Robotiq’s Camera opens new possibilities for automation: “The Robotiq Camera breaks all the integration barriers that we are used to see with vision systems in manufacturing automation. We could think of many pick & place robot tasks that can now be programmed very fast. We will need this solution for upcoming projects with UR robots,”  says Victor Canton, Manufacturing Engineer, Continental Automotive Spain SA.


“We kept seeing projects that would work much better with machine vision, but manufacturers stayed away because of the complexity and cost of existing solutions,” explains Samuel Bouchard, CEO of Robotiq. “This is why we have set out to create a camera and vision software that could be set up and used by anyone.”

rsz_wrist-camera3.jpg

The compact camera design fits perfectly on the UR wrist and offers direct connectivity to the controller. Moreover, the Robotiq Camera’s user-friendly software is seamlessly embedded within Universal Robot’s graphical user interface. There is no external PC required to setup, program or run Camera.  Everything is done right from the robot user interface.

teach_vision-_camera_locate_1-780006-edited.png


You can teach Robotiq’s Camera a new part in just 5 minutes, and it will locate the part in its field of vision. Because of its unique wrist mount design on the UR, this robot vision system does not need complex calibration procedure or extra external illumination.  Being mounted on the robot's wrist also has the benefit of expanding the search area without dealing with complex fixtures. “The robot's arm moves, so the Camera can locate the parts in a wider work area,”  explains Jean-Philippe Jobin, Robotiq’s CTO.

Here is a demonstration of the simple steps in order to use the camera: 

 


Robotiq’s vision system for Universal Robots is commercially available now.  A live demonstration of the product can be seen at Robotiq’s booth at Automatica 2016, Hall B5, booth 512.


For more details visit the Product Page

Leave a comment

Related posts

How to Use Robot Vision With Big or Awkward Objects

What if your objects are too big or awkward to teach to a robot vision system?

Is robot vision only suitable for small, regular...

Alex Owen-Hill
By Alex Owen-Hill - August 21, 2020
Do Robots Need 3D Vision? One Insect Says No

To use 3D or not to use 3D? That's the question. Which properties are the most important for robot vision? The natural world...

Alex Owen-Hill
By Alex Owen-Hill - March 28, 2019
Bin Picking the Easy Way vs the Hard Way With Robot Vision

It's one of the trickiest robotic tasks in the world. But, you don't need a complex solution to solve it. There's a hard way to...

Alex Owen-Hill
By Alex Owen-Hill - March 21, 2019