Subscribe

Select Topics

Posts by Tag

See all

Latest Blog Post

The Right Gripper for the Kuka Lightweight Robot (LWR)

Nicolas Lauzier
by Nicolas Lauzier. Last updated on May 05, 2016 5:11 PM
Posted on Jun 05, 2012 9:25 AM. 3 min read time

The Kuka lightweight robot is innovative in many aspects. Its low weight and capability to detect external forces applied on it makes it the first robot of its kind to be safe enough to surround humans in their workspace. This capability has the potential to bring robotics into a new era, enabling many novel applications in various fields. However, a robot arm is nothing without a good end-effector and luckily for the LWR, our 3-Finger Adaptive Gripper has everything to be its perfect match!

The Fraunhofer IFF lightweight robot offering candies to the crowd at Automatica 2012

The Fraunhofer IFF lightweight robot offering candies to the crowd at Automatica 2012

Examples of Successful Integration

Presently, several institutions have a LWR equipped with a Robotiq Adaptive Gripper. For example, the Fraunhofer IFF (shown in the picture above) uses it as an industrial mobile manipulator; Kuka Labs has one on an OmniRob, another mobile platform; Université Laval's Robotics Laboratory has one for a research project on human-robot collaborationTecnalia recently acquired a Gripper for one of their Lightweight robots. The increasing popularity of the Kuka LWR / Robotiq Adaptive Gripper match is a sign that these versatile devices are well suited for each other.

Reasons for Being a Good Fit

One reason for which our Gripper is a great addition to the Kuka LWR is its intrinsic adaptability. Indeed, the LWR, due to its safety features, like its ability to detect external forces, is well suited for applications in which the robot evolves in an uncontrolled environment. These types of environments naturally require the ability to grip variously shaped objects.

Another reason is the payload for the robot which is 7kg. The 3-Finger Adaptive Gripper weights 2.3kg and has a recommended payload of 3kg for the fingertip grip and 10kg for the encompassing grip. These payloads synchronize well, so that the LWR equipped with the Adaptive Gripper is effective for gripping objects with different weights.

In addition to this, the Adaptive Gripper is rugged and able to withstand a high number of cycles with low maintenance, which makes it a flexible Gripper that is very robust and not fragile or prone to breakdown.

Ease of Integration of the Gripper on the LWR

This was a quick summary of some of the reasons for which the 3-Finger Adaptive Gripper is a great fit with the Kuka LWR. If you are considering the use of an LWR with one of our Grippers and you still have questions, please contact us and it will be our pleasure to help you find the best solution for your application.
Innovative robotic r&d projects robotiq

Leave a comment

Nicolas Lauzier
Written by Nicolas Lauzier
Senior Product Manager R&D
Connect with the writer:
http://www.robotiq.com

Related posts

What's New In Robotics?  07.12.2018

-UR celebrates 10 years since 1st sale-China robot production data -World's first automated ferry -Hello Bennu-Elowan the...

Emmet Cole
By Emmet Cole - December 7, 2018
Demo Week Highlights

What's trending on DoF this week? Demo week kick-off, circle move looped twice, security planes, use of Arduino to control...

Amanda Lee
By Amanda Lee - February 9, 2017
Trending on DoF This Week - Nov. 17

What's trending on DoF this week? Using one snapshot position to sort multiple parts, sampling rate for polishing, Revtech...

Amanda Lee
By Amanda Lee - November 17, 2016