Subscribe

Latest Blog Post

Robot Giving a Hand to Make... a Robot Hand!

Samuel Bouchard
by Samuel Bouchard. Last updated on Dec 19
Posted on Nov 30, in Robots
3 min read time

Bringing humans and robots together in the same working environment is a big research and development theme across the global robotics community. The promise of robots that are safe for humans will shift the paradigm about industrial robots from "programmable machines autonomously executing structured tasks" to "collaborative devices working with humans to complete loosely structured tasks". Instead of being considered like machinery, these new robots will be seen as a new generation of intelligent co-workers with whom human operators can intuitively interact to be more productive. Industrial platforms are not mature enough yet for extensive deployment, but the video below gives a preview of how a robot and an operator could collaborate to do fine assembly, for example at a robotic hand manufacturer, SME.

You can also download the video of the Kuka Light Weight robot with a robotic hand.

Human-Robot Collaboration: Why is it Interesting in Assembly?

Fine assembly is still a very challenging task for robots. The combination of sensory and fine motor skills that humans possess are extensively used in these tasks. This explains why there is a lot of room for automation in fine assembly. At any automotive car manufacturer for instance, you will see very few humans, but many robots doing the welding and painting. On the assembly side of the plant, it is the opposite situation. 

Considering that robotic capabilities will not be available in the short term to fully automate these fine assembly tasks, why not instead have collaborative robots helping humans so they can keep adding value continuously? In a factory, we want the operations that add the most value to the final product to be continuously running. In assembling, a worker adds value when he is putting parts together to make the product. Moving parts around or picking parts does not add value, so let's have a robot do this.

Kuka LWR Robotic with a Robotic Hand as a Co-Worker

robot-hand-kuka

The KUKA Light Weight Robot has many interesting features that make it suitable for human-robot interaction. Here are a few examples:

  • Round shape -- Sharp edges increase the risk of painful pressure points that a robot could exert when impacting with a nearby human co-worker. Having rounded parts is a simple way to decrease the risk that this problem occurs. 
  • Collaborative mode -- The robot is equipped with torque sensors at every joint and can be in impedance control mode. What this means is that instead of trying to follow a cartesian trajectory like an industrial robot usually does, the LWR controller makes it react to external efforts as if it was a mass-spring-damper system. Using the right parameters, this enables the operator to move the robot around intuitively and safely by interacting physically with it. This collaborative mode can be used to teach the robot trajectories or adjust its position/orientation for a better operator ergonomics before the part holding sequence.
  • Autonomous mode -- Like more conventional industrial robots, the LWR can move autonomously from point A to point B. So when the operator is not directly interacting with it, it can go fetch the next part to be assembled. Plus, it has a decent payload of 7 kg to move around parts.
In the video, the robot does several things so the human keeps assembling:
  • Feeds the human with the next part automatically.
  • Holds the parts for assembly operations that would require a holding device.
  • Indexes parts position between two successive tasks between which you would need to change the position/orientation of the assembly.

About this human-robot collaboration demonstration

The Laval University Robotics Laboratory acquired Adaptive Grippers and a Kuka LWR to pursue their work on human-robot physical interaction. As they were still setting up the equipment in the lab, we did with them this quick demo to show how the LWR equipped with one of our grippers can become a human helper in high-mix assembly tasks. You can view a similar demo done by the European SME Robots Research Consortium.

Compare 19 collaborative Robots here >>

Leave a comment

Samuel Bouchard
Written by Samuel Bouchard
Samuel is CEO and co-founder of Robotiq. His mission is to free human hands from repetitive tasks. He is also the author of Lean Robotics: A Guide to Making Robots Work in Your Factory. He lives in Québec City with his wife and four children.
Connect with the writer:
http://robotiq.com

Related posts

Industrial Robots: 5 Most Popular Applications

Industrial robots have been in use for about 50 years. The first industrial robot was used for material handling in a General...

Jean-Philippe Jobin
By Jean-Philippe Jobin - December 19, 2024
How to Combat The Great Resignation and Keep Talent with Robots

As the dust is settling on the 2020 global pandemic, many workers are finding themselves in a unique position. An abundance of...

Alex Owen-Hill
By Alex Owen-Hill - January 6, 2023
How to Convince Employees to Accept Robot Workers

When a company like yours first wants to adopt robots into the workplace, there can be resistance from employees.

Some people...

Alex Owen-Hill
By Alex Owen-Hill - October 25, 2022