Skip to content
English
  • There are no suggestions because the search field is empty.

Error - Capability not supported : DIGITAL_OUTPUT_MODE

Setting the correct Tool I/O Control Source in the UR Installation tab

This article addresses the “Capability not supported : DIGITAL_OUTPUT_MODE” error, commonly encountered when setting up a Robotiq Gripper with a Universal Robots controller. The issue typically results from incorrect configuration in the Installation > Tool I/O section of the UR interface. Proper configuration is essential for the gripper to communicate correctly with the robot.


Error Description

You may see the following error on your teach pendant during setup or when attempting to use the gripper:

pro-dZrywE8u.jpeg

This error prevents the gripper from functioning and is caused by an incorrect Tool I/O control setting, depending on your hardware configuration.


Resolution Steps

1. Open Tool I/O Menu

  1. On the UR teach pendant, go to Installation > General > Tool I/O Interface.

  2. Identify the Control Source setting.

2. Identify Your Coupling Type

Check which type of Robotiq coupling you are using:

  • CB-Series coupling

  • E-Series coupling

  • I/O coupling

3. Apply the Correct Setting

Set the Control Source as follows:

  • CB-Series coupling
    → Set to: Controlled by Users

  • E-Series coupling
    → Set to: Controlled by Robotiq Gripper

  • I/O coupling
    → Set to: Controlled by Robotiq Wrist Connection

⚠️ If you are unsure of your coupling type, refer to Couplings and Cables for Universal Robots (UR) Robots. 


Conclusion

The “Capability not supported : DIGITAL_OUTPUT_MODE” error is resolved by selecting the correct Control Source in the Tool I/O menu, based on your coupling type. Always verify this setting during initial setup to avoid communication issues with your gripper.

Need help? Contact Robotiq Support.

Updated: August 25, 2026